Arduino Portenta H7 Development Board

View table of contents ...  

image

 

{tabbedtable} Tab LabelTab Content
About

Portenta H7 simultaneously runs high level code along with real time tasks. The design includes two processors that can run tasks in parallel. For example, is possible to execute Arduino compiled code along with MicroPython one, and have both cores to communicate with one another. The Portenta functionality is two-fold, it can either be running like any other embedded microcontroller board, or as the main processor of an embedded computer. Use the Portenta Carrier board to transform your H7 into an eNUC computer and expose all of the H7 physical interfaces. Portenta can easily run processes created with TensorFlow™ Lite, you could have one of the cores computing a computer vision algorithm on the fly, while the other could be making low-level operations like controlling a motor, or acting as a user interface.

image

H7's main processor is the dual core STM32H747 including a Cortex® M7 running at 480 MHz and a Cortex® M4 running at 240 MHz. The two cores communicate via a Remote Procedure Call mechanism that allows calling functions on the other processor seamlessly. Both processors share all the in-chip peripherals and can run:

 

Graphics Accelerator Probably one of the most exciting features of the Portenta H7 is the possibility of connecting an external monitor to build your own dedicated embedded computer with a user interface. This is possible thanks to the STM32H747 processor's on-chip GPU, the Chrom-ART Accelerator™. Besides the GPU, the chip includes a dedicated JPEG encoder and decoder.

 

A new standard for pinouts The Portenta family adds two 80 pin high density connectors at the bottom of the board. This ensures scalability for a wide range of applications by simply upgrading your Portenta board to the one suiting your needs.

 

On-board Connectivity The onboard wireless module allows to simultaneously manage WiFi and Bluetooth® connectivity. The WiFi interface can be operated as an Access Point, as a Station or as a dual mode simultaneous AP/STA and can handle up to 65 Mbps transfer rate. Bluetooth® interface supports Bluetooth Classic and BLE. It is also possible to expose a series of different wired interfaces like UART, SPI, Ethernet, or I2C, both through some of the MKR styled connectors, or through the new Arduino industrial 80 pin connector pair.

 

USB-C Multipurpose Connector The board's programming connector is a USB-C port that can also be used to power the board, as a USB Hub, to connect a DisplayPort monitor, or to deliver power to OTG connected devices.

 

The Arduino Portenta H7 is based on the STM32H747 microcontroller, XI series.

 

  • Microcontroller STM32H747XI dual Cortex®-M7+M4 32bit low power ARM MCU (datasheet)
  • Radio module: Murata 1DX dual WiFi 802.11b/g/n 65 Mbps and Bluetooth 5.1 BR/EDR/LE (datasheet)
  • Secure Element (default): NXP SE0502
  • Board Power Supply (USB/VIN): 5V
  • Supported Battery: Li-Po Single Cell, 3.7V, 700mAh Minimum (integrated charger)
  • Circuit Operating Voltage: 3.3V
  • Current Consumption: 2.95 μA in Standby mode (Backup SRAM OFF, RTC/LSE ON)
  • Display Connector: MIPI DSI host & MIPI D-PHY to interface with low-pin count large display
  • GPU: Chrom-ART graphical hardware Accelerator™
  • Timers: 22x timers and watchdogs
  • UART: 4x ports (2 with flow control)
  • Ethernet PHY: 10 / 100 Mbps (through expansion port only)
  • SD Card Interface for SD Card connector (through expansion port only)
  • Operational Temperature: -40 °C to +85 °C
  • MKR Headers: Use any of the existing industrial MKR shields on it
  • High-density Connectors: Two 80 pin connectors will expose all of the board's peripherals to other devices
  • Camera Interface: 8-bit, up to 80 MHz
  • ADC: 3× ADCs with 16-bit max. resolution (up to 36 channels, up to 3.6 MSPS)
  • DAC: 2× 12-bit DAC (1 MHz)
  • USB-C: Host / Device, DisplayPort out, High / Full Speed, Power delivery
Important Dates

Enrollment Begin: Sept 22 2020

Enrollment Ends: Oct 27 2020

RoadTesters Selected: Nov 6 2020 (estimated)

Product Shipped: Nov 13 2020

RoadTesting Begins: Nov 20 2020

Reminder/Update Email: Dec 20 2020

Submit Reviews By: Jan 20 2020

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

Terms and Conditions

Arduino Portenta H7 Dev Board

Terms and Conditions

These are the terms and conditions which govern the IArduino Portenta H7 Dev BoardRoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

 

Key dates:

Applications Close: midnight (GMT) on Oct 27 2020

Announcement of Winner (estimated): Oct 30 2020

Prize:Arduino Portenta H7 Dev Board

Additional Prizes: none

Competition Site: https://www.element14.com/community/groups/roadtest?ICID=menubar_resources_roadtest

Site or element14 Community: www.element14.com/community

Judges: members of the element14 community team chosen at the Organiser’s discretion.

Judging Criteria, All of the following which will have equal weighting:

· Demonstrated competence with the technologies including links or descriptions of past projects

· Qualifications as indicated by current job role and/or schooling/vocational training;

· A thorough description of how the prize would be tested;

· Likelihood that the Applicant will blog about the prize and provide a review on element14.com;

· Originality;

· Innovation.

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:

· Provide a RoadTest application describing what he/she would do if awarded the Prize including similar previous projects, product experience and qualifications

Terms: these terms and conditions which govern the Competition and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

  1. Eligibility
  2. Applications:
  3. Selecting Winners:
  4. Liability:
  5. General:

1.1 Save as set out in these Terms, the Contest is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.2 All Applicants must be aged at least 18 at the time of their application.

1.3 Applicants must not enter the RoadTest if doing so or taking part may:

1.3.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.3.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.3.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in competitions such as these or receiving prizes under them and the Organiser respects those policies and practices.

The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly.

1.4 Multiple applications are not permitted.

1.5 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.6 The Contest is NOT open to:

1.6.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.6.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser and Sponsors; or

2.1 Each Applicant must fully complete and submit a RoadTest Application by the Application Close.

2.2 By submitting a Registration Form, each Applicant:

2.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the RoadTest;

2.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

2.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

2.2.4 Authorises the Organiser to copy, reproduce and use the Application and/or Review for the purposes of the RoadTest and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

2.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Contest. As between the Applicant and the Organiser the IP remains owned by the Applicant.

2.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Contest or the promotion of it or the Site;

2.2.7 Agrees to participate positively in all publicity surrounding the Contest;

2.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Contest (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

2.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

2.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the RoadTest.

2.3 All applications submitted to this RoadTest must meet the following criteria:

2.3.1 Applicants must be the author, creator and owner of the proposed review idea. Applicants must not submit someone else’s idea;

2.3.2 The proposed application must be reasonably achievable by the within the time constraints of the Contest;

2.3.3 Applications must not include or propose any of the following, the inclusion of which shall render any proposed application ineligible:

(a) Applications which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) Applications that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser;

(c) Applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

2.4 No Application may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

3.1 Winners will be selected by the Organiser on the basis of the quality of his or her application and its adherence to these Terms.

3.2 The total number of Winners selected will be at least the minimum number set out above but the actual number is at the sole discretion of the Organizer and/or the Sponsor, if applicable.

3.3 The Organiser will use all reasonable efforts to announce the Winners via an update to the RoadTest page by the date listed above.

3.4 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the RoadTest, the Products featured or other Contests with which the Organiser may be connected from time to time.

3.5 Details of the Winners may also be published in the media.

3.6 Winners are responsible for all applicable taxes, duties or other charges payable in relation to any prize.

3.7

4.1 The Organiser hereby excludes all and any Liability arising out of the Contest or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

4.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

4.3 Subject to 4.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Competition or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Competition, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned.

5.1 The RoadTest is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the RoadTest to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

5.2 The RoadTest may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a competition of this nature. The Organiser has the right to cancel or suspend the RoadTest at any time due to circumstances outside its reasonable control.

5.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the RoadTest or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

5.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the Contest Site and it is a condition of entry to the RoadTest that Applicants agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

5.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

5.6 These Terms and the operation of the Contest shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.

RoadTest Reviews
Comments
Anonymous
  • Thanks ,  I received the Arduino Portenta H7, looking forward to the road test.

    imageimage

  • I look forward to some great test reports.

     

    DAB

  • Congratulations to the road testers. This is a superb Arduino.

  • Important Dates Update

     

    Enrollment Begin: Sept 22 2020

    Enrollment Ends: Oct 27 2020

    RoadTesters Selected: Nov 6 2020 (estimated)

    Product Shipped: Nov 13 2020

    RoadTesting Begins: Nov 20 2020

    Reminder/Update Email: Dec 20 2020

    Submit Reviews By: Jan 20 2020

    *The element14 RoadTest Staff will send this reminder/update email.

    **If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

     

  • The following applicants have been selected as official roadtesters:

     

  • To all applicants,

     

    I've read all the applications for the first time. A lot of great ideas.

     

    There were 10 applications that did not answer any of the questions. Our policies are clear on this point. You have to answer all the questions. I will accept anything. (Not saying you will be selected as an official roadtester with anything!) But those eliminated did not provide any info whatsoever.

     

    Randall Scasny

    RoadTest Program Manager

  • The roadtest closed before a few hours of its countdown time, idk how... It was night time in India so I thought I would submit the application in the morning but it closed a few hours before what the counter had shown when I checked it in the night... I was a bit busy with other things because of which i got late in submitting my application but I really wanted to try this board - one of my projects can serve as an excellent roadtest for it...

  • The nRF52840 (and the nRF52832) also supports javascript btw image same with STM32F401/411 chips.

     

    Just posting it here in case you're interested in comparing those with the Arduino bunch too.

  • I opened it until October 30th. Hope that's enough time to submit an application.

     

    Randall

  • I didn't say he didn't see it. I just made a comment stating that it is possible someone could see the RoadTest posted in locations other than this site since these are being advertised elsewhere.

     

    How do you know they did not make an effort to submit for the RoadTest? Perhaps they were ready to do so but found it closed prior to the extended date. I'm not going to speculate their actions.

     

    Perhaps this attitude and mindset is the reason why there are fewer folks submitting for RoadTests.  It certainly doesn't motivate me.

  • At least from what I've saw from Neeraj's comments expressing how he wasn't able to be selected for 2 prior ones he already found the roadtest program and had made a review too... he also made applications to two other RoadTests...

     

    I wouldn't quite say he didn't see it, more like he didn't do anything about it until the deadline.

     

    Randall did indeed promise to open it up, but as Neeraj didn't attempt to make an application that is quite annoying to Randall.

  • Well, I've been seeing the RoadTests advertised on LinkedIn and other non element14 sites so it is possible that someone could learn of this rather late in it's posting and not see when it was first posted.  But, in all fairness, in this particular case, Randall posted he would extend submitting for the RoadTest until October 30th, so to close it 2 days prior seems a bit odd.

     

    I'm not taking a side on this, but I do not recall a time when it was posted that a RoadTest was being extended and then closed a couple of days prior. But, I don't run these and it is at the discretion of element14 to make changes as it sees fit.

     

    At least that is how I am seeing it.

  • I must take Randall's side...  usually I write my application as soon as I get an idea within the first 10 days, it's been open for a month and it's Neeraj's fault they didn't complete the applciation in time.

     

    It's not like a one week or two week enrollment period, a month should be enough time.

  • Randall,

     

    Although it is not my place to comment on this exchange and I really do believe you do a great job managing these RoadTests, however in this case I think it would be fair to allow for the extra time to post to the RoadTest.  You did post you would extend submitting until October 30th, so to be fair to Neeraj it might be best to honor that. It is possible that others had seen this and were considering submitting but would not be able to now.

    And, considering you have posted recently asking why folks are not submitting for RoadTests, I would think there would be more flexibility.

     

    Just my ha'penny worth of input.

     

    Cheers,

     

    Jon

  • The roadtest has been running for 34 days, 4-days over the required 30-day enrollment period. I checked the applications and did not see yours.So I figured you no longer wanted to apply. I had waited for you to apply after commenting on Oct 26th--two days ago. I would suggest you plan to submit your application in a more timely manner--65 other people applied before the deadline.

    Randall

  • Dear Sir,

                   You have enclosed enrollment today. That is 2 days before 30th Oct,2020.

     

    THANKS

    NEERAJ GUPTA   

  • All good in your side & i understand your limitations. I will respond positively.

     

    THANKS

    NEERAJ GUPTA

  • Neeraj,

     

    This roadtest has been in enrollment since Sept 22nd. I think I have given you plenty of time without even extending it. I'm willing to extend it one day.

     

    Randall

  • I would like to try but catch is that it is my working day.

     

    THANKS

    NEERAJ GUPTA