The The specified item was not found.Esplora is a microcontroller board derived from the The specified item was not found. Leonardo. The Esplora differs from all preceding Arduino boards in that it provides a number of built-in, ready-to-use setof onboard sensors for interaction. It's designed for people who want to get up and running with Arduino without having to learn about the electronics first. For a step-by-step introduction to the Esplora, check out the Getting Started with Esplora guide.
The Esplora has onboard sound and light outputs, and several input sensors, including a joystick, a slider, a temperature sensor, an accelerometer, a microphone, and a light sensor. It also has the potential to expand its capabilities with two Tinkerkit input and output connectors, and a socket for a color TFT LCD screen. Like the Leonardo board, the Esplora uses an Atmega32U4 AVR microcontroller with 16 MHz crystal oscillator and a micro USB connection capable of acting as a USB client device, like a mouse or a keyboard.
In the upper left corner of the board there is a reset pushbutton, that you can use to restart the board. There are four status LEDS:
ON [green] indicates whether the board is receiving power supply
L [yellow] connected directly to the microcontroller, accessible through pin 13
RX and TX [yellow] indicates the data being transmitted or received over the USB communication
The board contains everything needed to support the microcontroller; simply connect it to a computer with a USB cable to get started.
The Esplora has built-in USB communication; it can appear to a connected computer as a mouse or keyboard, in addition to a virtual (CDC) serial / COM port.
Testers will be selected on the basis of quality of applications: we expect a full and complete description of why you want to test this particular product.
Testers are required to produce a full, comprehensive and well thought out review within 2 months of receipt of the product.
Failure to provide this review within the above timescale will result in the enrolee being excluded from future Road Tests.
I really just want to see what this little guy can do. My first project would be the obvious, a HID controller. Then maybe hook up a display to it and make it a standalone handheld gaming device. Possibly hook it up to a pi and use it as a controller and drive its own display. I don't know really, but I would love one to play with.
Right now I'm working on a safety device for homes that can save up to 30.000 lives a year here in the US alone. I can test this device and its inputs and outputs along with my project in different ways.