Oscilloscope experience redefined: The InfiniVision 2000 X-Series oscilloscopes offer entry-level price points to fit your budget with superior performance and optional capabilities that are not available in any other oscilloscopes in this class, including recently added serial analysis capabilities and memory option. Agilent’s breakthrough technology delivers more scope for the same budget.
Development Kit
We have included with this RoadTest, the STM32F4DISCOVERY board. This innovative kit helps you to discover the STM32F4 high-performance features and to develop your applications easily. It includes everything required for beginners and experienced users to get started quickly.
Based on the STM32F407VGT6, it includes an ST-LINK/V2 embedded debug tool, two ST MEMS, digital accelerometer and digital microphone, one audio DAC with integrated class D speaker driver, LEDs and push buttons and an USB OTG micro-AB connector.
A large number of free ready-to-run application firmware examples are available on www.st.com/stm32f4-discovery to support quick evaluation and development.
To expand the functionality of the STM32F4 Discovery kit with Ethernet connectivity, LCD display and more, visit - www.st.com/stm32f4dis-expansion.
Key features/Specifications
Key specifications
70, 100, and 200 MHz bandwidth models
2 or 4 analog channels plus 8 digital channels (on MSO models or with the DSOX2MSO upgrade)
50,000 waveforms/sec update rate
8.5-inch display
Up to 2 GSa/s sample rate
Up to 1 Mpts MegaZoom IV responsive, uncompromised memory
Key features
See more of your signal more of the time with the largest screen in its class, the deepest memory and fastest waveform update rates
Do more with the power of up to 5 instruments in 1: oscilloscope, logic timing analyzer, WaveGen built-in 20-MHz function generator (optional), serial protocol triggering and decode (optional) and digital voltmeter (optional)
Get more investment protection with the only fully upgradable scope in this class, including memory and bandwidth, and a standard 5-year warranty
Video
This video is unavailable.
You don't have permission to edit metadata of this video.
Terms & Conditions
Testers will be selected on the basis of quality of applications: we expect a full and complete description of why you want to test this particular product.
Testers are required to produce a full, comprehensive and well thought out review within 2 months of receipt of the product.
Failure to provide this review within the above timescale will result in the enrolee being excluded from future Road Tests.
I'll add it to my list of things to look at. From previous experience, the interface on oscilloscopes usually doesn't lend itself well to entering text. I tend to either rename the files/add anotations once I've got the files on a PC.
Actually I've heard these scopes have some sort of web interface, and there is definitely PC control software available. Those are probably better options for capturing images, as then you have a full PC with a keyboard for typing.
Now we're on the subject of requests: one of the things I was curious at, was how the text entry (trace labels, file names) works; I've used the 3014 in the past, and found the text entry a bit clumsy at times. The sales engineer I talked to at the time told me a new firmware version would improve it, but since my contract ended a few months later I haven't checked again. Would be nice to see a demo / evaluation of that.
well, i just say that review looks better if you add at least one picture, or video. Think of this way, will you buy a car just by reading plane text ?
Just simple idea: In Terms & Conditions will add section, that at least one normal/good quality picture must be added to review. I believe if some one can enroll to roadtest , making one photo will not hurt, and lot of review don't have any pictures, just raw text. Well, that is my piont of view, i like to see stuff, not just read about it.
We have had a high number of very good quality applications, I'd like to thank everyone for taking the time in being so thorough. It's been a difficult choice, but after careful consideration, we've selected the following three applicants -
Sergiusz Bazański
Gregory M. Brettell
Jeremy Kuek
Thank you again, and I look forward to receiving your applications for other RoadTests.
Intensity graded display with high update rate is THE feature to have on a dso, IMHO. Sometimes it is so much easier to visually asses a situation than to pour over memory searching for pattern.
I am surprised to see that Danaher and Teledyne more or less completely ignore these new standards in the entry level dso arena. I know that money is better in the mid/high range, but once a young engineer starts with Agilent, guess whose rep they will call when they get a couple 100k budget for a new machine:)
I would love to do a review on this kit - developing a mixed signal application on the STM32 board and using the scope to its best capabilities - right up my street. Great Road Test - good luck everyone
Agilent’s InfiniiVision MSOX2024A, offers entry-level price points to fit your budget with superior performance and optional capabilities that are not available in any other oscilloscope in its class. The MSOX2000 Series adds 8 x digital/logic inputsin addition to the standard analog channels.