Enrollment closes in
Days 0 Hours 0 Mins 0 Secs 0
Powered separately to the Raspberry Pi means that the PiRack will not affect performance. This carrier card is part of the PiFace series and can be used with most IO expansion boards that are compatible with the Raspberry Pi IO header. PiRack also enables the Pi Camera Module to be used at the same time. By taking IO expansion boards directly off the Raspberry Pi, PiRack enables the camera module to easily connect onto the Raspberry Pi using to the top mount CSI interface.