InfiniiVision 1000 X-Series Oscilloscope DSOX1102G

View table of contents ...  

 

image

 

 

 

{tabbedtable} Tab LabelTab Content
About This RoadTest

The Keysight Technologies' InfiniiVision 1000 X-Series oscilloscope delivers professional-level functionality with industry-leading software analysis and 6-in-1 instrument integration. It uses Keysight’s MegaZoom IV custom ASIC technology, which enables a high 50,000 waveforms per second update rate. This makes it easier to see random and infrequent glitches and anomalies that similarly-priced oscilloscopes might miss. The 1000 X-Series also has a high sampling rate of up to 2 GSa/s and comes standard with two probes. And it uses segmented memory capability to maximize memory depth while helping the scope test faster.

 

image

 

Ideal for New Users

The 1000 X-Series oscilloscopes are ideal for new users and students. Not only are they low cost, but learning how to use the scope and set up measurements is simple. The front panel is easy to use and features built-in help so new users can quickly analyze signals to deliver results. The kit includes built-in training signals, a comprehensive oscilloscope lab guide written specifically for undergraduate students, and an oscilloscope fundamentals slide set for professors and lab assistants.

 

Six-in-one instrument integration

Six-in-one instrument integration means the 1000 X-Series gives users even more value for their money and saves valuable bench space. In addition to being an oscilloscope, the 1000 X-Series is also a serial protocol analyzer, digital voltmeter and frequency counter. The DSOX1102G model includes a frequency response analyzer and WaveGen function generator. Bode plot fundamentals are easy to teach with the built in WaveGen and frequency response analysis.

image

Signal Analysis

The 1000 X-Series provides professional-quality measurement and software analysis capability. The scope features 24 typical oscilloscope measurements to quickly analyze signals and determine signal parameters. Additional signal analysis is provided by the gated FFT function, which allows users to correlate time and frequency domain phenomenon on a single screen. And mask limit testing is also available to help users easily detect signal errors. The 1000 X-Series supports decoding and analysis of a wide range of popular embedded and automotive serial bus applications, which include I2C, SPI, UART/RS232, CAN and LIN.

 

DSOX1102G Features

 

  • Analog Channels: 2
  • Digital Channels: 1
  • Bandwidth: 70 MHz (base) / 100 MHz with DSOX1B7T102 option
  • Maximum Sample Rate: 2 GSa/s
  • Maximum Memory Depth: 1 Mpts
  • Segmented Memory: Standard
  • Mask/limit testing: Standard
  • WaveGen: 20 MHz function generators (includes Bode plot test)
  • Serial Protocol Analysis: I²C, SPI, UART/RS-232 - (DSOX1EMBD); CAN, LIN - (DSOX1AUTO)
  • Waveform math: Add, subtract, multiply, divide, FFT (magnitude and phase), low pass filter
  • Integrated digital voltmeter
  • Display: 7-inch TFT LCD WVGA
  • Waveform update rate: 50,000 waveforms per second
  • Connectivity: USB 2.0 (host and device)

 

Note: The total number of winners selected will be at least the minimum number set out above, but the actual number is at the sole discretion of the Organizer and/or the Sponsor.

Important Dates

Enrollment Begins: Mar 2, 2017

 

Enrollment Ends: Apr 7, 2017

 

RoadTesters Selected: Apr 18 2017

 

Product Shipped: Apr 21 2017

 

RoadTesting Begins: Apr 28 2017

 

Status Reminder/Update Email: Jun 13 2017*

 

Submit Reviews By: Jun 27 2017

 

* Status Reminder Email is sent by element14 RoadTest Program staff

Unboxing Video
Terms and Conditions

InfiniiVision 1000 X-Series Oscilloscope DSOX1102G  – RoadTest

Terms and Conditions

These are the terms and conditions which govern the InfiniiVision 1000 X-Series Oscilloscope DSOX1102G RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

InfiniiVision 1000 X-Series Oscilloscope DSOX1102G(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on 3  March 2017

Announcement of Winner (estimated): 3 May 2017

Prize:  InfiniiVision 1000 X-Series Oscilloscope DSOX1102G

Additional Prizes: none

Competition Site: https://www.element14.com/community/groups/roadtest?ICID=menubar_resources_roadtest

Site or element14 Community: www.element14.com/community

Judges: members of the element14 community team chosen at the Organiser’s discretion.

Judging Criteria, All of the following which will have equal weighting:

· Demonstrated competence with the technologies including links or descriptions of past projects

· Qualifications as indicated by current job role and/or schooling/vocational training;

· A thorough description of how the prize would be tested;

· Likelihood that the Applicant will blog about the prize and provide a review on element14.com;

· Originality;

· Innovation.

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:

· Provide a RoadTest application describing what he/she would do if awarded the Prize including similar previous projects, product experience and qualifications

Terms: these terms and conditions which govern the Competition and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

  1. Eligibility
  2. Applications:
  3. Selecting Winners:  
  4. Liability:
  5. General:

1.1 Save as set out in these Terms, the Contest is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.2 All Applicants must be aged at least 18 at the time of their application.

1.3 Applicants must not enter the RoadTest if doing so or taking part may:

1.3.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.3.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.3.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in competitions such as these or receiving prizes under them and the Organiser respects those policies and practices.

The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly.

1.4 Multiple applications are not permitted.

1.5 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.6 The Contest is NOT open to:

1.6.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.6.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser and Sponsors; or

2.1 Each Applicant must fully complete and submit a RoadTest Application by the Application Close.

2.2 By submitting a Registration Form, each Applicant:

2.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the RoadTest;

2.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

2.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

2.2.4 Authorises the Organiser to copy, reproduce and use the Application and/or Review for the purposes of the RoadTest and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

2.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Contest. As between the Applicant and the Organiser the IP remains owned by the Applicant.

2.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Contest or the promotion of it or the Site;

2.2.7 Agrees to participate positively in all publicity surrounding the Contest;

2.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Contest (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

2.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

2.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the RoadTest.

2.3 All applications submitted to this RoadTest must meet the following criteria:

2.3.1 Applicants must be the author, creator and owner of the proposed review idea. Applicants must not submit someone else’s idea;

2.3.2 The proposed application must be reasonably achievable by the within the time constraints of the Contest;

2.3.3 Applications must not include or propose any of the following, the inclusion of which shall render any proposed application ineligible:

(a) Applications which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) Applications that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser;

(c) Applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

2.4 No Application may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

3.1 Winners will be selected by the Organiser on the basis of the quality of his or her application and its adherence to these Terms.

3.2 The total number of Winners selected will be at least the minimum number set out above but the actual number is at the sole discretion of the Organizer and/or the Sponsor, if applicable.

3.3 The Organiser will use all reasonable efforts to announce the Winners via an update to the RoadTest page by the date listed above.

3.4 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the RoadTest, the Products featured or other Contests with which the Organiser may be connected from time to time.

3.5 Details of the Winners may also be published in the media.

3.6 Winners are responsible for all applicable taxes, duties or other charges payable in relation to any prize.

3.7

4.1 The Organiser hereby excludes all and any Liability arising out of the Contest or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

4.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

4.3 Subject to 4.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Competition or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Competition, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned.

5.1 The RoadTest is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the RoadTest to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

5.2 The RoadTest may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a competition of this nature. The Organiser has the right to cancel or suspend the RoadTest at any time due to circumstances outside its reasonable control.

5.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the RoadTest or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

5.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the Contest Site and it is a condition of entry to the RoadTest that Applicants agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

5.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

5.6 These Terms and the operation of the Contest shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.

Official RoadTesters

Thanks for everyone who applied. I will say it was a difficult decision because the supplier told me they were amazed at all of the high quality of applications. Here are the people who were chosen as official RoadTesters:

 

Tax LiabilityAs per the RoadTest T&Cs, you are responsible for taxes associated with this product. For US applicants, if you are selected as an official RoadTester, you will be issued a 1099 that will report the product as income due to the cost of this product.
RoadTest Reviews
Comments
Anonymous
  • Hi Mark,

    yes the language overlay on the oscilloscope is in German (I'm living in Austria).
    Indeed, the menu language also the help comes in mixed languages.

    And also here in this forum.... image we also talking about in (D)English.

    I switched the browser favorite language to English because some web site frames and forms are in English.

     

    Is it frustrating to have to work simultaneously in two languages when using the oscilloscope?

    Every days my live is in 3 languages, de, en, hu. image Is there a doctor who can help me because i have migraines.image
    But i use a translating tool for complex sentences.

     

    The DSO1102G is a good device for many measurements.

    But better, I suggest a 4-channel oscilloscope with minimum 200 or 300Mhz.
    In digital measurements are the most important lines, Enable, Read, Write, CS, etc...
    With which you can synchronize the data, address measurements.
    Going there is now a MDO the better solution, then you have everything in one device.
    I love to see everything at the same time. So for serial data logs to capture,

    a 3 to 4 channel device would be just right or minimum.

     

    So the DSO1102G would good for service but a bit small in the laboratory.

     

    Best Regards,

    Gerald

    ---

  • Thanks for posting this Gerald. I don't have any SPI devices set up for testing right now, so it is great that you contributed this.

     

    I notice that you have selected German language overlay on the oscilloscope (Ich denke dass ist Deutsch ich sehe im video).  I also noticed that only some of the text appears in German.  The menu boxes are a mix of German and English, but the help screen for the SPI signals is entirely in English. I expected the language support would have been complete and consistent for all functions.

     

    Is it frustrating to have to work simultaneously in two languages when using the oscilloscope?

  • Hi All,

     

    Unfortunately, I was not one of the winners of this Roadtest but thankfully, I could borrow the DSO1102G from the friendly company X-Test for testing in the Roadtest TLE94112EL_shield.
    Infineon DC Motor Shield w/ TLE94112EL for Arduino - Review

     

    X-TEST in Austria: Many thanks to Mr. Brandtner.

    https://www.element14.com/community/external-link.jspa?url=http%3A%2F%2Fwww.xtest.at%2F1000x%2F

    https://www.element14.com/community/external-link.jspa?url=http%3A%2F%2Fwww.xtest.at%2Ffeedback-kontakt%2F

     

    Here, in this Roadtest, the most important for me was testing the SPI interface.
    I would like to contribute as a review here in this post.

    SPI normally requires 3 or 4 lines:
    MOSI, MISO, CLK, EN

    But the DSO1102G has only 2 measurement channels and 1 input for triggering.
    How can you display at least 3 lines at the same time? - I've set this up:
    The external trigger I used for the CLK line, the second channel for EN, the first channel for either MOSI or MISO.
    With this setting you can test an Enable controlled SPI interface.

     

     

    The example timing diagram of the TLE94112EL Roadtest:

    image

     

    1) Set BUS to digital serial - SPI (in the video just was shown that BUS was now set as 2. setting; but if you set BUS after the Trigger, Trigger will not show the Trigger type)

    2) Set the Trigger to external and set the type of Trigger to SPI.

    Set the Bit with to 16 bits, set the Trigger edge to X

    3) Set the BUS Signals

    - CLOCK to external, level to middle of the signal level (50%), trigger edge: LOW for SDI, HIGH for SDO as mentioned in the datasheet

    - MOSI or MOSI, I used the 1. channel (yellow) of the DSO; set the signal level to middle (as mentioned in the datasheet - timing diagram); the triggering edges are also described in the datasheet

    - CS, I used the 2. channel (green); set to the frame signal edge so that the trigger will start if the CS starts or ends.

    - CS is low active, so I've set the signal level down to near 10% above GND.

    - Set to bit width to 8 bit.

    - Set LSB/MSB to LSB - the needing of this can you read in the datasheet

     

    Also the trigger: automatic - If you set to automatic, the displayed signal will run over the screen and measuring or reading would be difficult.

    The right setting would be, set the trigger to "normal" and set to the correct edges, bit rates, data bit width, then the trigger will work fine and the data values will displayed syncronized correctly to the SLCK signal (third 1/3 of the video).

     


    The other option is to test the SPI with SCLK timeout.

     

     

    Basically the setting will be the same but in the BUS settings the CS will be changed from CS edge to clock timeout.


    Here I have also set the external trigger for the SCLK, but the two vertical inputs are connected to with the data lines,
    channel 1 for MOSI, channel 2 for MISO (but sorry in this video was wrong pressed the button MOSI to 2 but the probe was connected to SDO).
    With this setting you can now measure both data lines simultaneously, synchronized with SCLK.
    The timeout after the last Clock_Cycle terminates the trigger.

    This timeout can be set at the Scope, eg. 100μs after the last clock, a new transmission frame is displayed.

    The DSO1102G also displays the associated data values with the BUS_ setting.

    In the videos shown, I show the different settings.
    Also, deliberate error settings, so you can see how the data is misrepresented.
    An important point in this is setting the trigger levels, and edges.

     

    Ok, a 4 channel oscilloscope would be nice to measure all lines simultaneously.

     

    A bit confusing can be with MOSI, MISO, SDO, SDI.... "who is who, which is which...."

    Well this DSO1102G is a fine oscilloscope.

     

    Thank you very much to all Roadtesters for your fine review.

     

    Best Regards

    Gerald

    ---

     

     

     

  • Thanks for keeping on top of everything Road Test related.  The program has realized improvements under your keen oversight.

     

    Congratulations to my fellow Road Testers on completing their fine reviews of this capable entry level instrument.  I enjoyed the review process and have plans to add a few more sections to my review.

     

    Mark A

  • Thanks Hendrik!

    Looking forward to your review.

  • Google did find this page for me: Download FREE Digital Voltmeter (DVM) for 1000 X-Series Oscilloscopes | Keysight (formerly Agilent’s Electronic Measurem…  where I got the license file for the DVM. It also explains how to install it.

    The frequency counter is part of the DVM functionality (although you need a signal with an AC part to be able to select it)

  • Till date, I have never used a Keysight scope. The TBS12xx serves us well but your inputs will be very useful to understand the ups and downs.

    All the best.

  • My scope arrived on time (on Thursday). I looked up the installed licenses, and its fully loaded (full bandwidth and all the serial triggers). I need to do the registration. The scope is a tad smaller than my TBS1202B-EDU (about 1cm), but it is much heavier. And the fan is quite loud - this is something that I need to look into it.

    From my first impressions it seems that Keysight  attached great importance to usability. Many tasks that need to be done regularly are easily accessible. I need to do more work with it do find out which layout of the controls I like better, but so far I did not find any fault with the Keysight.

    (But first I need to repair my main computer - it seems as if its Linux OS partition is gone, so I need to reinstall image  But thats why you want to have some buffer in your test schedule...

  • Peter,

     

    I have registered the 'scope with Keysight, but I don't see where you get the license for the voltmeter and counter.

    Any hints?

  • Thanks Mark.

     

    I had the same impression as well. It was small! I'm looking forwardign to the reviews.

     

    Randall

  • , the DSOX1102G arrived safe and sound this afternoon!

    image

    Appears to have the same configuration as unit.

    Looks positively miniature next to my Tektronix MDO4104-3, however, after playing with it for just a few minutes I can tell this scope punches well above its weight.

    I am so looking forward to getting to know this little beast better over the course of my review.

  • I actually planned buying the DSOX1EMBD license since I would need it (and with 140EUR its priced quite OK). If its included with the test, that would be perfect though.

  • I completely agree with you on that.

     

    Kas

  • Cool, I probably would have made a proposal if I had thought all those serial options would be included.

  • You lucky ducky!

    Now you've got something to CRO about!

     

    Here's a challenge to all of the roadtesters - see if they can get their 1000X to decode OWP (One Wire Protocol).

    It can be done so there is a solution.

    Take up the challenge and show us!

     

    Whilst you're at it - take the challenge and show it decoding the IBM PS/2 or PC AT keyboard protocol.

  • Hi All, I just verified on my scope (It arrived a few days ago image )

    the included options are as follows (Assuming there all the same)

     

    • DSOX1EMBD - Serial protocol analyzer – triggering and decode  (I2C, SPI, RS232)
    • DSOX1AUTO - LIN and CAN bus.
    • DSOX1B7T102 - Upgrade from 70Mhz to 100Mhz
    • WaveGen built-in 20 MHz function generator
    • Digital voltmeter and frequency counter (Licence when you register the scope)

     

    Oh and it comes with 2 * 200Mhz passive probes. switchable between 10:1 and 1:1 input attenuation

     

    There is nothing I can find to imply these are just time limited versions so it looks like there for life .... NICE.

     

    That's pretty much every option there is for this scope, the only other thing I know you could do with it is hack in a 200Mhz upgrade image but this is not for the faint of heart and will absolutely void any warranty and you could destroy your scope in the process, if your ever tempted to do this I would suggest wait till the end of the road test or you may not be able to complete it. I also make no claims to the ethical nature of this hack, Dave Jones is a very popular blogger and has a great relationship with Keysight, they have not yet told him to remove the video (I am NOT responsible for any loss of equipment should you try this), I am only including this link for interest sake.

     

  • Thanks for that clarification! I will know on Thursday what is installed and what is not.

     

    hli

  • My understanding is the base unit is 70Mhz; the upgrade is for 100Mhz. I have some email correspondence to the effect that they installed the upgrade before they sent the units to me. I didn't open them so I'll have to rely on the RoadTesters.

     

    When you start testing it, let me know if the license was not installed.

     

    Randall

     

  • I don't know off hand. I'll look into it this week.

     

    Randall