Raspberry Pi 2/3 Weather Sensor Shield

Table of contents

image

 

{tabbedtable} Tab LabelTab Content
About

The DPP904R000 from Sensor Solutions - TE Connectivity is a MEAS Pi weather shield. It provides necessary hardware to interface HTU21D digital relative humidity sensor, MS5637 digital barometric pressure sensor, TSYS-01 temperature system sensor, TSD305-1C55 digital thermopile sensor to any system that utilizes Raspberry Pi compatible expansion ports configurable for I²C communication.

image

 

The HTU21D is a self-contained humidity and temperature sensor that is fully calibrated during manufacturing and can operate from 1.5V to 3.6V has selectable resolution, low battery detection and checksum capability. The MS5637 is a self-contained pressure and temperature sensor that is fully calibrated during manufacturing and can operate from 1.5V to 3.6V. The temperature system sensor TSYS-01 series is a self-contained temperature sensor that is fully calibrated during manufacturing and can operate from 2.2V to 3.6V. The TSD305-1C55 is a contactless temperature measurement system in a TO5 package.

 

Features

  • 0% to 100% relative humidity range, -40°C to 125°C temperature (HTU21D sensor)
  • MS5637 measures pressure from 300mbar to 1200mbar, temperature from -40°C to 125°C
  • TSYS01 measures temperature from -40°C to 125°C, accuracy from 0.1°C to 0.5°C
  • Contactless temperature measurement from 0°C to 100°C (TSD305-1C55)
  • HTU21D, TSYS01 has a low power stand-by mode for power-sensitive applications
  • Dimension is 64.97322mm x 56.4134mm
Important Dates

Enrollment Begins: August 23 2017

Enrollment Ends: September 29 2017

RoadTesters Selected: Oct 6 2017 (estimated)

Product Shipped: Oct 18 2017

RoadTesting Begins: Oct 25 2017

Reminder/Update Email:Nov 25 2017

Submit Reviews By: Dec 26 2017**

 

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

The supplier chose the following as official RoadTesters:

 

Terms & Conditions

Raspberry Pi 2/3 Weather Sensor Shield– RoadTest

Terms and Conditions

These are the terms and conditions which govern theRaspberry Pi 2/3 Weather Sensor Shield RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

Raspberry Pi 2/3 Weather Sensor Shield

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Sept 29 2017

Announcement of Winner (estimated): Oct 6  2017

 

Prize: Raspberry Pi 2/3 Weather Sensor Shield

Additional Prizes: none

Competition Site: https://www.element14.com/community/groups/roadtest?ICID=menubar_resources_roadtest

Site or element14 Community: www.element14.com/community

Judges: members of the element14 community team chosen at the Organiser’s discretion.

Judging Criteria, All of the following which will have equal weighting:

· Demonstrated competence with the technologies including links or descriptions of past projects

· Qualifications as indicated by current job role and/or schooling/vocational training;

· A thorough description of how the prize would be tested;

· Likelihood that the Applicant will blog about the prize and provide a review on element14.com;

· Originality;

· Innovation.

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:

· Provide a RoadTest application describing what he/she would do if awarded the Prize including similar previous projects, product experience and qualifications

Terms: these terms and conditions which govern the Competition and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

  1. Eligibility
  2. Applications:
  3. Selecting Winners:   
  4. Liability:
  5. General:

1.1 Save as set out in these Terms, the Contest is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.2 All Applicants must be aged at least 18 at the time of their application.

1.3 Applicants must not enter the RoadTest if doing so or taking part may:

1.3.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.3.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.3.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in competitions such as these or receiving prizes under them and the Organiser respects those policies and practices.

The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly. 

1.4 Multiple applications are not permitted.

1.5 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.6 The Contest is NOT open to:

1.6.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.6.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser and Sponsors; or

2.1 Each Applicant must fully complete and submit a RoadTest Application by the Application Close.

2.2 By submitting a Registration Form, each Applicant:

2.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the RoadTest;

2.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

2.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

2.2.4 Authorises the Organiser to copy, reproduce and use the Application and/or Review for the purposes of the RoadTest and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

2.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Contest. As between the Applicant and the Organiser the IP remains owned by the Applicant.

2.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Contest or the promotion of it or the Site;

2.2.7 Agrees to participate positively in all publicity surrounding the Contest;

2.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Contest (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

2.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

2.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the RoadTest.

2.3 All applications submitted to this RoadTest must meet the following criteria:

2.3.1 Applicants must be the author, creator and owner of the proposed review idea. Applicants must not submit someone else’s idea;

2.3.2 The proposed application must be reasonably achievable by the within the time constraints of the Contest; 

2.3.3 Applications must not include or propose any of the following, the inclusion of which shall render any proposed application ineligible:

(a) Applications which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) Applications that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser;

(c) Applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

2.4 No Application may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

3.1 Winners will be selected by the Organiser on the basis of the quality of his or her application and its adherence to these Terms.

3.2 The total number of Winners selected will be at least the minimum number set out above but the actual number is at the sole discretion of the Organizer and/or the Sponsor, if applicable.

3.3 The Organiser will use all reasonable efforts to announce the Winners via an update to the RoadTest page by the date listed above.

3.4 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the RoadTest, the Products featured or other Contests with which the Organiser may be connected from time to time.

3.5 Details of the Winners may also be published in the media.

3.6 Winners are responsible for all applicable taxes, duties or other charges payable in relation to any prize.

3.7 

4.1 The Organiser hereby excludes all and any Liability arising out of the Contest or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

4.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

4.3 Subject to 4.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Competition or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Competition, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned. 

5.1 The RoadTest is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the RoadTest to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

5.2 The RoadTest may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a competition of this nature. The Organiser has the right to cancel or suspend the RoadTest at any time due to circumstances outside its reasonable control.

5.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the RoadTest or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

5.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the Contest Site and it is a condition of entry to the RoadTest that Applicants agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

5.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

5.6 These Terms and the operation of the Contest shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.

RoadTest Reviews
Comment List
Anonymous
  • My review will be submitted this evening. I have not been feeling well the past few days. I apologize for this delay.

  • OK I get it!

    Kas, look at the board,

    TSY and HTU have cutouts around, which make them relative easy to take off the "mainboard"

    but only temp. sensor is accompanied with relating holes convienient to solder wires or insert pins/ connector etc...

    Besides temperature measurement placed in the middle of the board  is most affected by "RPI heating station"

  • but why select the TSY over any other part ?

     

    Kas

  • Thank you

    After separation of TSY its readouts differ at last from the board temperature!

  • What was the reason? - mostly the dilemmas described in my post above (Nov 17)

    I think Gerrits charts and my results confirms the decision was correct.

    My readouts of the ambient are fine now.

    But maybe there is a little misunderstanding I didn't remove the sensor at all, I have it extended using the wires.

     

    BTW (TSY offtopic) the pressure is still lower than expected (...maybe this is the reason of my headacheimage)

  • The fact that the sensor board closely is connected to the raspberry pi certainly influences the temperature readout.

    As an example below the graph of the temperature readings of my raspberry pi based home automation system.

    Voeding is a sensor glued to the power supply, kast is a sensor inside the case of the system, binnen is my room temperature, measured with a sensor outside the case, buiten is the outside temperature and cpu is the cpu temperature.

    image

  • What prompted you to remove this part as opposed to the others on the board.

     

    Kas

  • Good news from my lab:

    Breaking out the TSY part from the board improved the reliability/ credibility of the readouts!

    Remark for other daredevils - beware when soldering, the paths are narrow, the best solution is to press tightly 4pin connector.

    Good luck!

  • I'm confused a little with the accuracy of sensors after comparison with other instruments.

    For sure, there is the influence of the board especially in readouts from additional temperature sensors from:

    HTU21D

    MS5637

    TSD305-1C55

    but TSYS0101 seems to be slightly separated from the board, thanks to "cutting-ready" solution (in the meaning of the heat transmission, convection can be neglected and in my opinion, the radiation also)

    Why has it shown around 30C from the beginning of my tests (around 10 days).

    The ambient temp is below 22!

    Remaining (additional) t. sensors give more than 32C - I treat it as the relative board temperature. And frankly, these three, quite similar measures - look quite reliable... (<1%error)

    Another doubt relates to the pressure, it's around 10hPa lower than measured with another equipment. I agree there is also only 1% but... we expect something better in case of industrial equipment... (max ∓4% according to papers)

    Is it possible that the quality of readouts is so miserable.

     

    Regarding the mentioned above cuttings around the TSY sensor, I think, I grown-up to break-out this part, separate it from the board and generally minimalize the influence of RPI thermodynamics...

    Did anybody dare that movement before?

  • I would have liked a small box, nothing fancy but when I'm done using kits I like to beable to put them away easily in a recognizable box for easy reuse later. If there is only an ESD bag its much harder and will find its way into a basket with other like boards making it harder to find.

     

    Kas