Sub-1 GHz Sensor to Cloud IoT Gateway

Table of contents

image

IoT Technology: Get Connected with SimpleLink Sub-1 GHz Sensor to Cloud solution

 

This TI Design provides a reference for creating an industrial IoT gateway that is capable of connecting a network of wireless sensors to an enterprise cloud provider. In this reference design, a long-range, low-power wireless network, made up of Sub-1 GHz CC1310 or CC1350 devices (both are supported) that run the TI 15.4-Stack-based application, is connected to the AWS IoT cloud. In addition, an online dashboard is provided that allows the user to visualize the real-time sensor data as well as send actuation commands from anywhere in the world using an Internet-connected device with a web browser.

 

Main Features

  • Large network to cloud connectivity enabling long range, up to 1 km line of sight (LOS)
  • IEEE 802.15.4e/g standards based Sub-1 GHz solution with the TI 15.4-stack SDK
  • Based on proven hardware designs enabling quick time to market with out-of-the-box ready to use demonstration software
  • TI Processor SDK for Linux provides scalability across multiple Sitara processors such as AM437x and AM57x

-image

 

Sitara AM335x device on the BeagleBone Black

The connection between the wireless sensor network and the cloud is made possible by TI’s Sitara AM335x device on the BeagleBone Black development platform. On one side, the AM335x is connected to a Sub-1 GHz device acting as the central node in the wireless network, and on the other side, the device is connected to the AWS IoT cloud using Ethernet. These two connections allow the AM335x device to act as a gateway to get the sensor messages from the wireless network to the cloud and, also, to get the actuation requests from the cloud dashboard sent back to the wireless network.

 

Due to the long-range and low-power capabilities of the Sub-1 GHz sensors, this TI Design is useful for any type of application that would benefit from distributed sensing. This reference design provides a blueprint that gives the ability to visualize or actuate tens or hundreds of sensors while only needing one gateway device, TI’s Sitara AM335x, to be connected to the Internet.

 

Contents

This reference design provides a list of required hardware, schematics, and foundational software to quickly begin your Internet of things (IoT) product development. Amazon Web Services (AWS) IoT service, which is brokered by stackArmor, was chosen as the cloud service provider for the demonstration. The software design, however, is architected to be flexible to enable other cloud service providers.

 

Applications

This TI Design enables IoT in numerous applications, such as building security gateways, door and window sensor networks, asset management and tracking, and other IoT-enabled home and industrial automation applications.

 

 

{tabbedtable} Tab LabelTab Content
Important Dates

Enrollment Begins: Sept 28 2017

Enrollment Ends: Oct 30 2017

RoadTesters Selected: Nov 20 2017

Product Shipped: Nov 21 2017

RoadTesting Begins: Nov 28 2017

Reminder/Update Email: Dec 28 2017

Submit Reviews By: Jan 29 2018

 

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

RoadTesters

The following applicants have been selected as official roadtesters:

 

Terms & Conditions

 

Sub-1 GHz Sensor to Cloud Industrial IoT Gateway– RoadTest

Terms and Conditions

These are the terms and conditions which govern the Sub-1 GHz Sensor to Cloud Industrial IoT Gateway contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment/component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 60 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition:

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

 

Sub-1 GHz Sensor to Cloud Industrial IoT Gateway

(RoadTest or Contest)

Key dates:

Applications Close: midnight (GMT) on Oct 30 2017

Announcement of Winners (Official RoadTesters) (estimated): Nov 6 2017

Prize

 

Sub-1 GHz Sensor to Cloud Industrial IoT Gateway

 

Additional Prizes: none

Competition Site: https://www.element14.com/community/groups/roadtest?ICID=menubar_resources_roadtest

Site or element14 Community: www.element14.com/community

Judges: members of the element14 community team chosen at the Organiser’s discretion.

Judging Criteria, All of the following which will have equal weighting:

· Demonstrated competence with the technologies including links or descriptions of past projects

· Qualifications as indicated by current job role and/or schooling/vocational training;

· A thorough description of how the prize would be tested;

· Likelihood that the Applicant will blog about the prize and provide a review on element14.com;

· Originality;

· Innovation.

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:

· Provide a RoadTest application describing what he/she would do if awarded the Prize including similar previous projects, product experience and qualifications

Terms: these terms and conditions which govern the Competition and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

  1. Eligibility
  2. Applications:
  3. Selecting Winners: 
  4. Liability:
  5. General:

1.1 Save as set out in these Terms, the Contest is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.2 All Applicants must be aged at least 18 at the time of their application.

1.3 Applicants must not enter the RoadTest if doing so or taking part may:

1.3.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.3.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.3.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in competitions such as these or receiving prizes under them and the Organiser respects those policies and practices.

The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly.

1.4 Multiple applications are not permitted.

1.5 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.6 The Contest is NOT open to:

1.6.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.6.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser and Sponsors; or

2.1 Each Applicant must fully complete and submit a RoadTest Application by the Application Close.

2.2 By submitting a Registration Form, each Applicant:

2.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the RoadTest;

2.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

2.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

2.2.4 Authorises the Organiser to copy, reproduce and use the Application and/or Review for the purposes of the RoadTest and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

2.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Contest. As between the Applicant and the Organiser the IP remains owned by the Applicant.

2.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Contest or the promotion of it or the Site;

2.2.7 Agrees to participate positively in all publicity surrounding the Contest;

2.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Contest (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

2.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

2.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the RoadTest.

2.3 All applications submitted to this RoadTest must meet the following criteria:

2.3.1 Applicants must be the author, creator and owner of the proposed review idea. Applicants must not submit someone else’s idea;

2.3.2 The proposed application must be reasonably achievable by the within the time constraints of the Contest;

2.3.3 Applications must not include or propose any of the following, the inclusion of which shall render any proposed application ineligible:

(a) Applications which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) Applications that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser;

(c) Applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

2.4 No Application may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

3.1 Winners will be selected by the Organiser on the basis of the quality of his or her application and its adherence to these Terms.

3.2 The total number of Winners selected will be at least the minimum number set out above but the actual number is at the sole discretion of the Organizer and/or the Sponsor, if applicable.

3.3 The Organiser will use all reasonable efforts to announce the Winners via an update to the RoadTest page by the date listed above.

3.4 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the RoadTest, the Products featured or other Contests with which the Organiser may be connected from time to time.

3.5 Details of the Winners may also be published in the media.

3.6 Winners are responsible for all applicable taxes, duties or other charges payable in relation to any prize.

3.7

4.1 The Organiser hereby excludes all and any Liability arising out of the Contest or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

4.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

4.3 Subject to 4.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Competition or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Competition, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned.

5.1 The RoadTest is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the RoadTest to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

5.2 The RoadTest may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a competition of this nature. The Organiser has the right to cancel or suspend the RoadTest at any time due to circumstances outside its reasonable control.

5.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the RoadTest or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

5.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the Contest Site and it is a condition of entry to the RoadTest that Applicants agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

5.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

5.6 These Terms and the operation of the Contest shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.

More Information

Sub-1 GHz Sensor to Cloud Industrial IoT Gateway Reference Design

User Guide (Detailed)

AM335x Sitara™ Processors

Sample Application: Door & Window Sensor

stackArmor Backgrounder

RoadTest Reviews
Comment List
Anonymous
  • I procured  two of these kits and was able to successfully run the default application.Now I want to customize the application/create my own application that runs on the gateway to push data from sensors to SAP Cloud platform.I am not getting any information on how i can update the application that runs on gateway.A USB to serial cable comes with the kit but I am not sure where which pins will it fit to since there is no documentation around it.Please can anybody guide.

  • No problem Kas!

     

    I should have added that this was using the normal data rate of 50kbps, there is an even lower data rate of just 5kbps that promises longer range so I should think you'd definitely be ok using this underwater.

     

    A

  • ,

     

    Thank you very much, I appreciate all the effort you have gone to for me. From what you are measuring that's some serious attenuation but what's nice is even at -100 dBm you are still getting a solid signal. And with the frequency at 868 MHz this looks like a possible solution for short underwater hops.

     

    Kas

  • Hi Kas, the device has now been in the water!

     

    I hooked up the CC1350 Sensor board from the IoT kit with a sensors booster back and some breadboard to get 3xAA battery power into the device, wrapped it in two layers of self seal bags, then put it inside a clear plastic box, weighted it all down with a brick, and plunged it into some seriously cold water outside!

     

    It was at a depth of about 60cm, though the tank itself is only about that diameter so I reckon there was only about 30cm of water all around. On top of that, though, is the distance back to the base station of BeagleBone and the other CC1350 board, which is easily 10m, and back inside as well, so there was a fair degree of attenuation there too.

     

    The screenshot below shows we got an RSSI of -100dBm from in the water, when I pulled it back out again that went up to about -76dBm. This is on the EU 868MHz frequency, but I don't really expect that will make a difference.

     

    image

     

    I'll add more details into my RoadTest report, and I'll give some more thought to how we could collect you some better data too. I guess taking the system out on a road trip to a marina or harbour would be the next step, what sort of depth are you looking for in your application?

     

    A

  • A meter would be a great start, my only question is what type of out of water linking is there. By this I mean how much of the signal is going through the water and how much is going water->air->Water. I really appreciate you looking into this for me.

     

    Kas

  • Hi Kas, the next step for me is to battery power this, so I'll then seal it up in a box and give it a try underwater!

     

    What sort of depth were you looking for? I could probably manage a metre relatively easily.

     

    A

  • Congrats to the winners, I'm looking forward to their reviews. Would be interested in possible underwater usage of these radios or from above to underwater and what range you get in each case..

     

    Kas

  • Update on Important Dates

     

    Enrollment Begins: Sept 28 2017

    Enrollment Ends: Oct 30 2017

    RoadTesters Selected: Nov 20 2017

    Product Shipped: Nov 21 2017

    RoadTesting Begins: Nov 28 2017

    Reminder/Update Email: Dec 28 2017

    Submit Reviews By: Jan 29 2018

     

    *The element14 RoadTest Staff will send this reminder/update email.

    **If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Lead, , as soon as possible before the deadline.

     

  • The following applicants have been selected as official roadtesters:

     

  • The closing date for this keeps getting bumped back - first 30 Oct, then 6 Nov, now 8 Nov. Is there a problem? Maybe hoping for better entries?