RoadTest: Anaren AIR B-Smart BoosterPack
Author: gsgill112
Creation date:
Evaluation Type: Evaluation Boards
Did you receive all parts the manufacturer stated would be included in the package?: True
What other parts do you consider comparable to this product?: Bluegiga's BLE112/113 BLE Module
What were the biggest problems encountered?: No Android Support
Detailed Review:
Road Test Review:
First of all, I want to thank Anaren, Element14 and RoadTest Program for providing me an opportunity for RoadTesting this product. Unfortunately, I own an Android Mobile so I won’t be able to test the application side of the product. I will be uploading application point of view once Anaren releases Android applications.
This review will be a Q/A kind of a review where I will answer all the key points Anaren wants as a part of review, and I will also post my findings. Finally I will be comparing this with other BLE Module I have been using.
1. What did you think of the kit when it first arrived, even before you opened the box?
I had been through many documentations (Anaren has a really Good Documentation set), about the kit and I knew what I was about to get. I was very fascinated by the kit as it is a really promising kit, featuring,
A2542R24A BLE 4.0 Module with CC2541 SoC
Voltage Regulator on Module
Pre-certification to FCC/IC and ETSI compliant
Low Power Consumption
The best feature I liked about the module is that this module had an on Module Regulator which is really awesome. Why? Because as per TI with the correct Regulator you can get up to 30% power performance improvement
that’s awesome

2. On opening the box, what struck you first about the layout of its contents and the overall component packaging?
Well, let me assure you Anaren has taken that extra step for you to give you great aesthetics satisfaction. Everything in the box has its own compartment and is elegantly and neatly packed. I just had one of those Awwwweeee… Moments while unboxing this kit. Well, where they have taken extra care of even boxing the – connector, I was disappointed by the quality of USB cable provided with the kit
. Even a 9.9$ Ti’s MSP430 Launchpad has a better Quality of USB B cable. But, anyways the provided cable worked so its fine
.
A neat feature of the box is space for an MSP430
. This board can be used as a stand-alone system with MSP430 and AIR Module by soldering few components at place and Bingo
. So they have provided a neat small space for an Extra MCU if ever you need one
.
3. On unpacking the box and looking at all the parts, what did you feel we could have added to the kit, or even excluded from the kit, for that matter?
AS mentioned above, the Quality of USB cable according to me was not up to mark, so, definitely some improvement at that department. There’s no need for a special packing for the connector cable. Though it seems cool, but is unnecessary.
AS this is a Development Board, I really would have liked a USB Module which can connect to the kit and you can debug the Gatt Profiles, etc. (Currently I do not own an iPhone so I am not able to test anything
)
4. Were you successful in connecting the kit to your embedded application?
Well, YES and NO. While running the demo code which compiled successfully, there was no way for me to check whether the code was running fine or not. Further there is no other way to check the transmission and test the BLE side as there aren’t any tools like CC2540DK/BLE4.0 Dongle/etc. currently shipped with the board.
5. Were you successful in connecting your kit/embedded application to the Em-hub using the tools and instructions included with the kit?
Anaren and Emmoco has done a really good job with documentation of the kit and steps for setting up the simple demo. The learning experience is really seamless as everything you need is right there at the em-hub portal or the em-Builder IDE.
An important point I want to mention here is the toolchain setup, usually companied have a long tiring setup methods for even the most simple work and that’s really painful to go through. In this case the em-Builder IDE is really the savior of the day. I was able to set up the entire toolchain with the most easy to install software within 30min, and was able to sit for a couple of ours and got the basic programs up and running. Too bad I couldn’t see the output on the mobile front instead I had to settle with Ti’s BLE device Monitor (Download Link) in conjunction with TI’s CC2540 DK usb dongle found here.
Finally, I realized that there’s a BLE Device monitor (Few other BLE Apps are also available here) which works Ok with any BLE4.0+ compatible mobile, but is extremely unreliable. I was able to see the entire GATT profile on my Mobile but the App crashed as soon as I tried changing some parameters inside GATT.
6. How was your experience with the Em-hub itself?
Em-Hub is a really cool experience with all the information required available there, but it does have some serious Glitches.
7. Did the kit live up to, exceed, or fall short of your expectations?
Yes, it did. This is easy to use and interface and really does the job. It has an on board Voltage Regulator, so approx. no External components for the Module.
8. Would you recommend this kit to your customers and colleagues?
Well, the answer depends. I would prefer/recommend this module, if
Now, Lets Compair this with the BLE Module I am using 
I am Using a BLE 4.0 Module (based on ti's CC2541) from BlueGiga Tech, called BLE-113. I was using BLE112 earlier which was based on CC2540. The Anaren AIR A2542R24A Module is also based on CC2541 chipset. I have tabulated all my findings below.
| BLUEGIGA BLE113 | Anaren AIR A2542R24A |
|---|---|
| Based on Ti's CC2541 SoC | Based on Ti's CC2541 SoC |
| Only the SoC and Antenna on Module | Comes with Voltage Regulater giving better performance |
| Needs Ti's CC Debugger to work with | Can be programmed using the Launchpad/Serial Prog. |
| Smaller in size | quite Larger as compared to BLE113 |
Runs Bluegiga's Stack (Stack is Heavy Adds 2Bytes to Header Dec the payload ) | Runs Emmoco's Stack (Based on Ti's BLE Stack) |
| Extreamly Easy to use (It is as simple as Arduino) | Difficult to use as compared to BLE113 but Extremely easy to set up the prog. env. |
Documentation is not up to the mark and the example programs aren't so helpful | Extremely well written Documentation and plethora of examples to start with |
| No Learning Video's or tutorials are available | Learning tutorials provided |
The A2542R24A module is really interesting and I will switch (in near future) to this module from BLE because of it's awesome support and tutorials. Though, I already have wasted an enormous amount of time on the BLE Module to learn those, so will stick to them for now.
Which one to choose?
Well that depends on application. For my application I have to transmit Medical Data over BLE so I would suggest the Anaren's Module. But, if Size is the main concern then go with the Bluegiga's BLE Module as they are crazy Smaller. Recently Ti Announced a BlE 4.1 IC with antenna embedded inside. I will try and get my hands on them to evaluate their performance, but meanwhile will stick to these
Some Advantages and disadvantages of the BoosterPack:
Adv
Can be used as a stand alone Board
Configuration switches for easy use
Emmoco BLE Stack is lighter than others 
Dis-Adv
Jumper's are not Standard 0.1" spacing instead they are 2mm