RoadTest: Enroll to Review the Arduino GIGA R1 WiFi + Camera
Author: crisdeodates
Creation date:
Evaluation Type: Development Boards & Tools
Did you receive all parts the manufacturer stated would be included in the package?: True
What other parts do you consider comparable to this product?: Portenta H7, Arduino Mega / Due
What were the biggest problems encountered?: Availability of onboard off-the-shelf ports such as grove ports could have been better (solvable using shields)
Detailed Review:
First of all, I would like to thank rscasny, the roadtest program team, and element14 for giving me this awesome chance to roadtest this amazing product Arduino Giga R1 Wifi board. Element14 was kind enough to send me a piece for road testing. I have been playing with Arduino boards ever since I started my robotics path. In fact, my first major project from college was using an Arduino Nano, dating back to the early beginning of the previous decade. So Arduino is not new to me and this beast of a thing is absolutely monstrous. Seriously? 76 GPIOs? Even Mega and Due had only 54 of them. When this board was available for the road test, I was determined to try this, not just for the kind of monster it is in the embedded space, but also to explore the endless possibilities it can provide in terms of scaling and productivity in the maker space. More interestingly, I was intrigued by the following statement from the official page: “You can for example run MicroPython and Arduino code simultaneously and communicate via an RPC”
Let's have a look at the kit and its components:

The box came with the following components:
(Yes, Randall was kind enough to include a camera module for the road testers)
The Arduino board in its “Giga” form really made an excellent first impression. The board was massive to hold at 101.6mm x 53.3mm (just like its older cousins Mega and Due), even dwarfing the Raspberry Pi 4 board's 56.5mm x 85.6mm footprint.

By default, the Arduino Giga board seems to come with a multicolor LED blink arduino program that seems to cycle between the Red, Green, and Blue colors of the inbuilt RGB LED that is present next to the audio jack.
There are basically 3 boards that could potentially be compared to Arduino Giga R1 Wifi.
Arduino GIGA R1 WiFi board basically inherits the STM32H7 dual-core Cortex-M7/M4 microcontroller of Portenta H7 boards while maintaining the larger Arduino Mega/Due form factor.
Performance in comparison to Portenta H7:
Arduino GIGA R1 WiFi board could be expected to have the same high computing capacity as Portenta H7 boards since they share the same STM32H7 microcontroller.
However, in contrast to the Portenta H7, the Giga board comes with 76 GPIO, an audio jack, a USB 2.0 Type-A host port, and extra connectors for a display and a camera. At the same time, the Giga board has no support for DisplayPort over USB-C, no on-board 10/100M Ethernet PHY, no high-density connectors, and no built-in battery support which are present in the Portenta H7 board.
Both boards feature a USB Type-C port for programming, integrating 2 MB of flash memory, 1 MB of RAM, 16 MB QSPI Flash memory, and 8 MB of SDRAM. Additionally, both boards have a Murata module for wireless connectivity (Wi-Fi and Bluetooth Low Energy BLE). Both boards can be programmed with the Arduino IDE or MicroPython. The dual-core design allows two programs to be run simultaneously with either both cores running Arduino code or one core running an Arduino sketch and the other a MicroPython script. An additional advantage of dual-core design as stated by the Arduino team is that, with this architecture, we can separate higher-level logic such as displays, interfaces, and networking from time-critical tasks such as motor control.
Features in comparison to Arduino Mega / Due:
At first look, the Giga board resembles the look of the Mega / Due form factor, although the Mega and Due can never match Giga in terms of performance.

Image courtesy: MakerHero
The key difference is that Giga boasts a whooping 76 GPIO in contrast to the 54 GPIO in Mega / due boards. Also, Giga additionally has wireless connectivity, an audio jack, a USB 2.0 Type-A host port, a JTAG connector, and extra connectors for a display and a camera. The Giga also comes equipped with a crypto chip and an antenna. Within the generous 76 GPIO pins, 12 support PWM, 12 with analog input & 2 DACs. There are 4 UART, 3 I2C, and 2 SPI buses, plus CAN bus support (requires external transceiver). The Giga board also includes two new pins in contrast to Mega / Due. They are a VRTC pin to keep the real-time clock running when the main power is removed and an OFF pin that shuts down the board. Giga board can be powered with inputs varying from 6-24V DC while the other two only support up to a maximum of 12V. Even though all the existing shields seem compatible, Giga is a 3.3-volt logic device. Hence most of the existing shields might not work if they operate at the 5V levels. Since the microcontroller operates on a voltage of 3.3V, applying a higher voltage than that, such as 5V, to a pin might damage the microcontroller.
Here are some links to get started:
Let's have a look at the datasheet and some specifications of the Arduino Giga R1 Wifi board.
The Arduino GIGA R1 is one of the most feature-packed Arduino boards to date. It is supported by the same powerful, ML-capable, dual-core microcontroller found in the Arduino Pro family's Portenta H7.

Image Courtesy: DroneBotWorkshop
More detailed top view:

Image Courtesy: Arduino
More detailed bottom view:

Image Courtesy: Arduino
The reference ICs are:
|
Ref. |
Description |
Ref. |
Description |
|
U1 |
STM32H7 Dual Core Microcontroller IC |
U8 |
AT25SF128A-MHB-T 16 MB Flash IC |
|
U3 |
AS4C4M16SA 8MB SDRAM IC |
U4 |
ATECC608A-MAHDA-T Secure Element IC |
|
U5 |
LBEE5KL1DX-883 Wi-Fi®/Bluetooth® Module |
U6 |
MP2322GQH Buck Converter 3.3V IC |
|
U7 |
MP2269GD-Z Buck Converter 5V IC |
JANALOG |
Analog input/output headers |
|
JDIGITAL |
Digital input/output headers |
JSIDE |
Digital input/output headers |
|
SPI |
SPI headers |
JTAG |
JTAG Headers |
|
J2 |
USB 2.0 A Host |
J15 |
3.5 mm audio in/out |
|
PB1 |
RESET Button |
PB2 |
BOOT0 button |
|
J14 |
Micro UFL connector |
J5 |
Camera |
|
J6 |
Camera |
DL1 |
Power LED |
|
DL2 |
RGB SMLP34RGB2W3 Common anode LED |
J12 |
CX90B-16P USB-C® connector |
Here are the main technical specifications.
The pinout of the Arduino Giga R1 Wifi board is as follows.

Image Courtesy: Arduino
|
Pin |
Function |
Type |
Description |
|
Three-Pins Header – J1 |
|||
|
1 |
OFF |
Digital |
3V3 Enable Pin (U6) |
|
2 |
GND |
Power |
Ground |
|
3 |
VRTC |
Reset |
Real-Time Clock Battery |
|
Analog |
|||
|
1 |
NC |
NC |
Not Connected |
|
2 |
IOREF |
IOREF |
Reference for digital logic V - connected to 3.3V |
|
3 |
Reset |
Reset |
Reset |
|
4 |
+3V3 |
Power |
+3V3 Power Rail |
|
5 |
+5V |
Power |
+5V Power Rail |
|
6 |
GND |
Power |
Ground |
|
7 |
GND |
Power |
Ground |
|
8 |
VIN |
Power |
Voltage Input |
|
9 |
A0 |
Analog |
Analog input 0 /GPIO |
|
10 |
A1 |
Analog |
Analog input 1 /GPIO |
|
11 |
A2 |
Analog |
Analog input 2 /GPIO |
|
12 |
A3 |
Analog |
Analog input 3 /GPIO |
|
13 |
A4 |
Analog |
Analog input 4 /GPIO |
|
14 |
A5 |
Analog |
Analog input 5 /GPIO |
|
15 |
A6 |
Analog |
Analog input 6 /GPIO |
|
16 |
A7 |
Analog |
Analog input 7 /GPIO |
|
17 |
A8 |
Analog |
Analog input 8 /GPIO |
|
18 |
A9 |
Analog |
Analog input 9 /GPIO |
|
19 |
A10 |
Analog |
Analog input 10 /GPIO |
|
20 |
A11 |
Analog |
Analog input 11 /GPIO |
|
21 |
DAC0 |
Analog |
Digital to Analog Converter 0 |
|
22 |
DAC1 |
Analog |
Digital to Analog Converter 1 |
|
23 |
CANRX |
Digital |
CAN Bus Receive |
|
24 |
CANTX |
Digital |
CAN Bus Transfer |
|
Digital |
|||
|
1 |
D21/SCL1 |
Digital |
GPIO 21/I2C 1 Clock |
|
2 |
D20/SDA1 |
Digital |
GPIO 20/I2C 1 Dataline |
|
3 |
AREF |
Digital |
Analog Reference Voltage |
|
4 |
GND |
Power |
Ground |
|
5 |
D13/SCK |
Digital |
GPIO 13/SPI Clock (PWM~) |
|
6 |
D12/CIPO |
Digital |
GPIO 12/SPI Controller In Peripheral Out (PWM~) |
|
7 |
D11/COPI |
Digital |
GPIO 11/SPI Controller Out Peripheral In (PWM~) |
|
8 |
D10/CS |
Digital |
GPIO 10/SPI Chip Select (PWM~) |
|
9 |
D9/SDA2 |
Digital |
GPIO 9/I2C 2 Dataline (PWM~) |
|
10 |
D8/SCL2 |
Digital |
GPIO 8/I2C 2 Clockline (PWM~) |
|
11 |
D7 |
Digital |
GPIO 7 (PWM~) |
|
12 |
D6 |
Digital |
GPIO 6 (PWM~) |
|
13 |
D5 |
Digital |
GPIO 5 (PWM~) |
|
14 |
D4 |
Digital |
GPIO 4 (PWM~) |
|
15 |
D3 |
Digital |
GPIO 3 (PWM~) |
|
16 |
D2 |
Digital |
GPIO 2 (PWM~) |
|
17 |
D1/TX0 |
Digital |
GPIO 1 / Serial 0 Transmitter |
|
18 |
D0/TX0 |
Digital |
GPIO 0 / Serial 0 Receiver |
|
19 |
D14/TX3 |
Digital |
GPIO 14 / Serial 3 Transmitter |
|
20 |
D15/RX3 |
Digital |
GPIO 15 / Serial 3 Receiver |
|
21 |
D16/TX2 |
Digital |
GPIO 16 / Serial 2 Transmitter |
|
22 |
D17/RX2 |
Digital |
GPIO 17 / Serial 2 Receiver |
|
23 |
D18/TX1 |
Digital |
GPIO 18 / Serial 1 Transmitter |
|
24 |
D19/RX1 |
Digital |
GPIO 19 / Serial 1 Receiver |
|
25 |
D20/SDA |
Digital |
GPIO 20 / I2C 0 Dataline |
|
26 |
D21/SCL |
Digital |
GPIO 21 / I2C 0 Clock |
|
STM32 ICSP |
|||
|
1 |
CIPO |
Internal |
Controller In Peripheral Out |
|
2 |
+5V |
Internal |
Power Supply of 5V |
|
3 |
SCK |
Internal |
Serial Clock |
|
4 |
COPI |
Internal |
Controller Out Peripheral In |
|
5 |
RESET |
Internal |
Reset |
|
6 |
GND |
Internal |
Ground |
|
Digital Pins D22 - D53 LHS |
|||
|
1 |
+5V |
Power |
+5V Power Rail |
|
2 |
D22 |
Digital |
GPIO 22 |
|
3 |
D24 |
Digital |
GPIO 24 |
|
4 |
D26 |
Digital |
GPIO 26 |
|
5 |
D28 |
Digital |
GPIO 28 |
|
6 |
D30 |
Digital |
GPIO 30 |
|
7 |
D32 |
Digital |
GPIO 32 |
|
8 |
D34 |
Digital |
GPIO 34 |
|
9 |
D36 |
Digital |
GPIO 36 |
|
10 |
D38 |
Digital |
GPIO 38 |
|
11 |
D40 |
Digital |
GPIO 40 |
|
12 |
D42 |
Digital |
GPIO 42 |
|
13 |
D44 |
Digital |
GPIO 44 |
|
14 |
D46 |
Digital |
GPIO 46 |
|
15 |
D48 |
Digital |
GPIO 48 |
|
16 |
D50 |
Digital |
GPIO 50 |
|
17 |
D52 |
Digital |
GPIO 52 |
|
18 |
GND |
Power |
Ground |
|
Digital Pins D22 - D53 RHS |
|||
|
1 |
+5V |
Power |
+5V Power Rail |
|
2 |
D23 |
Digital |
GPIO 23 |
|
3 |
D25 |
Digital |
GPIO 25 |
|
4 |
D27 |
Digital |
GPIO 27 |
|
5 |
D29 |
Digital |
GPIO 29 |
|
6 |
D31 |
Digital |
GPIO 31 |
|
7 |
D33 |
Digital |
GPIO 33 |
|
8 |
D35 |
Digital |
GPIO 35 |
|
9 |
D37 |
Digital |
GPIO 37 |
|
10 |
D39 |
Digital |
GPIO 39 |
|
11 |
D41 |
Digital |
GPIO 41 |
|
12 |
D43 |
Digital |
GPIO 43 |
|
13 |
D45 |
Digital |
GPIO 45 |
|
14 |
D47 |
Digital |
GPIO 47 |
|
15 |
D49 |
Digital |
GPIO 49 |
|
16 |
D51 |
Digital |
GPIO 51 |
|
17 |
D53 |
Digital |
GPIO 53 |
|
18 |
GND |
Power |
Ground |
Recommended Operating Conditions of Giga are:
|
Symbol |
Description |
Min |
Typ |
Max |
Unit |
|
VIN |
Input voltage from VIN pad |
6 |
7 |
32 |
V |
|
VUSB |
Input voltage from USB connector |
4.8 |
5 |
5.5 |
V |
|
VDD |
Input high-level voltage |
0.7*VDD |
VDD |
V |
|
|
VIL |
Input low-level voltage |
0 |
0.3*VDD |
V |
|
|
TOP |
Operating Temperature |
-40 |
25 |
85 |
°C |
Note: VDD controls the logic level and is connected to the 3.3V power rail and VAREF is for the analog logic
Here is the functional block diagram:

Image Courtesy: Arduino
The power distribution is below:

Image Courtesy: Arduino
Let us also look at the Arducam module and its datasheet.
The camera is based on an OmniVision 0.3MP OV7675 image sensor. It excels in image capture with its advanced features and exceptional performance and supports RAW/RGB/YUV output format. It is fully compatible with Arduino GIGA R1 board allowing versatile image capture and processing capabilities.
The pinout of the Arducam module is shown below.

Image Courtesy: ArduCam
Now, let’s get down to business and start tinkering with our new Arduino Giga R1 Wifi board. The initial setup with MbedOS is pretty straightforward like any other Arduino board.

Now let us try an example blink sketch

INFO: Normally, if the sketch fails for some reason, the board resets. On the GIGA R1, whenever the MbedOS fails, the board does not reset automatically. Instead, if it fails, the onboard red LED will start to blink in a looping pattern of 4 fast blinks and 4 slow blinks. Hence the red LED does NOT mean your board is broken or bricked. Instead, you can either press the reset button once to reset the sketch or double-tap the reset button to enter bootloader mode which allows you to re-program the board.
Here we will test the various features and capabilities of the Arduino Giga R1 Wifi board, along with the interfacing of various sensors and actuators.
Let's connect a bush button to Digital pin 7 of the GigaR1 and read its value.
In the Arduino IDE, go to File -> Examples -> Basics -> DigitalReadSerial
Change the variable pushButton to 7 for Digital Pin number 7 in GigaR1.
Compile and upload the sketch.
Connect a push button to the Digital Pin 7 of the GigaR1.
I used a DFRobot Gravity Push button: https://www.dfrobot.com/product-2362.html
Connect the power pins of the pushbutton to 3.3v and the GND pins of the GigaR1.

Observe the state of Digital Pin 7 in the serial monitor output.

Reference: https://docs.arduino.cc/tutorials/giga-r1-wifi/cheat-sheet#wi-fi
Let's see how the Wifi could be set up in GigaR1.
In the Arduino IDE, go to File -> Examples -> Wifi -> WifiWebClient
Change the SSID and password in the arduino_secrets.h file
Change the server variable name to google.com in WifiWebClient.ino file
Compile and Upload the program

We can see that the Giga R1 successfully connected to our local Wifi and was able to access the Google server webpage.
Connecting to Arduino Cloud:

Reference: https://docs.arduino.cc/tutorials/giga-r1-wifi/giga-usb
Generic USB keyboards could be easily connected to the GIGA R1's USB-A connector without any additional circuitry. However, we need the USBHostGiga library.
Note: To enable the USB-A port, you will need to define it as an output (PA_15). We can also disable it inside of a sketch by writing a LOW state to it.
#include "USBHostGiga.h"
Keyboard keyb;
HostSerial ser;
void setup() {
Serial.begin(115200);
while (!Serial);
pinMode(PA_15, OUTPUT);
keyb.begin();
ser.begin();
}
void loop() {
if (keyb.available()) {
auto _key = keyb.read();
Serial.println(keyb.getAscii(_key));
}
while (ser.available()) {
auto _char = ser.read();
Serial.write(_char);
}
//delay(1);
}
Once the code is uploaded, connect your USB keyboard to the USB-A port of GigaR1.

Open the serial monitor and start pressing the keyboard keys.
The keys pressed will be displayed on the serial monitor.

GIGA R1 board can also be transformed or emulated into a Human Interface Device (HID), e.g. mouse & keyboard, game controller, etc.
Let's try to emulate a keyboard.
In the Arduino IDE, go to File -> Examples -> USBHID -> Keyboard
Open a notepad after the code is uploaded

We can see that the GigaR1 now emulates a keyboard and prints the text “Hello World” as if typed from a keyboard device.
CAUTION: The keyboard continues to print as soon as the code is uploaded as it is inside the loop. Hence make sure you are bringing up a notepad or another textual area as soon as the code upload is finished or the board is reset.
CAUTION: Once the GigaR1 is configured as an HID, it will fail to upload any more sketches. In that case, double press the RST button (to the right of the USB-C port) to enter bootloader mode. You will be able to upload new sketches now.
Reference: https://reference.arduino.cc/reference/en/libraries/arduino_usbhostmbed5/
Let's try to read the contents of a USB drive connected to the USB-A port of the GigaR1.
Go to the Library Manager and install the Arduino_USBHostMbed5 library
Compile and upload the below code:
#include <DigitalOut.h>
#include <FATFileSystem.h>
#include <Arduino_USBHostMbed5.h>
USBHostMSD msd;
mbed::FATFileSystem usb("usb");
void setup()
{
Serial.begin(115200);
pinMode(PA_15, OUTPUT); //enable the USB-A port
digitalWrite(PA_15, HIGH);
while (!Serial)
;
Serial.println("Starting USB Dir List example...");
// if you are using a Max Carrier uncomment the following line
// start_hub();
while (!msd.connect()) {
//while (!port.connected()) {
delay(1000);
}
Serial.print("Mounting USB device... ");
int err = usb.mount(&msd);
if (err) {
Serial.print("Error mounting USB device ");
Serial.println(err);
while (1);
}
Serial.println("done.");
char buf[256];
// Display the root directory
Serial.print("Opening the root directory... ");
DIR* d = opendir("/usb/");
Serial.println(!d ? "Fail :(" : "Done");
if (!d) {
snprintf(buf, sizeof(buf), "error: %s (%d)\r\n", strerror(errno), -errno);
Serial.print(buf);
}
Serial.println("done.");
Serial.println("Root directory:");
unsigned int count { 0 };
while (true) {
struct dirent* e = readdir(d);
if (!e) {
break;
}
count++;
snprintf(buf, sizeof(buf), " %s\r\n", e->d_name);
Serial.print(buf);
}
Serial.print(count);
Serial.println(" files found!");
snprintf(buf, sizeof(buf), "Closing the root directory... ");
Serial.print(buf);
fflush(stdout);
err = closedir(d);
snprintf(buf, sizeof(buf), "%s\r\n", (err < 0 ? "Fail :(" : "OK"));
Serial.print(buf);
if (err < 0) {
snprintf(buf, sizeof(buf), "error: %s (%d)\r\n", strerror(errno), -errno);
Serial.print(buf);
}
}
void loop()
{
}
Now connect a FAT-formatted USB pen drive to the USB-A port of the GigaR1.

Please note that the name of the USB drive should be “usb”.
You should be able to see the drive contents in your serial monitor output.
Note: For some strange reason, my pendrive was not mounted. I will try later with another pen drive.

Reference: https://docs.arduino.cc/tutorials/giga-r1-wifi/giga-camera
The GIGA R1 has a dedicated camera connector that allows us to mount certain camera modules directly on the board. This will enable the possibility to use machine vision in our GigaR1 projects.
The GIGA R1 currently supports the following cameras, via the Camera library that is bundled with the Arduino Mbed Core:
We can access the Camera Library here: https://github.com/arduino/ArduinoCore-mbed/tree/master/libraries/Camera
The 20-pin camera connector onboard the GIGA R1 is designed to be directly compatible with some breakout boards from ArduCam. This allows us to simply connect the camera module directly to the board, without making any additional circuit.

Image Courtesy: Arduino
Let's try to access the camera module using GigaR1.
We will need to install the software called Processing in order to read the serial camera buffer data sent from GigaR1.
Step 1: Configure Arduino to send camera data via Serial
Connect the camera module to the 20-pin camera connector.
In the Arduino IDE, go to File -> Examples > Camera > CameraCaptureRawBytes
Make sure the correct camera module is selected inside the code. Eg: OV7675
Compile and upload the sketch

Step 2: Configure Processing to read the camera data via Serial
Open the Processing app.
Copy the following code to the processing app:
import processing.serial.*;
import java.nio.ByteBuffer;
import java.nio.ByteOrder;
Serial myPort;
// must match resolution used in the Arduino sketch
final int cameraWidth = 320;
final int cameraHeight = 240;
// Must match the image mode in the Arduino sketch
final boolean useGrayScale = false;
// Must match the baud rate in the Arduino sketch
final int baudRate = 115200;
final int cameraBytesPerPixel = useGrayScale ? 1 : 2;
final int cameraPixelCount = cameraWidth * cameraHeight;
final int bytesPerFrame = cameraPixelCount * cameraBytesPerPixel;
final int timeout = int((bytesPerFrame / float(baudRate / 10)) * 1000 * 2); // Twice the transfer rate
PImage myImage;
byte[] frameBuffer = new byte[bytesPerFrame];
int lastUpdate = 0;
boolean shouldRedraw = false;
void setup() {
size(640, 480);
// If you have only ONE serial port active you may use this:
//myPort = new Serial(this, Serial.list()[0], baudRate); // if you have only ONE serial port active
// If you know the serial port name
//myPort = new Serial(this, "COM5", baudRate); // Windows
myPort = new Serial(this, "/dev/ttyACM0", baudRate); // Linux
//myPort = new Serial(this, "/dev/cu.usbmodem14301", baudRate); // Mac
// wait for a full frame of bytes
myPort.buffer(bytesPerFrame);
myImage = createImage(cameraWidth, cameraHeight, ALPHA);
// Let the Arduino sketch know we're ready to receive data
myPort.write(1);
}
void draw() {
// Time out after a few seconds and ask for new data
if(millis() - lastUpdate > timeout) {
println("Connection timed out.");
myPort.clear();
myPort.write(1);
}
if(shouldRedraw){
PImage img = myImage.copy();
img.resize(640, 480);
image(img, 0, 0);
shouldRedraw = false;
}
}
int[] convertRGB565ToRGB888(short pixelValue){
//RGB565
int r = (pixelValue >> (6+5)) & 0x01F;
int g = (pixelValue >> 5) & 0x03F;
int b = (pixelValue) & 0x01F;
//RGB888 - amplify
r <<= 3;
g <<= 2;
b <<= 3;
return new int[]{r,g,b};
}
void serialEvent(Serial myPort) {
lastUpdate = millis();
// read the received bytes
myPort.readBytes(frameBuffer);
// Access raw bytes via byte buffer
ByteBuffer bb = ByteBuffer.wrap(frameBuffer);
// Ensure proper endianness of the data for > 8 bit values.
// The 1 byte bb.get() function will always return the bytes in the correct order.
bb.order(ByteOrder.BIG_ENDIAN);
int i = 0;
while (bb.hasRemaining()) {
if(useGrayScale){
// read 8-bit pixel data
byte pixelValue = bb.get();
// set pixel color
myImage.pixels[i++] = color(Byte.toUnsignedInt(pixelValue));
} else {
// read 16-bit pixel data
int[] rgbValues = convertRGB565ToRGB888(bb.getShort());
// set pixel RGB color
myImage.pixels[i++] = color(rgbValues[0], rgbValues[1], rgbValues[2]);
}
}
myImage.updatePixels();
// Ensures that the new image data is drawn in the next draw loop
shouldRedraw = true;
// Let the Arduino sketch know we received all pixels
// and are ready for the next frame
myPort.write(1);
}
Make sure to select the correct serial port and baud rate in the code.
Press the Play button on the app to run the code.

We can see that the processing code will display the output of the serial data sent by the GigaR1 module.
CAUTION: If the serial port says busy in the processing app, make sure that the serial monitor is not open in the Arduino IDE.
The Arduino Giga R1 Wifi was a very fun and interesting board to work with. The readily available out-of-the-box Arduino example sketch will allow anyone to directly jump into using and tinkering with the kit, although the advanced features such as Dual core programming, multi-channel ADC, etc require some experience. MicroPython support also allows a robotics project to be realized with little to no effort. The availability of good documentation is also a plus as it allows in-depth programming and interfacing. The peripheral interfacings are also well set and we have access to a plethora of interfacing pins and options.
The major pros and cons of the kit are summarized below.
Future Prospects
I wish to do a bit more testing on the advanced capabilities such as Dual core programming, Multi-channel ADC, actuator interfacings, etc.