Baby Thermometer

View table of contents ...  

RoadTest: Review the ams OSRAM Digital Temperature Sensor Kit and Companion App AS6221-DK

Author: swathic

Creation date:

Evaluation Type: Semiconductors

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: STM Sensortile, Clinical Thermometer, IR thermometer

What were the biggest problems encountered?: The device is difficult to place and hold for continuous monitoring if not used with body strap or wrist strap.

Detailed Review:

Essential newborn care involves immediate care at the time of birth, and essential care during the entire newborn period. It is needed both in the health facility and at home.

Essential newborn care includes:

  • Thermal care
  • Breast milk feeding
  • Nurturing care
  • Infection prevention
  • Assessment of health problems
  • Recognition and response to danger signs

Thermal care is the one which is important for the infants to elders to timely monitor the temperature of the body. If anyone fall ill the first and foremost measurement undergone is temperature of body. Most babies have an average body temperature of about 36.5°C to 38°C. A fever is when your baby's body temperature rises above 38°C. Temperature measurement is done at different places for different aged people, the main important is to know the body temperature of the babies because they can easily infected if the body temperature is not well. 

Age Oral Rectal/Ear Armpit
0–12 months 95.8–99.3°F
(36.7–37.3°C)
96.8–100.3°F
(37–37.9°C)
94.8–98.3°F
(36.4–37.3°C)
Children 97.6–99.3°F
(36.4–37.4°C)
98.6–100.3°F
(37–37.9°C)
96.6–98.3°F
(35.9–36.83°C)
Adults 96–98°F
(35.6–36.7°C)
97–99°F
(36.1–37.2°C)
95–97°F
(35–36.1°C)
Adults over age 65 93–98.6°F
(33.9–37°C)

94–99.6°F
(34.4–37.6°C)
92–97.6°F
(33.3–36.4°C)

In market there are clinical digital thermometers but they can display real-time data value and cannot have storage & long time visualization. There is a need to have devices other than clinical thermometer or IR thermometer to monitor continuously and store the data for future analysis. Then here come the arm  OSRAM Digital temperature sensor kit and companion app Roadtest hardware to monitor the data continuously and connect about eight such devices to app and monitor data.

image

 Out-of-box video and measurement of data https://youtu.be/dQC4vz9SOjU   And important information on Digital temperature can follow in the video https://youtu.be/_i5MbkN921M 

Test

Baby temperature monitor is important because as we know baby is carried by mother in her lap to different locations along with her like to shopping malls, office, hospitals, etc need to travel in different modes of transport. During the travel baby is exposed to different environment which leads to change in body temperature. A regular monitoring will help to know the body temperature condition so that mother can take precocious care.

I have used the Roadtest kit to monitor the baby temperature by placing it on forehead and the device measure the temperature faster and data can visualize on the screen and real time data can record in Xls file.

imageimage

image 

The demo device show the baby temperature is fine at forehead this test will help to know the body temperature.

The test will help the mother to use the suitable carrier at different environment conditions like in winter and in summer. The arm OSRAM Digital temperature sensor kit with companion app is a suitable device to get instructions from pediatrics on the baby health on the temperature report. It also help in-advance to know the temperature of baby before carrying to hospital so that on time medicine can be given instead of waiting for temperature monitoring at hospital. The bath tube water temperature can also measure with the water resistance kit so that the baby health will not effect. There are many applications with the thermometer devices but the current roadtest will have extra benefits due to small size and connect to mobile app for data storage or visualization. Below figure shows how the temperature can be monitored with app in real-time when THREE devices connected.

 image

Figure shows three sensor read room temperature.

As the app can be connected to 8 different devices so multiple points data can be recorded. The test has performed with the help of pediatrics and suggest some recommendations.

Additional Inclusions to the Device

  1. If the device has Display like clinical thermometer on top it will help to check the real time value instead of continues monitoring on app.
  2. WiFi connectivity make to monitor remotely from long distance as Bluetooth range is limited.
  3. Beep sound when connection loss in mobile or on the device during operation. 
  4. Button for changing mode to display data in app or on-board.

Conclusion

The sensor kit has salient features to carry the temperature monitoring to any age people when it is needed. In some accident cases also it help as fist-aid device to know the body temperature of the patient before reaching to hospital which gives the information of the patient condition. It can be used as thermometer in first-aid box, ambulances, medical kit, body strap, etc. The device is easy to carry in pocket to monitor the body temperature and can connect to app for data visualization and record for a length of 1 hour 30 minutes. It also help for the animal, birds temperature monitoring can be used for the pet cares.

Anonymous