MultiComp MP011888 cordless GRINDER set review

View table of contents ...  

RoadTest: RoadTest Open Call

Author: robogary

Creation date:

Evaluation Type: Workshop Tools

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: dremel , workpro, hardell

What were the biggest problems encountered?: The grinder stalls fairly easy, but it protects itself against a prolonged stall . The USB requires a beefy cell phone charger (not provided) . It doesnt come with a carry bag, and the bit accessories are meager.

Detailed Review:

Road Test Preface: 

An essential tool in my workshop is a small high speed grinder. The grinder is often referred to as a Dremel tool, after the popular manufacturer’s name. 

When working on home projects, the grinder tool is particularly helpful when fiberglass PCB need cut, routed, drilled, corners rounded, etc. , 3D prints also need trimmed, routed, polished, drilled. Bolts and screws may need cut off. Plastic boxes need drilled, cut, routed, etc.

My corded corded grinder is great for big jobs, but for lighter detail work, the corded grinder tool is bulky, cord clumsy, and can overpower a delicate operation, burn plastic, etc .

A smaller cordless grinder could be really useful on my workbench or in my portable toolbox.

The Multicomp MP011888 cordless mini grinder could be a solution. It is cordless, light, uses all the same bits and cutting accessories as a bigger high speed grinder, and seems an appropriate output torque for workbench size projects.

Road Test Scoring and Evaluation:

Product performed to expecations: 4 of 5 stars  - I didnt expect alot of torque for a battery powered device.

It did OK for a 5V USB charged device, it does stall if pushed. The battery itself is 3.6V 

USB doesnt mean you can charge with your PCs USB port. You'll need a decent USB phone charger for this grinder. 

Alot of cordless grinders are 12V, which means they need a separate charger provided with them.  

The grinder body has a contoured comfortable feel and grip.

 

The price to performance ratio was good: 3 of 5 stars - meh , most 4 V grinders are half the list price.

Most grinder tool kits are more generous with the bit accessories in the kit.   

I had to provide my own see thru "grinder tool bag" to keep the grinder, cables, and bit accessories together.  

 

Road Test Details:

Performance Video: sorry it runs 23 minutes, but shows battery life and real time performance with 6 various materials. I wasn't that gentle either.

https://youtu.be/k4KWLYiF78Q

featuring: 

1) Cutting, shaping, drilling an ABS 1/8” black plastic sheet - not a challenge

2) Cutting a fiberglass PCB - great job 

3) Cutting a ¼ inch( 6.2 mm ) stainless steel bolt - very challenging

4) Cutting & Shaping a piece of 1/8 inch ( 3.26 mm ) thick lexan industrial plastic sheet - a challenge to cut, but as expected 

5) Cutting & Shaping a piece of 3/16 inch ( 9.7 mm ) thick plywood - the grinder does fairly well 

6) Cutting 1/16 inch ( 3.26 mm ) steel washer - thick steel washer wins round 1 

----- battery died ---

Retry the steel washer cut after a full recharge - grinder does better, but the steel washer is still a mighty challenge

Opening the box: 

image

image

image

image

image

image

image

 

Out of box experience

√ Operation disabled while charging – good

√ Battery indicator – green, yellow, red  LEDs. displays only while in operation – good

√ Battery indicator – red when charging,

√- green LED lit when fully charged , took 2-3 hours from a dead battery using my cell phone Samsung Adaptive quick charger , 9V 1.67 A  , 5V 2.0A , matching the instruction manual specification for charging X - green LED when fully charged – never turned green, even after tens of hours charging using a 5V 350mA power supply. Instruction manual recommends a 5V 500mA – 2A power source.

  

X Motor low output (stall) torque –can stall shaft with bare fingers, can run grinder while pressing lock shaft button                

  • Low speed stalled shaft – speed control audibly buzzes with shaft stalled but continues to run in locked up (stalled) state
  • High speed stalled shaft - speed controller shuts down operation
Anonymous
  • I have that extension as well.

    Very useful for pinpoint uses.

  • Absolutely. The testing was intentionally pushing the limits, to compare it to the jobs a corded tool would do. The grinder did very well cutting a fiberglass PCB and drilling plastic.  It is very handy for an electronics workbench, being cordless, a nice grip, and light weight. It is also good for an "on the go" toolbox. 

  • Quite a detailed video. The tool is a must for machine enthusiasts. 

  • Nice review.

    I have had a Dremel for decades and just love it.

    So versatile and useful for so many different tasks.

  • Great review! I really appreciated the honest breakdown of the torque limits and how it behaves under load, especially on tougher materials like the stainless steel bolt and steel washers.

  • Interesting device. I have this one, which I really like, but is underpowered. 

    image

    One thing they really got right is that the power doesn't deplete quickly when in the power-off state, so that even after half a year there can still be some charge to use it - perfect for occasional use which suits me. But only has enough power for fine surface work such as engraving or cutting a PCB trace.

    However the MP011888 appears to have a proper slide switch, so I'm guessing it may be even better in that respect. Despite being called a grinder, I think perhaps the MP011888 could also be useful for enlarging small holes in PCBs, or cutting tracks and so on.

  • For precision with the mains powered one I have here, I have placed it on a hook and am using this kind of extension:

    image

    It really helps with fine details, but I often have to lower the rotation speed a lot to avoid burning through instead of cutting.

  • Great review! I really enjoyed the video, and I could relate to so many of those situations with my Dremel Smile. Thanks for sharing!