RoadTest: Cool Tools: 105 Piece Standard Screwdriver Set
Author: vlaine
Creation date:
Evaluation Type: Workshop Tools
Did you receive all parts the manufacturer stated would be included in the package?: True
What other parts do you consider comparable to this product?: TEKTON 2841 Everybit ($34.55 USD) or 33pc Security Bit Set ($6.29 USD) + a standard screwdriver set (approx. $15 USD)
What were the biggest problems encountered?: Not really a problem, but I did not know the name of each bit so I had to Google some of them. It would be nice to have a chart included with the set.
Detailed Review:
This screwdriver set is an incredible value for money.
It cost less than $22 CAD ($15.30 USD) and contains everything you need.
As a comparison, my current old rusty kit was purchased 20 years ago for $18.00.
Because I am always missing the bit I need, I purchased a lot of bits separately.
So my old kit plus the bits I purchased must have cost between $30 and $40.
Buy: http://www.newark.com/duratool/22-3495/105-piece-security-standard-screwdriver/dp/96B1231
| {gallery:autoplay=false} The package |
|---|
Duratool 22-3495 - 105 Piece Security and Standard Screwdriver set |
My old rusty kit as a comparison |
My old rusty kit as a comparison |
The screwdriver set, without the package |
The Duratool ratchet handle vs my old screwdriver: The Duratool fits better in the hand. It has an anti-slip finish and is well balanced |
| {gallery:autoplay=false} The bits |
|---|
Slot |
Slot |
Slot and Philipps |
Philipps |
Square |
Hex |
Hex |
Clutch G |
Pozi |
Hex and Torx |
Hex and Torx Closeup |
Hex and Torx Closeup |
Hex and Trox Closeup |
Security Bits - Tri-wing, Spanner, Security Hex, Security Torx |
| {gallery:autoplay=false} The Box |
|---|
Height - 7.5'' or 19 cm: Fits in my workshop drawer |
Width - 8 3/4'' or 22.5cm: Fits in my workshop drawer |
Top View |
Bottom View: Very stable when standing up because of the bottom legs |
Standing Up: Very stable because of the bottom legs |
| {gallery:autoplay=false} Real World Use |
|---|
Security Torx on my lawn mower battery pack |
Tri-Wing on my coffee maker |
I found the correct Tri-Wing bit for my coffee maker |