RoadTest: Raspberry Pi 3 in a Box
Author: rancell
Creation date:
Evaluation Type: Development Boards & Tools
Did you receive all parts the manufacturer stated would be included in the package?: True
What other parts do you consider comparable to this product?:
What were the biggest problems encountered?: Confusion about how to open drawers in box, missing simple instructions on how to assemble. Faulty SD card.
Detailed Review:
For this RoadTest we received a "Raspberry Pi Starter Kit" (as labelled on the box). This contains a Raspberry Pi 3, SD card, case, power supply, keyboard, mouse and HDMI cable - all the things you need to set up a Raspberry Pi desktop minus a display. The reviewers are one software engineer (me), my 6.5 and 8 year old daughters and an my four year old son. The older children are already experienced in using Raspberry Pi, but haven't assembled one themselves. I was particularly interested to see how they would be able to get everything working with minimal help.
This is actually a bit of a strange review, because the product appears to be discontinued having been replaced by the Raspberry Pi 4 Desktop Kit. So if you think this review is great, then you probably can't actually get the product unless you find some old stock. I'll review it for what it is, which is hopefully useful for anyone looking at a similar product. Some of the hardware and information is outdated, but I will review it as if it is the era of those components.
Everything comes in a beautiful 30 x 22 x 9cm box. The design is minimal, with a vibrant Raspberry Pi logo on the front. It gives the immediate impression of a high quality product.
Removing the lid continues the minimal design, with the case taking center stage. The case is just sitting in the insert, and is easy to remove. Opening the case shows the Raspberry Pi board already inserted. Arrows on the insert indicate the steps required to continue through the box and get to the mouse, power supply and HDMI cable which are contained in small drawers. This step was actually a little confusing, as it wasn't clear to me or my daughters how to open these drawers. I think this was due to there being no arrows on this step. I was looking for something to fold up and didn't consider that the drawers were there. Once you realized how to work them they are quite clever and effective.
The power supply came with US, EU, UK and AUS/NZ connectors that slide on. My daughters liked being able to assemble this. The USB LED mouse is slightly off white (doesn't quite match the case) and has a tidy looking Raspberry Pi logo. It feels a little bit plasticy, but seems to function well. The HDMI cable is a white 1m cable with Raspberry Pi branding. Pulling out the cardboard insert shows the final components, the USB keyboard, micro SD card and an "Adventures in Raspberry Pi" book (second edition). The keyboard is the same off-white as the mouse, but feels a little bit higher quality. It has the Raspberry Pi logo key (what is normally a Windows logo), which my daughters noticed and made more use of when running the Raspberry Pi desktop. The keyboard is small and thin, which is great for children using it. It has the standard fold out feel for elevating it, which my daughters noted as liking.
Some of the book was a bit outdated, which was quickly evident by the archaic Raspberry Pi 1 pictures in the early chapters. However, looking online shows there is a third edition available that is updated for this. If this product was still in production, I would expect it to come with the third edition. The book is well written and illustrated, and my daughters found it interesting and accessible. The chapter layout is a traditional "from command line to GUI" journey through the Raspberry Pi which I was surprised about. This is the way I learnt about computers, but most modern material does this in reverse so as not to put learners off.
With all the parts our of the box it was time to build a computer. The USB mouse and keyboard were easy to connect, but the other parts required a bit of prompting to show where they went. What helped was the names of all the components being written on the side of the box. The book wasn't a great help here for assembly as it didn't show the exact equipment in the box. What I think would have really helped was a one page diagram in the box that showed where everything went. This should be cheap to make but would really complete the unboxing experience. The Raspberry Pi board came inside the case, and only required the rubber feet stickers to be added. I think it would have made the assembly a little more exciting if you had to put the board inside the case, but this is a minor point.
We powered it on and.... Nothing. It turned out that the supplied SD card was faulty.
I attempted to reformat it but it was thoroughly dead. I hope this was bad luck and not representative of the SD cards in this kit. Another SD card was found and we got back to booting.
The next steps should be pretty familiar if you've used a Raspberry Pi with Raspbian before. You go through a slow installation process, the desktop boots up. It's simple but functional. The board in the kit is a Raspberry Pi 3 model B, which is sufficiently powerful to use the desktop without major concerns. The most notable absence was the lack of on-board WiFi - as USB WiFi dongle solved this for us.
My eldest immediately went to the Scratch chapter and followed the project there. She found the book easy to use and contained more detail than online tutorials have.
This kit is a great way for someone to quickly get a Raspberry Pi desktop up and working. The box is beautiful, and makes the whole product look high quality. The supplied book has plenty of information on what you can do with the Raspberry Pi. With the addition of a simple one page assembly instruction I think this would mean anyone should be able to quickly assemble everything.
Both the Raspberry Pi and book were a little out of date, but they would have been modern at the time this product was introduced.
My children loved unboxing and using the kit so I could recommend this product for children to get started in computing.
If you have a Raspberry Pi 4 Desktop kit I'd be interested to hear in the comments how you find it compares to this!