RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Polls Poll: Why Haven't You Applied for this Roadtest: STM32H7B3I-DK -  DISCOVERY KIT
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 1 Jul 2020 10:04 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:59 PM
  • Views 3381 views
  • Likes 2 likes
  • Comments 35 comments
Related
Recommended

Poll: Why Haven't You Applied for this Roadtest: STM32H7B3I-DK -  DISCOVERY KIT

Summertime is one of those busy times of year where people spend quality time with family, friends, and significant others. But this year you may be spending your summer time closer to home. And what better way to spend your quality time than with an element14 roadtest!

 

Inn particular, this roadtest: STM32H7B3I-DK -  DISCOVERY KIT

 

There are so many good things I could say about this dev board (with display). But the thing that stands out for me is what you can do with this board given all the peripherals you can experiment with:  the board help to evaluate the following peripherals: USB HS OTG, microSDTm card, 8-bit camera interface, audio DAC stereo with audio jack input and output, 128-Mbit SDRAM memory, 512-Mbit Octo-SPI Flash memory, Wi‑FiRegistered module (802.11 b/g/n compliant), I2C extension connector, FD-CAN, 20-pin microphone MEMS connector with DFSDM interface, 4.3-inch TFT-LCD (480*272) using an RGB interface with a capacitive touch panel.

 

You can even take advantage of three graphical stacks running on the same board with many featured applications:

– Menu launcher

– Audio player TGFX application (MP3 support)

– Clock and Weather with Alarm feature

– Video player TGFX application (enabled)

– TGFX Graphic demonstration

– STemWin Graphic demonstration

– EWZ Graphic demonstration

 

Poll Question: What's holding you back from applying to this roadtest?

  • scasny
  • community survey
  • community roadtest survey
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • rstone
    rstone over 6 years ago +7
    How about; Other, it's beyond my knowledge set. Rick
  • dougw
    dougw over 6 years ago +5
    This is a high end and very capable microcontroller kit. I am working on several projects that need a microcontroller, but this beast is way overkill for my projects. For modules like this I would mainly…
  • michaelkellett
    michaelkellett over 6 years ago +5
    The board shares a problem with many other dev boards - it's stuffed with goodies and that means it's only suitable for fun and not much use for work. I've looked at the chip and might use it, I have current…
  • hugohu
    hugohu over 6 years ago in reply to Jan Cumps

    Thank you, but international shipping is often more than the price of the product itself.

    Still, thank you for the offer!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crisdeodates
    crisdeodates over 6 years ago

    Didn't apply as already doing another roadtest and is yet to complete, which is unfortunately taking more time than expected due to some unforseen reasons.

    As soon as it is finished, will apply for the ones available at that time.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to hugohu

    I can send mine to you if you commit to write a report on element14 and want to pay the shipping from Belgium. I finished my road test.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hugohu
    hugohu over 6 years ago

    I didn't apply because I didn't find this place until it ended image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Andrew J
    Andrew J over 6 years ago in reply to Andrew J

    Following some of the comments on here, I've had my mind changed.  Jan saying what he would/wouldn't do is a good approach; Fred's view on the roadtest approach for boards like this I pretty much agree with, particularly "...decide if it's suitable for them" - that, if documented well, could be very informative for everyone.  I suspect some people would use such a board as a test-bed for the processor; whilst others would use the board as a product in its own right.  Price-wise it certainly stacks up against the Arduino+LCD+shields combination, and certainly the 4Duino boards I've been playing with. 

     

    I think I was initially overawed by the feature set and thinking how could one review that in such a short time and do it justice! 

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago

    I recently purchased two STM boards (it was new to me, that they come in two variants, a Nucleo board, and a feature-rich Discovery board). I picked up both variants for an STM F7 chip, since I wanted to try different things with them. I'm going to use the Discovery board for general experimenting with data/algorithms, and the Nucleo board for attaching specific bits of hardware (I've attached a SD card so far) to learn what I'd want on a custom board. They're awesome. The H7 series looks amazing.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 6 years ago

    It looks like a nice kit, but I leave these types of road tests to newer members.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 6 years ago in reply to rscasny

    With the previous more free-form road test applications I used to often say what I would and also wouldn't be doing. If you were expecting more than I could manage then I'd rather not be selected. Also, it meant that if I was selected then I knew when it was done and it was to the standard that had been agreed. With the new application format I haven't really felt this to be as necessary.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rscasny
    rscasny over 6 years ago in reply to Jan Cumps

    That sounds like a good approach: Define the scope of our roadtest. Scope: what you will do and won't do.

     

    Thanks for mentioning.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 6 years ago in reply to Fred27

    I agree.  I would suspect it would be of a benefit to the vendor to have someone new or not so familiar with the platform to see how hard it is to get to 'Blinky'. Although, with many of these vendors, the tools/IDE keep changing, so one with experience with the platform a couple of years ago might have a new learning curve with the new tools. Even TouchGFX has transitioned from a standalone tool to being incorporated into STM32CubeMX and STM32CubeIDE.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
>