Browse By Tags

  • XC7Z010 not able to bootup with DDR3L ( MT41K256M16TW-107 AUT:P) operating frequency of 533MHz

    Hi, we are facing the issue while booting up with 533MHz operating speed of DDR3L. Processor Part number : XC7Z010-2CLG400I DDR3L Part number : MT41K256M16TW-107 AUT:P Case 1: we have configured DDR3L operating speed to 533.333MHz in Vivado…
  • Double DRAM capacity on Beaglebone Black

    Is there a demand for more than 512MB DDR3 memory on the Beaglebone Black? Intelligent Memory is in production with 8Gbit DDR3 components with a single chip-select (part# IM8G16D3FBBG) that would make it possible to upgrade the Beaglebone to 1GB by replacing…
  • JEDEC Publishes DDR3L Low Voltage Memory Standard

    JEDEC, a developer of standards for the microelectronics industry , has announced the publication of JEDEC DDR3L, an addendum to its JESD79-3 DDR3 Memory Device Standard. DDR3L ( aka DDR3 Low Voltage) devices adhering to the new standard will operate…