555 Timers
  • Technologies
  • More
555 Timers
Forum Long Timing with a 555 IC
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 555 Timers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 4 answers
  • Subscribers 51 subscribers
  • Views 4116 views
  • Users 0 members are here
Related

Long Timing with a 555 IC

paddler47
paddler47 over 5 years ago

I am not an engineer. I am an old retiree who took up woodworking as a hobby and recently took an interest in making whirligigs. My third whirligig had a nautical theme, with a sailboat and a buoy which rocks when the wind blows. This time I decided to put a blinking LED on the buoy and started watching videos on YouTube to learn about LED's and solar charging circuits. I soon had a steadily blinking LED on my buoy, but wanted it to have an on-off-off-off-on-off-off-off, etc. pattern, so soon found Karen's videos on the 555 IC, and now have the desired blink pattern on my buoy. Now I want sound.

 

I picked up a few of those greeting card type MP3 player circuits and have gathered some suitable nautical sound files ranging in length of from about five seconds to about a minute. The MP3 players are triggered by a momentary push button switch, which I want to replace with a pulse timed to play the file, wait a while, and play it again. I need a circuit to generate those pulses.

 

The 555 IC claims "timing from microseconds through hours", but I've only seen demonstrations of fast blinking or flashing LED's, and I've seen the formulas and the nomograph in the data sheet, but just can't figure out where or how to start to get the necessary time delays. Do I start with a capacitor and the desired delay in microseconds and figure the R values from there?  I'm really lost. Am I on the right track at all?

 

I'm very new on this site, and this is my first post. I hope it's appropriate and in the right place. This is a very busy web site, and I get confused easily.

 

Message was edited by: John O'Neil Sorry for the long delay in getting back to this, but we had a major wind and rain storm the beginning of the week and the electricity has been off since Tuesday night. I'm going to have to start over reading the replies and studying the new information, and I have some catching up to do with other things, so it will be another day or so before I get back again. I think I should have mentioned that I'm talking about the astable mode of the 555, so my specific issues are the values of the two resistors and the capacitor, frequency, and the duty cycle. Thanks again!

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 5 years ago +6 verified
    There is a graph in the following link (labelled Monostable Nomograph) that allows you to pick any combination of resistance and capacitance that achieves the time you want: https://www.electronics-tutorials…
  • Jan Cumps
    Jan Cumps over 5 years ago +3 suggested
    If you need to tweek the duty cycle (to get 3 offs for 1 on), you need a bit of extra components. I have found speedy examples , no slow ones. Checking if I have a 555 in my bin ...
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to Jan Cumps +3 suggested
    So I did not find an NE555 but LTSpice has a model. I've replicated this design from All About Circuits (the article discusses several options); R3 and R4 are the 500K potentiometer of their schematic…
Parents
  • dougw
    0 dougw over 5 years ago

    There is a graph in the following link (labelled Monostable Nomograph) that allows you to pick any combination of resistance and capacitance that achieves the time you want:

     

    https://www.electronics-tutorials.ws/waveforms/555_timer.html

     

    image

    Time = 1.1 x R x C

    C = T / (1.1 x R)

    For example if you want 52 seconds, and you pick R to be 1MOhm, then C is about 47 uf.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 5 years ago

    There is a graph in the following link (labelled Monostable Nomograph) that allows you to pick any combination of resistance and capacitance that achieves the time you want:

     

    https://www.electronics-tutorials.ws/waveforms/555_timer.html

     

    image

    Time = 1.1 x R x C

    C = T / (1.1 x R)

    For example if you want 52 seconds, and you pick R to be 1MOhm, then C is about 47 uf.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer