Transportation & Automotive
  • Technologies
  • More
Transportation & Automotive
Blog Hybrids in industrial machinery
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Transportation & Automotive to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 14 Jun 2011 8:47 PM Date Created
  • Views 900 views
  • Likes 1 like
  • Comments 1 comment
  • alternative_energy
  • electric
  • transportation
  • industrial
  • ev
  • on_campus
  • hybrid
  • university
  • machinery
  • innovation
Related
Recommended

Hybrids in industrial machinery

Eavesdropper
Eavesdropper
14 Jun 2011
imageimage
 
 
Here is a perfect example of, "I can not believe this has not been done already."
 
Aalto University in Finland is testing the use of hybrid technology in non-road, mobile industrial machinery. Think Prius versions of cranes, bulldozers, tractors, and diggers. Their concept is to capture of the energy from the work being performed by each machine that is lost when in operation. Like in hybrid cars, deceleration, braking energies are being absorbed as well as energy from such tasks as lowering a load. For the record, no one has attempted making hybrids in this area.
 
Head researchers Professor Jussi Suomela spoke of the impetus of the project, "These heavy duty machines are operated for long periods of time, so by the end of the day emissions and fuel consumption have added up. Being able to target them is a significant improvement." From recent experimental data, Suomela has show that involving such combustion/electric hybrids in work machinery has the potential to save 50% of the fuel costs in stand alone operation, and even more if the system is plugged into the power grid.
 
Now it is not a question of can it be done, but when can it be implemented. Great work, Aalto University.
 
Eavesdropper
  • Sign in to reply
  • DAB
    DAB over 15 years ago

    This is a Great Idea.  If they could combine their equiment with solar and wind generated power, they could reduce their operating costs and get better efficiency from their equipment.

    Plus, in a controlled environment, they could utilize designs that work more efficient without needing to be robust enough to survive in hostile environments.  This approach could really reduce the costs to produce and use this type of equipment on a larger scale.

    I encourage everyone to think about things they use outside and consider how they could make it work under more benign conditions to make it better and safer.  There could be some real eye opening opportunities here.

     

    Thanks

    DAB