Transportation & Automotive
  • Technologies
  • More
Transportation & Automotive
Blog Inertial sensors enable active safety
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Transportation & Automotive to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: iLOVEautomotive
  • Date Created: 13 May 2011 11:25 PM Date Created
  • Views 672 views
  • Likes 1 like
  • Comments 1 comment
  • ap:automotive
  • in:automotive
  • esc
  • car
  • mems
  • harmems
  • accelerometer
  • xtrinsic
  • sp:freescale
  • electronic_stability_control
  • cars
  • low_g
  • safety
Related
Recommended

Inertial sensors enable active safety

iLOVEautomotive
iLOVEautomotive
13 May 2011

by Mike Stanley

image


Expanding on the topic of “active safety,” Freescale recently announced advanced Xtrinsic sensors for use in Electronic Stability Control (ESC). ESC works by comparing vehicle responses to user control inputs. If the two are inconsistent, ESC applies the individual wheel brakes of the car to bring things back in line. ESC is standard in high end vehicles today, but the technology is moving into the mainstream market as well. The U.S. National Highway Traffic Safety Administration will require the technology in most 2012 model vehicles. ESC has the potential to prevent nearly one-third of all fatal car accidents and 70 percent of fatal accidents of light trucks and vans.

 

The MMA690xQ dual-axis (X/Y) low-g accelerometers were designed specifically for safety critical applications. The devices are controlled via a standard SPI interface. Built with safety requirements in mind, the SPI module checks data parity and number of clock edges in a packet and flags errors to the host. The MMA690xQ also monitors critical internal voltages, on-chip clock frequencies, device temperature and programmed data integrity. The integrated self-test feature can apply an electrostatic force to stimulate and confirm accelerometer mechanical movement.

 

 

Interested? Read the complete entry

  • Sign in to reply

Top Comments

  • DAB
    DAB over 14 years ago +1
    This technology looks a lot like a program I worked on a bunch of years ago called "The Pilot Companion", where the computer would monitor the pilots normal reactions to situations and alert them when…
Parents
  • DAB
    DAB over 14 years ago

    This technology looks a lot like a program I worked on a bunch of years ago called "The Pilot Companion", where the computer would monitor the pilots normal reactions to situations and alert them when they were outside of the area of "normal" operation.  I am actually surprised that it took them this long to realize that you can privide a gentle assistance to drivers without forcing them to interact with the system.  Now if they could just find a way to detect when the driver is impaired and disable the vehicle, we could probably save a lot of lives.

     

    Thanks

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 14 years ago

    This technology looks a lot like a program I worked on a bunch of years ago called "The Pilot Companion", where the computer would monitor the pilots normal reactions to situations and alert them when they were outside of the area of "normal" operation.  I am actually surprised that it took them this long to realize that you can privide a gentle assistance to drivers without forcing them to interact with the system.  Now if they could just find a way to detect when the driver is impaired and disable the vehicle, we could probably save a lot of lives.

     

    Thanks

    DAB