Transportation & Automotive
  • Technologies
  • More
Transportation & Automotive
Blog Opel introducing new 1.6L diesel engine family; fuel consumption reduced by up to 10%
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Transportation & Automotive to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: autoembedded
  • Date Created: 17 Jan 2013 10:27 PM Date Created
  • Views 677 views
  • Likes 0 likes
  • Comments 0 comments
  • opel
  • transportation
  • fuel_efficiency
  • diesel
  • engines
  • automotive
  • engine
  • turbo-diesel
  • fuel_economy
Related
Recommended

Opel introducing new 1.6L diesel engine family; fuel consumption reduced by up to 10%

autoembedded
autoembedded
17 Jan 2013

Opel is introducing a new four-cylinder, 1.6-liter turbo-diesel engine as part of the fundamental renewal of its powertrain portfolio. The second family of new downsized power units to be introduced after the gasoline 1.6-liter SIDI Ecotec, the 1.6-liter CDTI Ecotec diesels will replace existing 1.7-liter engines and certain lower powered versions of the 2.0-liter range.

Featuring closed-loop combustion control and an aluminum block, the new 1.6 CDTI Ecotec is the first diesel from Opel to comply with future Euro 6 emissions requirements. The engine will be available in a variety of power outputs across several carlines.

Class-leading attenuation of noise, vibration and harshness, high power/torque density and low fuel consumption were the main development objectives.

Initially maximum power and torque have been increased versus the 1.7-liter engine to 136 hp (101 kW) and 320 N·m (236 lb-ft) respectively, while fuel consumption has been reduced by up to 10% compared with similarly powerful 2.0-liter diesels.

The new 1.6-liter diesel and its engine control unit have been entirely developed in-house by a global team of engineers in Turin, Rüsselsheim and the US. This approach has enabled a comprehensive system optimization from the beginning of the design process.

Beginning in spring, the 1.6 CDTI ECOTEC will be manufactured at the same “flex plant” as the new 1.6-liter gasoline engine, in Szentgotthard in Hungary.

Via Gcc