Transportation & Automotive
  • Technologies
  • More
Transportation & Automotive
Blog Students Build a Hydrogen-Fuel-Cell-Powered Locomotive
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Transportation & Automotive to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: autoembedded
  • Date Created: 27 Aug 2012 7:47 PM Date Created
  • Views 901 views
  • Likes 2 likes
  • Comments 2 comments
  • research
  • transportation
  • green
  • hydrogen
  • Technology
  • fuel_cell
  • automotive
  • university
  • automotive_innovation
  • locomotive
  • train
  • innovation
Related
Recommended

Students Build a Hydrogen-Fuel-Cell-Powered Locomotive

autoembedded
autoembedded
27 Aug 2012

Engineering students at the University of Birmingham in the U.K. have successfully built and demonstrated a hydrogen-fuel-cell-powered locomotive.

 

In testing at the Stapleford Miniature Railway in Leicestershire, the hydrogen-powered narrow-gauge train managed to carry a load that weighed more than 8,800 pounds. ”The hydrogen system worked quietly, efficiently and reliably throughout two days of testing,” said project leader Stephen Kent. “The same could not be said for the mechanical, electrical and control systems, all of which required a degree of fettling.”

 

Though it’s the first hydrogen-powered locomotive to be built in the U.K., so-called “hydrail” projects have been underway elsewhere since 2002, when the first hydrogen-powered locomotive prototype debuted in a mine in Val d’Or, Quebec. Since then, projects in Japan, China, and Denmark have attempted to fuel trains with hydrogen, and there’s even an annual hydrail conference sponsored by Appalachian State University.

 

The appeal of a hydrogen-powered locomotive is especially great for rural lines, where diesel is the current fuel of choice. “It is highly unlikely they will ever be electrified, and at some point diesel is going to become too scarce and too expensive to carry on using,” Kent said. “Hydrogen appears to be an ideal alternative.”

 

The student-built locomotive features a hybrid drivetrain that combines a hydrogen fuel cell and lead acid batteries for power storage. It has a 1,320-gallon hydrogen tank that stores fuel at a low pressure of just 72.5 psi, and it’s possible to fit a larger tank to allow for greater range.

 

According to Kent, the first “rail-world” uses of hydrogen fuel cells will likely be in low-power situations. For example, trams, trolleys, shorter branch lines and switchers don’t require the same power needs as, say, a high-speed passenger train.

 

“It is probably not yet a viable solution for more power-hungry applications such as high-speed trains, but then high-speed services increasingly tend to operate on electrified routes, so perhaps that’s not an issue,” he said.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

via Wired

  • Sign in to reply
Parents
  • DAB
    DAB over 14 years ago

    Great demo.

     

    I always smile when people tell me their is a fuel shortage.

    Given all of the Hydrogen, Methane and other renewable fuels, we have enough to power all of our needs until the Sun expands and burns up the planet.

    I just hope that the fuel cell technology advances enough that they become a small part of the cost factor.

    Until then, we will have to get by with the combustion engine, which will also run on hydrogen.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 14 years ago

    Great demo.

     

    I always smile when people tell me their is a fuel shortage.

    Given all of the Hydrogen, Methane and other renewable fuels, we have enough to power all of our needs until the Sun expands and burns up the planet.

    I just hope that the fuel cell technology advances enough that they become a small part of the cost factor.

    Until then, we will have to get by with the combustion engine, which will also run on hydrogen.

     

    DAB