Transportation & Automotive
  • Technologies
  • More
Transportation & Automotive
Blog Unique electric and solar bicycle
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Transportation & Automotive to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 1 Jul 2011 5:04 PM Date Created
  • Views 710 views
  • Likes 0 likes
  • Comments 1 comment
  • bicycle
  • electric
  • transportation
  • ev
  • on_campus
  • hybrid
  • innovation
Related
Recommended

Unique electric and solar bicycle

Catwell
Catwell
1 Jul 2011
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 
Self taught, Terry Hope has made his own solar power generating electric bicycle. Hope fitted the stock Specialized FRS 18 speed bike with a front grill and windshield for mounting eighteen 6"x6" mono crystalline sollar cells. Approximately 4 watt (@ 8.7v) output on each cell. Totaling 72 watts if all conditions are ideal. A 24V motor controller moves the 1 HP motor at the core of the project. Batteries are 6s1p 5000mah LIPO as the main, and two 4s1p LIPO 5000mah as "booster packs" which are wired in series. I assume he uses the "boosters" to overdrive the motor. Across the handle bars are several buttons used to turn the solar on or off for direct use, button for the booster, and the all important red E-stop. Hope added toggles to use solar for battery charging.
 
The motor itself drives the main sprocket. As with most multi-speed bicycles, the pedals are not engaged by the motor. The drive system is very unique compared to other electric bicycles. However, this is not ready for mass production. It is still very much a labor of love. I like the smaller electric bicycle Hope has made more than the 18 speed, see his launch page.
 
Can we do better? Help me build an electric bicycle with the rest of the community.
 
Cabe
  • Sign in to reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    Looks really nice. How is it coming along? How did you make the chain from the motor "freewheel" on the crankset? Was welding involved? Good luck!