Transportation & Automotive
  • Technologies
  • More
Transportation & Automotive
Forum Very Cool Looking - BMWs Diesel-Electric Hybrid Concept Sports Car
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Transportation & Automotive to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 86 subscribers
  • Views 978 views
  • Users 0 members are here
  • electric
  • sp:bmw
  • in:automotive
  • diesel
  • hybrid
Related

Very Cool Looking - BMWs Diesel-Electric Hybrid Concept Sports Car

tech1
tech1 over 17 years ago

BMW has created a new concept sports car in support of it's new greener credentials (though it is a shame to se them pull out of formula 1).

 

According to an article I read at edmunds.com, the car uses a turbo charged 1.5 litre three cylinder engine in combination with 2 electric motors coupled to the front and rear axels to deliver 356hp.

 

Check out the look of this thing though, now that look might convert me to hybrids!

 

BMW-VED-Diesel-Electric-concept.jpg

Related Article

  • Sign in to reply
  • Cancel
Parents
  • awinning
    awinning over 17 years ago

    Found the BMW PR, gives some more details

     

    Innovative concept car gets M3 power with record-breaking supercar economy and emissions figures BMW at the Frankfurt Motor Show

     

    The BMW Vision EfficientDynamics is BMW’s most innovative concept car ever and sets a new performance car agenda. Its unique powertrain, ground-breaking performance potential and exo-skeletal style bodywork crafted from aerodynamic knowledge gained in Formula One set it apart from anything previously seen.

     

    Powered by a three-cylinder turbo diesel engine and two electric motors, the BMW Vision EfficientDynamics is capable of BMW M3 performance but with a fraction of that model’s CO2 emissions and far greater fuel economy. The striking concept car is showcased with a powertrain producing an anticipated 356hp and 800Nm of torque for true supercar performance. However, the vehicle has been designed to be capable of recording 75.1mpg on the combined cycle and CO2 emissions of 99g/km.

     

    The vehicle’s impressive performance figures improve further when it runs solely in hybrid mode. When taking the sources of electrical energy generation into account the CO2 emissions of the BMW Vision EfficientDynamics drop to a staggering 51g/km*.

    The BMW Vision EfficientDynamics highlights a number of technologies that will appear on BMWs of the near future. BMW’s Air Curtain system that channels air through a front valance with the air exiting ahead of the front wheel is fitted. The Air Curtain system’s exiting air flow effectively deflects air from entering the wheel arch and causing turbulence thus improving all round performance.

     

    The bodywork of the BMW Vision EfficientDynamics also takes styling cues from the marque’s involvement in Formula 1. The exo-skeletal appearance of elements of the design mean the vehicle cleaves through the air with the least possible resistance. The drag co-efficient is 0.22 – the lowest figure of any BMW road car. The subtle folds of the bodywork that sit proud of the passenger cocoon create downforce without the need to have large spoilers.

     

    The 1.5-litre three-cylinder turbocharged diesel engine is another feature that indicates production potential. In isolation this new engine is capable of recording peak power of 163hp, a new record in terms of output per litre at 109hp, and a peak torque of 290Nm. Mounted transversely and ahead of the rear axle, the diesel engine can be the sole power source for the vehicle or it can work in conjunction with the electric drive. Alternatively the diesel engine can be used to charge the electric drive battery pack.

     

    The hybrid drivetrain features two electric motors – one on each axle. At lower speeds just the electric drive mode functions. The rear axle motor can produce up to 38kW of power and 290Nm of torque, while the second axle motor is capable of 60kW and 220Nm of torque. However, an overboost function allows the driver to top this up to 84kW for a 30 second boost and 104kW for a 10 second power enhancer. When taking all three power sources into account these figures equate to a car that records a peak power of 356hp and torque of 800Nm. Power is transmitted to the road via an enhanced version of BMW’s existing seven-speed Double Clutch Transmission.

    The BMW Vision EfficientDynamics has a range of 31 miles when driving only on electric mode. Combined with the three-cylinder diesel engine this extends to a total possible distance between fill-ups and charges of 431 miles. Using a conventional domestic power source at 220 V would result in the vehicle being fully recharged after 2.5 hours. Access to a slightly more powerful 380 V sees the charge time drop to 44 minutes.

     

    Unlike other hybrid vehicles that use existing vehicle architecture and then add a hybrid drivetrain, the BMW Vision EfficientDynamics isn’t penalised by weight. A V8 or larger capacity engine that would be the norm for a supercar has been substituted by a compact three-cylinder engine and two electric motors. This is fitted to an aluminium chassis to further save weight. The result of this is that the vehicle tips the scales at just 1,395kgs.

    The use of low rolling resistance tyres has also taken on another twist to offer something unique. Normally customer demand for larger alloy wheels with wider tyres is at odds with aerodynamic and rolling resistance targets. However, BMW engineers working with Michelin developed a solution to this conundrum. The contact patch of the BMW Vision EfficientDynamics has effectively been turned 90 degrees by virtue of specifying larger diameter wheel rims. Larger, but thinner tyres result in the same percentage of rubber being in contact with the road, but the cross section of the tyre as a whole is smaller making for less rolling resistance and greater aerodynamic efficiency.

     

    BMW is renowned for using lightweight materials as part of its EfficientDynamics strategy and this concept car is no different. The chassis and suspension are made entirely from aluminium while the roof and the outer skin of the doors are made of a lightweight polycarbonate glass. This material also comes with special properties that allow the glass to darken in sunlight to keep the cabin temperature at the desired level.

    The BMW Vision EfficientDynamics also showcases BMW’s Thermo Electric Generator currently fitted to the exhaust system of test cars and being developed for production. This works on the principle of the Seebeck effect to generate an electrical current courtesy of the temperature change between two metal based semi-conductors. This system alone generates enough charge to power some of the auxiliary features.

     

    Inside, and the 3D Head-up Display is another feature that highlights at possible production car capability as does a new incarnation of iDrive with a touchpad screen. The vehicle’s 4.6 metre length, 1.9 metre width and 1.24 metre height permit a 2+2 configuration that makes this supercar a practical form of transport. With the rear seats folded the BMW Vision EfficientDynamics even has room for two sets of golf clubs that can be stowed in the 150-litre luggage area.

     

    The BMW Vision EfficientDynamics is the centrepiece of the BMW stand at the Frankfurt Motor Show. Click here for more images and video footage of this model and other new products at the show.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • awinning
    awinning over 17 years ago

    Found the BMW PR, gives some more details

     

    Innovative concept car gets M3 power with record-breaking supercar economy and emissions figures BMW at the Frankfurt Motor Show

     

    The BMW Vision EfficientDynamics is BMW’s most innovative concept car ever and sets a new performance car agenda. Its unique powertrain, ground-breaking performance potential and exo-skeletal style bodywork crafted from aerodynamic knowledge gained in Formula One set it apart from anything previously seen.

     

    Powered by a three-cylinder turbo diesel engine and two electric motors, the BMW Vision EfficientDynamics is capable of BMW M3 performance but with a fraction of that model’s CO2 emissions and far greater fuel economy. The striking concept car is showcased with a powertrain producing an anticipated 356hp and 800Nm of torque for true supercar performance. However, the vehicle has been designed to be capable of recording 75.1mpg on the combined cycle and CO2 emissions of 99g/km.

     

    The vehicle’s impressive performance figures improve further when it runs solely in hybrid mode. When taking the sources of electrical energy generation into account the CO2 emissions of the BMW Vision EfficientDynamics drop to a staggering 51g/km*.

    The BMW Vision EfficientDynamics highlights a number of technologies that will appear on BMWs of the near future. BMW’s Air Curtain system that channels air through a front valance with the air exiting ahead of the front wheel is fitted. The Air Curtain system’s exiting air flow effectively deflects air from entering the wheel arch and causing turbulence thus improving all round performance.

     

    The bodywork of the BMW Vision EfficientDynamics also takes styling cues from the marque’s involvement in Formula 1. The exo-skeletal appearance of elements of the design mean the vehicle cleaves through the air with the least possible resistance. The drag co-efficient is 0.22 – the lowest figure of any BMW road car. The subtle folds of the bodywork that sit proud of the passenger cocoon create downforce without the need to have large spoilers.

     

    The 1.5-litre three-cylinder turbocharged diesel engine is another feature that indicates production potential. In isolation this new engine is capable of recording peak power of 163hp, a new record in terms of output per litre at 109hp, and a peak torque of 290Nm. Mounted transversely and ahead of the rear axle, the diesel engine can be the sole power source for the vehicle or it can work in conjunction with the electric drive. Alternatively the diesel engine can be used to charge the electric drive battery pack.

     

    The hybrid drivetrain features two electric motors – one on each axle. At lower speeds just the electric drive mode functions. The rear axle motor can produce up to 38kW of power and 290Nm of torque, while the second axle motor is capable of 60kW and 220Nm of torque. However, an overboost function allows the driver to top this up to 84kW for a 30 second boost and 104kW for a 10 second power enhancer. When taking all three power sources into account these figures equate to a car that records a peak power of 356hp and torque of 800Nm. Power is transmitted to the road via an enhanced version of BMW’s existing seven-speed Double Clutch Transmission.

    The BMW Vision EfficientDynamics has a range of 31 miles when driving only on electric mode. Combined with the three-cylinder diesel engine this extends to a total possible distance between fill-ups and charges of 431 miles. Using a conventional domestic power source at 220 V would result in the vehicle being fully recharged after 2.5 hours. Access to a slightly more powerful 380 V sees the charge time drop to 44 minutes.

     

    Unlike other hybrid vehicles that use existing vehicle architecture and then add a hybrid drivetrain, the BMW Vision EfficientDynamics isn’t penalised by weight. A V8 or larger capacity engine that would be the norm for a supercar has been substituted by a compact three-cylinder engine and two electric motors. This is fitted to an aluminium chassis to further save weight. The result of this is that the vehicle tips the scales at just 1,395kgs.

    The use of low rolling resistance tyres has also taken on another twist to offer something unique. Normally customer demand for larger alloy wheels with wider tyres is at odds with aerodynamic and rolling resistance targets. However, BMW engineers working with Michelin developed a solution to this conundrum. The contact patch of the BMW Vision EfficientDynamics has effectively been turned 90 degrees by virtue of specifying larger diameter wheel rims. Larger, but thinner tyres result in the same percentage of rubber being in contact with the road, but the cross section of the tyre as a whole is smaller making for less rolling resistance and greater aerodynamic efficiency.

     

    BMW is renowned for using lightweight materials as part of its EfficientDynamics strategy and this concept car is no different. The chassis and suspension are made entirely from aluminium while the roof and the outer skin of the doors are made of a lightweight polycarbonate glass. This material also comes with special properties that allow the glass to darken in sunlight to keep the cabin temperature at the desired level.

    The BMW Vision EfficientDynamics also showcases BMW’s Thermo Electric Generator currently fitted to the exhaust system of test cars and being developed for production. This works on the principle of the Seebeck effect to generate an electrical current courtesy of the temperature change between two metal based semi-conductors. This system alone generates enough charge to power some of the auxiliary features.

     

    Inside, and the 3D Head-up Display is another feature that highlights at possible production car capability as does a new incarnation of iDrive with a touchpad screen. The vehicle’s 4.6 metre length, 1.9 metre width and 1.24 metre height permit a 2+2 configuration that makes this supercar a practical form of transport. With the rear seats folded the BMW Vision EfficientDynamics even has room for two sets of golf clubs that can be stowed in the 150-litre luggage area.

     

    The BMW Vision EfficientDynamics is the centrepiece of the BMW stand at the Frankfurt Motor Show. Click here for more images and video footage of this model and other new products at the show.