Transportation & Automotive
  • Technologies
  • More
Transportation & Automotive
Forum LED软灯条方案D7001/D7002可大幅减少芯片使用数量
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Transportation & Automotive to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 88 subscribers
  • Views 1421 views
  • Users 0 members are here
Related

LED软灯条方案D7001/D7002可大幅减少芯片使用数量

power_biso
power_biso over 15 years ago

中心议题:

  • D7001/7002的典型应用
  • 高性能低成本LED软灯条、护栏管解决方案

解决方案:

  • LED软灯条方案D7001/D7002可大幅减少芯片使用数量

杨晓鹏:我今天要介绍的是高性能低成本LED软灯条、护栏管解决方案。LED装饰灯的份额逐年扩大,目前已经占据80%的份额。西方的圣诞节会采用大量的装饰灯来装点节日氛围,传统的装饰灯能源消耗很大。而采用LED装饰灯,要比传统照明节能85%,省电性能高,使用寿命长(可达50000小时以上),环保(无汞等有害物质)等优良的特点,确保了LED软灯条在户外,室内装饰照明市场的优异表现。LED装饰灯正成为一种潮流。

D7001、D7002套片是针对LED灯条、护栏管等装饰产品的解决方案,与传统产品相比,该方案具有高性能、高可靠性、设计简洁、低成本等诸多优势,为LED灯条、护栏管等产品升级换代提供了一个更优的解决方案。下面介绍下D7001、D7002的特点:

  • D7001为具有24路输出的LED驱动芯片,使用32脚5x5mm QFN封装,在软灯条上,这个面积已经很小了;
  • D7002为总线驱动芯片,使用8脚SOP封装。
  • 应用本方案驱动24路单色LED或者8组RGB全彩LED仅需一颗D7001和一颗D7002。

下图是套片典型应用线路图。D7001可按照恒流及PWM的方式驱动24路。D7002用于接收主控发送的控制数据,并把控制数据传递到下一级D7002,从而实现灯条或护栏管的多级级联。

image

该方案的特点是有丰富的显示效果:

  • D7001/7002应用了全新的控制方式并固化了多种预置显示模式,并且可根据需求定制。
  • D7001/7002芯片可以实现并超越任何现有灯条及护栏管产品的显示效果。
  • 流水灯、渐变、跳变、正反向移位、淡入、淡出、呼吸、七彩平滑过渡等各种显示效果。

更高的可靠性:

  • D7001/7002每组芯片有24路输出,可以驱动8组RGB全彩LED,大幅度降低了芯片的级联级数,提高了系统可靠性。
  • D7001/7002总线仅需要两条数据线,而且每级D7002都对总线数据进行了整形和再生和容错处理,总线传输的可靠性就得以大幅度提高。
  • D7001/7002最大限度的避免了控制信号中断、显示效果混乱以及长距离传输出错等故障。

 

 


下面是D7001/7002的典型应用电路图。上面是8颗5050 RGB LED,下面是LED驱动IC D7001和总线传输芯片D7002。外围元件只需要两颗电阻,一颗电容,元件非常少。

image

下面是一个宽度为15mm,长度为25cm的软灯条PCB,一组D7001/7002及8个5050 RGB全彩LED。PCB上外围器件很少,线路非常简单。

image

下图是一个护栏管PCB,尺寸80x12mm,此模块可以应用在真八段或真六段护外控栏管上,电源电压可以是12V或24V。

image

因为D7001/7002软灯条、护栏管方案大幅减少芯片使用数量,下面是驱动8颗RGB LED方案的成本对比。得倍方案的芯片使用两颗,一颗是LED恒流驱动芯片,一颗是总线控制芯片,外围使用2颗电阻,1颗电容,LED灯的焊接点是46个。从对比可看出,得倍方案大幅度的减少了行业同类产品所使用的芯片数量,并简化了电路设计、物料数量及生产工艺,从而节省成本。

  • Sign in to reply
  • Cancel
Parents
  • bharathmuthukuri
    bharathmuthukuri over 9 years ago

    Hello,

    Greeting from Bosch India.

     

    In one of my robotic project we are also have requirement to control LED brightness and color.

    So i am looking for a part you mentioned in above post. I google a lot for IC manufacturer but no use.

     

    Can you please help me to get this manufacturer and part as well.

     

    Thanks in advance.

    Best regards

    Bharath Muthukuri

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ling1995
    ling1995 over 8 years ago in reply to bharathmuthukuri

    I think kynix may give you some help,there are many electronics are in stock at kynix including D7001 and D7002.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ling1995
    ling1995 over 8 years ago in reply to bharathmuthukuri

    I think kynix may give you some help,there are many electronics are in stock at kynix including D7001 and D7002.