Transportation & Automotive
  • Technologies
  • More
Transportation & Automotive
Forum Why use relays over semiconductor switches?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Transportation & Automotive to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 89 subscribers
  • Views 1327 views
  • Users 0 members are here
  • mosfet
  • igbt
  • switches
  • thyristor
  • semiconductor
  • relay
Related

Why use relays over semiconductor switches?

e14 Contributor
e14 Contributor over 16 years ago

Can anybody help on this? For medium voltage applications, say 100V~ 600V, what is the benefit of using an electro-mechanical relay as opposed to electronic switches, either a thyristor/IGBT/MOSFET? Reliability, voltage isolation, safety issues? There are many advantages to using an electronic switch in terms of speed, avoiding spikes, power consumption, propensity to failure, cost, etc..? So would there be any reason to use an electro-mechanical relay over semiconductor based switches? Thanks so much..  BTW, the application does not involve switched mode power supply or anything that needs any speed in switching. I would really appreciate if anyone can help.

  • Sign in to reply
  • Cancel
Parents
  • Paul
    0 Paul over 16 years ago

    One reason you might want to use a relay is if the circuit being controlled needs to be electrically isolated rather than just being "off".

    Electronic switches do not completely isolate and will allow a small leakage current to flow when they are "off".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • M0DCD
    0 M0DCD over 16 years ago in reply to Paul
    Some other reasons to use electromechanical devices are first that the control/drive circuit is physically and electrically isolated from the load. Secondly, and possibly the most common is that these devices invariably fail open. Yes you can get contact welding, but in interlocking applications such as railway signalling this is the mode that is wanted. SSI (Solid State Interlocking) ends up be a mess of duplicated systems and voting control. Relays usually fail because of the contacts wearing out, but semiconductors often fail short circuit. UK regulation seems to shy away from innovation because of these issues - such as it took them 20+ years to accept LEDs as light sources for signalling.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • M0DCD
    0 M0DCD over 16 years ago in reply to Paul
    Some other reasons to use electromechanical devices are first that the control/drive circuit is physically and electrically isolated from the load. Secondly, and possibly the most common is that these devices invariably fail open. Yes you can get contact welding, but in interlocking applications such as railway signalling this is the mode that is wanted. SSI (Solid State Interlocking) ends up be a mess of duplicated systems and voting control. Relays usually fail because of the contacts wearing out, but semiconductors often fail short circuit. UK regulation seems to shy away from innovation because of these issues - such as it took them 20+ years to accept LEDs as light sources for signalling.