Transportation & Automotive
  • Technologies
  • More
Transportation & Automotive
Forum Is it possible to fly a glider with a plasma propulsion system.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Transportation & Automotive to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 87 subscribers
  • Views 2455 views
  • Users 0 members are here
Related

Is it possible to fly a glider with a plasma propulsion system.

e14 Contributor
e14 Contributor over 15 years ago

Is it possible to fly a glider with a plasma propulsion system.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 15 years ago in reply to autoembedded +1
    Sorry that video is blocked to the UK for copywrite reasons. Ion rocket engines have to be on for 100s if not 1000s of hours, they carry their own fuel. the engine I envisage is air breathing and air exhaust…
Parents
  • Catwell
    0 Catwell over 15 years ago

    Kevin,

     

    Is this the same type of plasma propulsion that NASA is working on?

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autoembedded
    0 autoembedded over 15 years ago in reply to Catwell

    "Frost mean Speed"

     

    I hear in this video that this project wants to be launch in this year (2011).

     

    And with this propulsion we could do a ride of 39 days to Mars.

     

    I'm perplexed.

     

    Greetings

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to autoembedded

    Sorry that video is blocked to the UK for copywrite reasons. Ion rocket engines have to be on for 100s if not 1000s of hours, they carry their own fuel. the engine I envisage is air breathing and air exhaust.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to autoembedded

    Sorry that video is blocked to the UK for copywrite reasons. Ion rocket engines have to be on for 100s if not 1000s of hours, they carry their own fuel. the engine I envisage is air breathing and air exhaust.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autoembedded
    0 autoembedded over 15 years ago in reply to e14 Contributor

    Kevin, thanks for the feedback.

     

    IDelgado

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to autoembedded

    what I would like is for someone to tell me that a plasma could be made in air in a tube and then pushed out with a magnetic field. I know plasma exhausts are very fast, but I was thinking that the ions would collide with other air atoms and set them in motion at the same time slowing the ions down to maybe 200mph. So although Ion and plasma engines are low thrust devices, by opperating them in the air in a tube each ion would push upto around 100 to 150 atoms of air, that doesn't sound much but when you get a million or so ions, all doing this energy exchange, you end up with a lot of thrust at a lower energy level. hopefuly at 200mph or so.

    Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    I don't get ion-pushing-air atoms part. Ion engine is just a very efficient engine. It works because of Newton's 2rd and 3rd laws just like similar combustion engines. There's no pushing, just preservation of momentum. There's no point of using ion engines in atmosfere since they cannot generate enough thrust to overcome movement air resistance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Hi Maciej Kucia. Ok so you don't get the ion pushing air atoms part. Imagine a pool table, the white ball is an ion and all the other balls are the air atoms, now the pool que is the magetic force that makes the ion move. so it drives the white ball (ion) into the other balls (air atoms), Does the white ball stop or does it move the other balls, if you've played pool you'll know that the balls move and the white might stop or deflect of into other air atoms. While the ion is in the magnetic field it will keep trying to move along its lines of force, and so the air is moved, but not as fast as the ions do.

    I hope this helps.

    Kevin.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    So basically what you are saying is: ions and air molecules are both within magnetic field and due to viscosity air molecules are being moved by ions. I am not engine engineer but I doubt that there are ion engines where air can enter magnetic field. And even if there is an air why do not lionize it and accelerate too! Actually I can imagine such engine but it would require tens if not hundredths of kilowat power.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Hi, Yes about 23 to 25 kilowatts to make somewhere between 150 to 200lbs thrust, and yes the air entering the magnetic field would get ionized and would push with the rest of the ions. Unlike the ion / plasma engines made to work in space, this ion engine would use just electricity (lots of it) to firstly ionize some of the air at the front of the engine, and then to accelerated the ions with a magnetic field, this will make the ions (which are the same density as the other air molecules that didn’t get ionized at the air intake) move through the rest of the air and push them out the back as well, and then finally neutralised the ions with electrons from emitters at the back of the engine.

     

    Kevin