Transportation & Automotive
  • Technologies
  • More
Transportation & Automotive
Documents Development Of World’s First “Corrosion Resistance BEARPHITE” Using Aluminum Bronze
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Transportation & Automotive to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: iLOVEautomotive
  • Date Created: 7 Jan 2013 5:29 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 5:22 AM
  • Views 674 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Development Of World’s First “Corrosion Resistance BEARPHITE” Using Aluminum Bronze

NTN Corporation (hereafter, NTN) has developed the “Corrosion Resistance BEARPHITE” for use in environments that result in fast corrosion of bearings, such as within gasoline.

 

Motorized fuel pumps and exhaust gas recirculation devices (EGR*1) for automobiles and motorcycles are generally equipped with bronze sintered bearings or white cooper sintered bearings. Bronze sintered bearings become corroded by the organic acids contained within gasoline, while white cooper sintered bearings need to use expensive nickel.

 

NTN has now successfully developed the world’s first “Corrosion Resistance BEARPHITE” that delivers outstanding corrosion resistance using aluminum bronze without the need to use nickel.

 

Aluminum bronze is a material that features outstanding corrosion resistance, however it forms an oxide on its surface under high temperatures, which until now meant it was not suited to powdered metal sintering. NTN has reviewed the composition of the material used, and developed the manufacturing process technology to improve the sintering performance for a level of corrosion resistance that is the same or better than white cooper materials. The friction coefficient has been reduced by including an optimum quantity of graphite within the material, which has drastically improved wear resistance.

 

NTN has already started to propose the developed product to manufacturers in the automotive industry, and in the future will propose the product in industrial machinery fields where bearings are used in corrosive environments such as salt water.

 

*1 EGR:Exhaust Gas Recirculation

 

Via AW

  • releases
  • automotive
  • cars
  • new_releases
  • gasoline