Transportation & Automotive
  • Technologies
  • More
Transportation & Automotive
Documents Audio Processing
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Transportation & Automotive to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: Sunnyzhuo
  • Date Created: 23 Nov 2009 12:51 AM Date Created
  • Last Updated Last Updated: 7 Oct 2021 1:27 AM
  • Views 538 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Audio Processing

Source: http://www.altera.com

 

Audio processing is becoming a key part of several automotive electronic modules, especially in the infotainment arena where more and more consumer applications are demanded to be part of the automotive offering. The move to higher resolution digital audio, combined with new and complex digital signal processing (DSP) algorithms, means 24-bit, fixed-point processors can no longer satisfy the requirements for audio quality, flexibility, and speed. We expect audio requirements to continue growing as high-definition multimedia applications are refined for automotive use.

The quality requirements of in-car audio are lower than those for domestic reproduction, due to the higher background noise of the environment.

 

However, digital audio is now established in this area via CD and digital radio, which is virtually immune to interference and does not need to be retuned during a journey. MiniDisc and other digital formats can also be incorporated.

 

Using an AlteraRegistered CycloneRegistered series FPGA for audio processing include the following benefits:
  All audio sources can be processed by the same FPGA, enabling digital

  amplification, equalization, and loudspeaker balancing
  Fast processing enables useful extra features, such as dynamic range compression
  Non-audio sources can also be processed by the same FPGA with its high I/O capability—software defined radio (SDR), global positioning     system (GPS), and digital radio text services—to provide a one-chip solution for in-car DSP requirements

 

Figure 1 shows a conceptual implementation of the next-generation audio processing systems. The combination of the NiosRegistered II 32-bit embedded RISC processor with a Cyclone series FPGA provides a high-performance, effective, and flexible solution. The Nios II processor provides the flexibility to implement a coder/decoder (CODEC) with the option of accelerating the compute-intensive portion of the algorithms with custom instructions or with the Nios II C-to-Hardware (C2H) Acceleration Compiler.

 

Figure 1. Conceptual Implementation of an Audio Processing System in an AlteraRegistered FPGA

 


image

Notes:
MCU = microcontroller unit
SPI = serial peripheral interface
AAC = advanced audio coding