Transportation & Automotive
  • Technologies
  • More
Transportation & Automotive
Documents Hydrogen Vehicles Gaining Momentum, Need Fueling Infrastructure Strategy
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Transportation & Automotive to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: iLOVEautomotive
  • Date Created: 12 Aug 2011 3:52 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 3:07 AM
  • Views 621 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Hydrogen Vehicles Gaining Momentum, Need Fueling Infrastructure Strategy

image

I was driving westbound through fog and heavy mist traversing the Florida panhandle  when it clicked. The same stuff that was reducing visibility – a  moisture saturated blanket of hydrogen and oxygen molecules – was also  powering the car I was driving, but in a different form.

 

The car was one of a fleet of three Mercedes-Benz F-Cell cars being  driven around the world to raise awareness of hydrogen fuel cell  vehicles. Along with two other automotive journalists, I was  participating in the first North American leg of the Mercedes-Benz  F-Cell World Drive. Over 125 days, the program will have logged more than 20,000 miles, crossed 14 countries, and traversed four continents.

How did my car work? Its fuel cell ‘stack’ was taking in hydrogen on  one side of a membrane and outside air containing oxygen on the other.  As the two elements interacted, a chemical reaction created electricity  with sufficient energy to power the car’s electric drivetrain. Very  cool.

image

A primary advantage of fuel cell power is that no combustion takes  place and the process is virtually emissions-free. While fuel cell cars  do have a tailpipe, it’s for evacuating water from the fuel cell since  the only emissions are water vapor and a little bit of heat. This clean  energy means fuel cells can be operated in congested areas without  environmental worries. Fuel cell technology is versatile and fully  scalable, too, with many applications outside transportation such as  providing back-up or primary power for households or industrial  electrical needs.

Number-one on the periodic table of elements, H2 (hydrogen) has the  atomic number of 1 with one proton and one electron. It’s both the  simplest element in our world and by far the most abundant in the  universe. The name hydrogen comes from the Greek words ‘hydro’ and  ‘genes,’ which translates into ‘water-forming.’ It is also the stuff  that fuels stars, and not just the ones in Hollywood that drive fuel  cell cars. Our sun is powered by hydrogen in a process called fusion.

image

Closer to home, the idea of powering our personal transportation with  hydrogen is very appealing. Hydrogen can be either burned in an  internal combustion engine or used to produce electricity in a fuel cell  stack without combustion, the latter producing no C02 greenhouse gases.  Most of the hydrogen we use today is produced from steam reformation of  natural gas. But it can also be made by other means including  electrolysis, a process that uses electrical current to split water  (H20) into hydrogen and oxygen.

Hydrogen is sometimes disparaged as a fuel source because it can take  nearly as much energy to produce as is contained in the hydrogen fuel  created. This becomes less of an argument as more efficient means of  hydrogen production are developed and when the electrical power used to  create H2 comes from renewable sources like wind, solar, hydro, and  off-peak power from nuclear and other powerplants that often goes to  waste.

Things have been relatively quiet on the hydrogen front over the past few years with so much attention being devoted to electric vehicles.  Still, most major automakers continue to develop hydrogen fuel cell  technology as a longer-term solution to our transportation needs. Our  experience on the F-Cell World Drive illustrates that these cars are  ready for prime time. All we need now is a hydrogen infrastructure,  which of course is no small thing.

 

 

SOURCE: GreenCar.com

  • automotive
  • hybrid
  • cars
  • innovation