Transportation & Automotive
  • Technologies
  • More
Transportation & Automotive
Documents Volkswagen to implement cylinder deactivation in 4-cylinder 1.4 TSI engines in 2012
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Transportation & Automotive to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: autoembedded
  • Date Created: 7 Sep 2011 4:28 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 3:40 AM
  • Views 1348 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Volkswagen to implement cylinder deactivation in 4-cylinder 1.4 TSI engines in 2012

Volkswagen will debut cylinder deactivation (cylinder shut-off) technology in the new  1.4-liter TSI turbocharged, direct-injection engine beginning in 2012.  Volkswagen is the first carmaker to implement this technology in a  turbocharged four-cylinder engine in large-scale production.

 

The primary goal of the system is to reduce significantly fuel  consumption by temporarily shutting off two of the four cylinders  (cylinders 2 and 3) during low to mid loads; Volkswagen says that  cylinder shut-off reduces fuel consumption of the 1.4 TSI by 0.4 liter  per 100 km in the NEDC driving cycle. When the Stop/Start functionality  is integrated, which deactivates the engine in neutral gear, the savings  effect adds up to about 0.6 liter per 100 km.

 

1.4 TSI
The new 1.4 TSI outputs 103 kW (140 PS, 138 hp), with 250 N·m (184 lb-ft) of torque between 1,500 and 4,000 rpm.

The greatest benefits of the technology are realized while driving at  constant moderate speeds. At 50 km/h (31 mph), in third or fourth gear, savings amount to nearly  one liter per 100 km. Even when running on two cylinders, the 1.4  TSI—with its excellent engine balance—is still very quiet and low in  vibration, Volkswagen says.

 

Cylinder shut-off is active whenever the engine speed of the 1.4 TSI  is between 1,400 and 4,000 rpm and its torque is between 25 and 75 N·m  (18–55 lb-ft). This applies to nearly 70% of the driving distance in the  EU fuel economy driving cycle. As soon as the driver presses the  accelerator pedal sufficiently hard, cylinders 2 and 3 are reactivated  unnoticed.

 

Under the deactivation process, the combustion chambers are filled  with air—this entrapped fresh air leads to minimal cylinder pressure and  therefore to lower energy consumption. Afterwards, the system closes  the intake and exhaust valves of cylinders 2 and 3; engine ignition only  occurs once per crankshaft revolution. The pistons of the deactivated  cylinder are now dragged by the crankshaft. On the other hand,  efficiency increases in the two active cylinders, because their  operating points are shifted to higher loads.

 

The valves are closed using a complex set of actuators: on both the  intake camshaft and the exhaust camshaft, there are two adjustable  sleeves (cam pieces) that are placed on special tooth systems. They are  responsible for the eight valves of the second and third cylinders. At  the ends of each cam piece, there are two different profiles adjacent to  one another: a conventional full profile and a so-called zero-lift cam.  The full profiles actuate the roller cam followers, which in turn  actuate the valves in four-cylinder operation; that is, they behave like  very conventional cams.

 

However, the zero-lift cams rotate over the  followers—i.e. they do not actuate them—and the valve springs hold the  valves shut. Engine management simultaneously shuts off fuel injection.

 

Spiral-shaped slots are milled in the outer surfaces of the rotating  cam pieces; these slots permit shifting the sleeves a few millimeters  along the shafts very quickly; when electromagnetic actuators in the  valve cover get a signal from the engine controller, two integrated  metal pins engage the slots from outside and move them to their end  positions. Finally, the cam pieces are locked in place by spring-loaded  balls. As soon as the driver presses the accelerator pedal sufficiently,  cylinders 2 and 3 are reactivated.

 

All mechanical switch-over processes are executed within one-half  camshaft revolution; they last between 13 and 36 milliseconds, depending  on engine speed. These processes are smoothed by accompanying  interventions in ignition and throttle valve control.

 

Volkswagen utilizes information from the gas pedal sensor to detect  the driver’s mode of driving. If the driving exhibits a non-uniform  pattern—e.g. while driving in roundabout traffic or in a sporty style on  a country road—shut-off functionality is suppressed.

 

The components for cylinder shut-off weigh a total of just over 3  kilograms. Their actuators, the camshafts and their bearing carriers are  integrated in the valve cover. Two roller bearings reduce the friction  of the shafts.

 

image

 

SOURCE: www.greencarcongress.com

  • transportation
  • fuel_efficiency
  • engines
  • vehicle_systems
  • automotive
  • volkswagen
  • auto