Transportation & Automotive
  • Technologies
  • More
Transportation & Automotive
Documents Bentley Continental GTC: first pics
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Transportation & Automotive to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: autoembedded
  • Date Created: 31 Aug 2011 2:17 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 3:45 AM
  • Views 613 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Bentley Continental GTC: first pics

image

 

This is the new Bentley Continental GTC, announced ahead of its official world premiere at - you guessed it - the Frankfurt motor show.

The second-generation of Bentley's iconic drop-top has been "improved  in virtually every aspect" over the first, some feat considering the  original was a lightly monstrous machine.

Power from the 6.0-litre twin-turbocharged W12 engine has swollen  from 552bhp to 567bhp, while torque rises from an already gargantuan  479lb ft to 516lb ft, which is enough to send the echoes of the Big Bang  skittering back into the corners of the universe.

 

See more pics of the new Bentley Continental GTC

 

The 0-60mph dash is covered in 4.5 seconds (0-62mph in 4.8s),  0-100mph takes 10.9 seconds and the top speed is 195mph. In fact,  30-50mph takes only two seconds, and 50-70mph takes a blink-of-an-eye  longer (2.4s). And should your moral allegiances force you into acting  greenly, that W12 also runs on E85 biofuel too.

 

That prodigious power output is, again, sent to all four wheels via a  ‘Quickshift' six-speed auto ‘box (said to cut shift time by up to 50  per cent), while a new rear-biased torque split of 40:60 is said to  reduce understeer and allow for "throttle steering". There's another  name for that. Hooning.

 

Bentley says advanced manufacturing techniques have produced new  aluminium front wings without the need for seams or welds, "creating the  look and feel of a coach-built car", while you are suitably indulged  inside with soft-touch leather, wood veneers, ‘cool-touch' metals,  deep-pile carpets and a tailored, multi-layered fabric hood developed  for optimum noise isolation. Rear passengers even get more legroom.

 

Top Gear drives the Bentley Continental GTC Speed

 

Wolfgang Dürheimer, Bentley chairman, said: "The GTC has always been  the most emotional model in the Continental range and a showcase for  Bentley design. It's a pure British convertible true to those classic  Bentleys of the past, but the excellence invested in this model means we  are now writing a new chapter for the Bentley convertible driver."

 

SOURCE: www.topgear.com

  • transportation
  • automotive
  • bentley
  • auto