Transportation & Automotive
  • Technologies
  • More
Transportation & Automotive
Documents ACAL Energy completes build of first field test system of FlowCath fuel cell technology
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Transportation & Automotive to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: autoembedded
  • Date Created: 25 Oct 2011 4:59 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 4:34 AM
  • Views 674 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

ACAL Energy completes build of first field test system of FlowCath fuel cell technology

UK-based ACAL Energy has completed the build of its first field test system of its FlowCath platinum-free  liquid cathode fuel cell technology, producing gross power of 3kW. (Earlier post.) The company has also achieved a new record single-cell peak performance power density of nearly 900 mW/cm2, which is a substantial improvement over the previously announced peak power record of around 600 mW/cm2.

 

image

Rendering of ACAL Energy’s fuel cell engine, showing stack and external regenerator.


FlowCath technology replaces up to 90% of the current level of platinum  catalyst in a proton exchange membrane (PEM) fuel cell with a low-cost,  durable liquid chemical. The liquid is continuously pumped through the  fuel cell stack into an external regenerator and then back to the stack.  The technology also significantly reduces the balance of plant costs by  eliminating the need for hydration, pressurization, complex cooling and  other expensive mechanical sub-systems commonly found in conventional  PEM fuel cells.

 

Field test unit. The first FlowCath demonstration unit will be  installed next month at Solvay Interox’s chemical plant at Warrington,  Cheshire. There, it will provide continuous electrical power to a remote  environmental monitoring system within the manufacturing facility. The  stack and regenerator sub-systems in the demonstration unit are together  capable of producing more than 3kW of gross electrical power and  represent a significant scale-up from the previous generation test unit  which produced about 1kW of gross power.

 

The demonstration system is part of a collaborative project that ACAL  Energy is leading, co-funded by the UK’s Technology Strategy Board. The  project is seen as a major step towards commercialization for this  technology, and is supported by ACAL Energy’s partners: Solvay Interox,  Johnson Matthey Fuel Cells, UPS Systems, the Centre for Process  Innovation, the University of Southampton and the Manufacturing  Engineering Centre at Cardiff University.

 

New peak power with focus on automotive. The new record peak power output from a single cell of nearly 900 mW/cm2 was achieved under the PEM Challenge grant project sponsored by the  Carbon Trust, which is funding accelerated development of ACAL Energy’s  technology for automotive applications. The latest performance results  give the company even greater confidence in the ability of its  technology to meet the efficiency requirements of nearly all stationary  and automotive applications, while delivering a substantially higher  level of durability than conventional fuel cells.

 

With the successful implementation of our FlowCath  technology into a full multi-kilowatt system, ACAL Energy has passed a  significant milestone in our business plan. We have shown that this new  low cost and durable fuel cell technology can be packaged and operated  in a form suitable for nearly all stationary power applications.

 

To have broken new performance records at the same  time is a very promising sign that we can also make this technology  suitable for automotive applications.

—Dr SB Cha, CEO of ACAL Energy
SOURCE: Green Car Congress
  • acal
  • transportation
  • flowcath
  • car
  • fuel_cell
  • automotive
  • auto