Transportation & Automotive
  • Technologies
  • More
Transportation & Automotive
Documents Former F1 Designer’s Tiny EV Gets 350 MPGe
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Transportation & Automotive to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: autoembedded
  • Date Created: 14 Nov 2011 6:59 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 4:42 AM
  • Views 590 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Former F1 Designer’s Tiny EV Gets 350 MPGe

image

 

Gordon Murray’s itty-bitty EV cleaned house at the Future Car  Challenge, achieving the equivalent of 350 mpg and trouncing cars like  the Nissan Leaf, BMW Active-E and various European diesels to take top  honors.

 

The Lilliputian T.27 electric car consumed 7 kilowatt-hours of energy  during a 57.13-mile jaunt from Brighton to London last weekend,  bringing the former Formula 1 designer his second consecutive victory at  the Royal Automobile Club’s Future Car Challenge. The point of the race  was not to reach the finish line first, but to do so using the least  amount of energy while completing the trip within the allotted time.

 

“This year’s success in combination with last year’s win with our petrol-powered T.25 proves absolutely that light weight is our most powerful tool for  solving our energy problems,” Murray said in a statement. “We look  forward to working with a manufacturing partner to make the T.27 with  its low running costs available to the motoring public.”

 

image

 

Murray pioneered the use of composites in Formula 1 with Brabham and  McLaren, then went on to design the McLaren F1 and Mercedes-McLaren SLR  supercars. Since leaving Formula 1 in 2006, Murray has focused like a  laser on making cars smaller, lighter and more efficient. He is  evangelical in his belief that cutting weight is the fastest, cheapest  way to reduce fuel consumption.

 

His Chapmanesque obsession with weight has great implications for  electric vehicles, because weight is the enemy of range. If you halve  the weight of the car, Murray told us last summer, you can halve the  size of the battery needed to power it.

 

At just a bit more than 4 feet wide and just a bit shy of 8 feet long, Murray’s city cars are smaller than a Smart ForTwo or Scion iQ yet they can seat three people or carry 750 liters [26 cubic feet] of cargo.

 

We hear you back there muttering about small cars being death traps.  Not so. The T.25 and T.27 feature a composite monocoque bonded to a  tubular steel frame and plastic bodywork. The T.25 has a four-star Euro  NCAP safety rating. Let those who doubt the strength of a well-designed  composite safety cell Google the words “Robert Kubica crash Canada 2007” or “Mark Webber crash Valencia 2010.” Go ahead. We’ll wait.

 

The T.27 electric vehicle draws juice from a 12.5 kilowatt-hour  lithium ion battery. It’s propelled by a 25-kilowatt motor. The claimed  range is 110 miles, though Murray says that drops to 85 when you’ve got  the heater and other stuff running.

 

Murray has no interest in building the T.25 and T.27 himself; he’s  talking to a third party about that. He built the prototypes to showcase  an innovative manufacturing method that replaces stamped steel with  composites. He calls it iStream, for Stabilized Tube-Reinforced Exoframe Advanced Manufacturing,  and says it requires 80 percent less capital investment and 60 percent  less energy that conventional auto manufacturing. Cars built using  iStream — which Murray says can be used for everything from microcars to  13-passenger vans — are 20 to 25 percent lighter than conventional  autos.

 

The T.27 led a field of 50 vehicles to take the overall victory at  the race. Second place went to a homebuilt electric Jaguar E-Type  (insert Lucas joke here) that used 8.5 kilowatt-hours of juice to make  the trip. Full results are available here. (.pdf)

 

SOURCE: Autopia

  • bmw
  • transportation
  • car
  • f1
  • automotive
  • electric_car
  • cars
  • auto
  • nissan