Transportation & Automotive
  • Technologies
  • More
Transportation & Automotive
Documents Toyota new hydrogen fuel cell concept vehicle
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Transportation & Automotive to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: autoembedded
  • Date Created: 15 Nov 2011 6:31 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 4:42 AM
  • Views 662 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Toyota new hydrogen fuel cell concept vehicle

Toyota unveiling new hydrogen fuel cell concept vehicle indicative  of 2015 production model at Tokyo Motor Show; Aqua hybrid and FT-EV III

 

Toyota Motor Corporation (TMC) will stage the world premiere of the FCV-R, a practical sedan-type next-generation  hydrogen fuel-cell concept vehicle, at the upcoming Tokyo Motor Show.  Toyota calls this concept model “a highly practical fuel-cell vehicle” that is planned for launch in about 2015.

 

image

 

With the fuel-cell unit located beneath the specially designed body, the  vehicle can accommodate up to four passengers and offers what Toyota  calls “impressive” luggage space. The fuel cell system, along  with a 70 MPa high-pressure hydrogen tank, has been improved to provide a  cruising distance of approximately 700 km (435 miles) or more under the  JC08 test cycle, according to TMC.

 

Four other concepts or prototypes will also have their world premieres at the Tokyo show:

  • The Aqua, an affordably priced compact-class dedicated hybrid vehicle.  Toyota says that the Aqua represents the future of compact vehicles with  a fuel efficiency of approximately 35 km/L (82 mpg US, 2.86 L/100km)  under the JC08 test cycle; 40 km/L (94.1 mpg US, 2.5 L/100km) under the  10-15 test cycle.  The body, at less than four meters long, offers  outstanding handling, while the minimized height enhances aerodynamic  performance, providing comfortable maneuverability with stylish  proportions.

     

    The hybrid system combines a 1.5-liter engine with a high-output motor  to create a low center of gravity for enjoyable operation and  outstanding maneuverability, all while still offering interior comfort  and ample luggage space.

     

    Following the launch in Japan, scheduled for late December 2011, the  Aqua will be sequentially rolled out to other countries and regions  worldwide.

     

    image

     

  • The FT-EV III is an electric concept vehicle with an ultra-compact and  lightweight package suitable for short-distance trips. TMC says it is  developing EVs with the aim of launching a vehicle suitable for  short-distance travel in 2012. Equipped with a lithium-ion battery, the  FT-EV III achieves an estimated cruising range of 105 km (65 miles) on a  fully charged battery.

     

  • The Toyota Fun-Vii, a concept vehicle that heralds a future where people, cars and society are linked.

 

  • The prototype model of a compact rear-wheel-drive vehicle jointly developed by Fuji Heavy Industries and TMC.

     

Toyota is also holding the Japan premiere of the Prius Plug-in Hybrid at the show. 

 

SOURCE: GreenCarCongress

  • transportation
  • hydrogen
  • car
  • fuel_cell
  • toyota
  • automotive
  • hybrid
  • cars
  • auto