Transportation & Automotive
  • Technologies
  • More
Transportation & Automotive
Documents Ethernet on wheels*
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Transportation & Automotive to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: autoembedded
  • Date Created: 27 Dec 2011 4:11 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 4:45 AM
  • Views 507 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Ethernet on wheels*

By Axel Streicher

 

Ethernet on wheels … is not really groundbreaking news, some may say.  No argument here, since 100Mbps Ethernet has been around for a while as  an on-board diagnostics (OBD) port and access point to the vehicle for  re-programming or flashing modules at the OEM dealership.

 

The news is that the automotive industry is making strong efforts to  standardize Ethernet as in-vehicle network for high bandwidth  applications such as cameras and multimedia. Up to now, high bandwidth  meant proprietary network architectures with cumbersome cabling,  expensive physical interface devices, custom tools and limited supplier  base.

 

Recently, Broadcom, BMW, NXP, Freescale, Hyundai Motor Company and Harman announced the formation of the OPEN Alliance SIG (One-Pair Ether-Net Special Interest Group).  The alliance’s goal is to enable wide scale adoption of Ethernet in  automotive, establish industry standards for Ethernet connectivity over a  single pair unshielded cable and enable migration from closed  application to open, scalable Ethernet-based network.

 

With more than 40 years of development history, Ethernet is the  de-facto industry standard for high bandwidth communication in  networking, office, industrial and other markets. Since these industries  spearhead the communication bandwidth requirements, the automotive  world can rely on future developments, wide availability of tools,  widespread knowledge base and broad support from the semiconductor  industry. Already today, many of Freescale’s microcontrollers feature an  integrated Ethernet MAC layer, including the 32-bit Qorivva MPC5604E MCU for ADAS applications that supports audio video bridging (AVB).

 

Key to the OPEN Alliance is the proliferation of Broadcom’s  BroadR-ReachRegistered technology as an open standard. It addresses key concerns  of the automotive industry such as the stringent EMC requirements,  weight reduction, availability from multiple sources and cost  efficiency. Based on single unshielded twisted pair cable (UTP), it  delivers a bandwidth of 100Mbps, perfectly suitable to handle  applications such as camera-based park assist systems.

 

Analysts project significant digital camera growth for advanced driver assistance systems. Broadcom, Freescale and OmniVision have collaborated to develop the world’s first Ethernet-based  360-degree surround view parking assistance camera system. Based on the  BroadcomRegistered BroadR-ReachRegistered BCM89810 physical layer transceiver (PHY), the  Freescale 32-bit Qorivva MPC5604E MCU, and OmniVision’s OV10630 color  CMOS image sensor, the system  expands the opportunity for OEMs to  deploy surround view parking assistance capability across a broad range  of vehicle classes, ranging from luxury to mass market automobiles.

 

Ethernet on wheels — ground breaking news? No, not really. But this  new way of using it will bring a host of automotive applications to  market that were never imagined before.

 

More about the article visit blogs.freescale.com

  • transportation
  • freescale
  • ethernet
  • car
  • wheels
  • automotive
  • cars
  • auto