Transportation & Automotive
  • Technologies
  • More
Transportation & Automotive
Documents EV Drivers Adopt Solar Chargers to Wean Themselves Off the Grid
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Transportation & Automotive to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: autoembedded
  • Date Created: 6 Dec 2011 8:26 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 4:45 AM
  • Views 451 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

EV Drivers Adopt Solar Chargers to Wean Themselves Off the Grid

image

 

Many Mini drivers accessorize their cars with things like  checkered-flag decals on the mirrors or the Union Jack on the roof.  Colby Trudeau chose something a little more radical.

 

When Trudeau’s family took delivery of an electric Mini E two years ago, they gave the little EV a big upgrade: a 4.4 kilowatt  solar-power system on the roof of their San Diego home.

 

Going solar  offset the Mini’s operating costs and covered most of the household  energy costs, dropping the family’s monthly electric bill to around $25.  When the Mini went back to BMW after its lease expired earlier this  year, a Chevrolet Volt took its spot in the garage.

 

The Trudeaus are early adopters among early adopters, one of a small  but growing number of people who are buying electric vehicles and  embracing the idea of true zero-emissions driving.

 

“Once we had the electric car, going solar made even more sense,”  said Trudeau, who grew so evangelical about cars with cords that he  started volunteering at the advocacy group Plug In America.  “Instead of sending our money overseas to power a polluting vehicle, we  are now powering our car on cheap, clean, domestic electricity from the  sun.”

 

It couldn’t be happening at a better time. Even as electric vehicles gain traction with consumers, the price of solar panels is falling  precipitously. The two technologies complement each other, which is why  many EV owners are going solar. It’s also why automakers like Ford are  teaming up with solar startups to make plugging into the sun easier than  ever.

 

Offsets and Arbitrage


Solar-powered EVs are a bit of a misnomer. Most chargers are tied into the grid and  use a variety of sources — including the sun — to directly charge the  car. But these systems typically produce enough power to offset the  electricity drawn by the car, and in some cases send power back to the  grid.

 

It’s an ideal arrangement, said Mike Tinskey, Ford’s associate  director for vehicle electrification and infrastructure. The automaker  recently announced a partnership with SunPower to offer solar  installations that offset the electricity needed to power a Ford Focus Electric driven 12,000 miles a year.

 

Critics will argue, “But that’s not a solar-powered EV.” Well, no,  not always. Although a car plugged in during the day would be powered by  the sun, most EVs are plugged in at night. Going solar lets an EV owner  offset that while also selling power to the utility during periods of  high demand while charging at night when demand, and rates, fall.

 

“People called it energy arbitrage,” Tinskey said. “Sell the power when you don’t need it and pull the power when you do.”

 

The customer base for solar EV chargers is varied. You’ll find  green-power advocates, energy-security activists, pacifists,  isolationists, off-grid DIYers and professional engineers.

 

They share a  fascination with driving without the need for fossil fuels or nuclear  power.

 

Of course, a large number of people interested in going electric also  are interested in going solar, if they haven’t already. Most of them  realize it isn’t cheap — even a modest system will set you back a few  grand — but it isn’t the bottom line so much as energy independence that  drives them.

 

“The idea that you can actually independently fuel your own car, or  cars, with a rooftop solar gas station for a reasonable price has  tremendous appeal that cuts across political lines,” said Christof  Demont-Heinrich, a University of Denver communications professor and  solar enthusiast who runs the SolarChargedDriving.com blog.

 

Demont-Heinrich estimates 30 to 50 percent of EV early adopters have  installed solar or expressed interest in doing so soon. It’s an  admittedly unscientific survey, once based upon polls at his site and  others, including mynissanleaf.com. Still, it suggests a growing trend, one he expects to continue as public awareness grows.

 

“It’s a really big step forward that large automakers like Ford, GM  and Nissan are actively promoting this synergy,” Demont-Heinrich said.  “I think most people are not aware of this at all. They’re barely aware  of EVs. To bring in solar as well makes it an even smaller percentage.”

 

That awareness will rise as automakers sing the solar gospel. GM  Ventures, General Motors’ VC arm, has invested $7.5 million in Sunlogics  and called on the company to build solar Chevrolet Volt charging  stations (pictured above) at 12 dealerships nationwide. Earlier this  year, Nissan installed 30 solar charging stations at its corporate HQ in  Smyrna, Tenn.

 

On the other side of the coin, several people who already use solar  power at home are considering electric vehicles. To that end, companies  specializing in home solar systems are beginning to offer EV chargers as  well. SolarCity has installed more than 2,500 residential solar EV  charging stations, for example, and REC Solar has joined GE to include  GE WattStation Level 2 chargers in new solar setups.

 

“A lot of the early adopters from PV (photovoltaic) are looking  forward to a good mainstream EV,” said Lee Johnson, CEO of REC Solar’s  parent company Mainstream Energy. “They’re saying, ‘I’m ready to get the  car, I need to upgrade my system a little bit.’”

 

From Homebrew to Turnkey


Until now, most of the solar charging rigs have been homebrew setups  by DIYers or systems custom designed and installed by professionals —  two approaches that could be time-consuming and expensive. As cars with  cords follow the Nissan Leaf, Chevrolet Volt and others to market,  automakers are joining solar installers to provide plug-and-play setups  you can buy alongside the car. The idea is to make going solar as easy  and inexpensive as possible.

 

“We said, let’s size a standard system to offset 12,000 miles of  driving per year and let’s get as much cost out of the system by  standardizing it,” Tinskey said.

 

The 2.5 kilowatt system SunPower developed with Ford consists of 11  modules, requires 153 square feet of roof space and has a 25-year  warranty. It isn’t cheap — Ford’s system is expected to come in for less  than $10,000 after tax rebates — but advocates of the technology say  prices will keep coming down.

 

“We’re on the cusp of multiple new technologies, and of solar becoming affordable for all the middle class,” Tinskey said.

 

We’ve already seen the cost of solar panels drop 17 percent between  2010 and 2011 and another 11 percent during the first half of this year.  Federal and local tax breaks cut costs further. Uncle Sam offers a 30  percent tax credit for solar installation, for example, and most EVs and  plug-in hybrids qualify for a $7,500 federal tax credit.

 

A Level 2 (240 volt) charger from SolarCity costs $1,500 installed. The photovoltaic cells needed to keep the juice flowing will  set you back $50 a month. By SolarCity’s math, the average urban driver  spends about $230 a month on gasoline (at an average of $3.65 a  gallon). Plugging into the grid cuts that to $107 a month, and a  SolarCity rig brings it to $54.

 

For many people, though, going solar with an EV is about more than  saving money. It’s about reducing dependence on petroleum, using  domestic energy sources and minimizing their carbon footprint. Anyone  who looks only at the upfront cost will almost certainly say, “Why  bother?” because you can buy a whole lot of gas for what it costs to  install even a basic solar rig.

 

That said, those willing to pay those initial costs eventually will  see long-term declines in home energy costs. The savings will eventually  offset the cost of installing the solar system, though how long that  might take depends upon local utility rates and tax incentives.

 

Tinskey estimates that drivers who use their Focus Electric 300 days  annually and drive 12,000 miles will see payback within four to 12  years. The quickest payback is in Raleigh, NC, where state, local and  utility rebates have brought the price of the installed solar system  down to about $5,000.

 

In addition to falling solar-panel prices, other factors will help make solar charging affordable.

 

“Lithium-ion batteries are coming down to a reasonable price level,  and obviously we’ve got all of the telematics pieces coming together for  control and time-of-use rates,” said Tinskey.

 

“If you take those three  trends and you add in the government incentives that are happening that  prime the pump, it’s actually a really good time in terms of cash outlay  to think of some of these technologies.”

 

SOURCE: Autopia

  • infrastructure
  • transportation
  • ev
  • car
  • plug-in_hybrids
  • electric_vehicles
  • automotive
  • cars
  • solar
  • auto