Transportation & Automotive
  • Technologies
  • More
Transportation & Automotive
Documents Effenco hydraulic hybrid system targeted at heavy-duty vehicles with high power demand auxiliaries
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Transportation & Automotive to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: autoembedded
  • Date Created: 19 Jan 2012 2:59 AM Date Created
  • Last Updated Last Updated: 8 Oct 2021 4:46 AM
  • Views 800 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Effenco hydraulic hybrid system targeted at heavy-duty vehicles with high power demand auxiliaries

Montreal, Canada-based Effenco has  developed a hydraulic hybrid system (HEAD, Hydraulic Equipment  Assisting Device) specifically targeted to vehicles with high power  demand auxiliaries, such as refuse trucks. The hybrid system comprises a  regenerative braking system which includes variable displacement  hydraulic pumps and a gearbox; a hydraulic accumulator; and a hydraulic  motor.

 

image

The Effenco hydraulic hybrid system can drive the existing hydraulic  pump for auxiliary equipment or assist the engine. Source: Effenco.  Click to enlarge.

 

Regenerative braking converts braking kinetic energy into a pressurized  fluid stored in the accumulator; the system regenerates more than 80% of  the braking energy under 22 mph (35 km/h). Rather than using the  recovered energy to provide power for acceleration, the Effenco system  can drive the vehicle’s existing hydraulic pump that supplies auxiliary  equipment, or assist the combustion engine at idle.

 

To do so, a variable displacement hydraulic motor is mechanically  coupled to the engine and to the hydraulic pump via a power take-off  interface of the transmission.

The accumulator has a capacity of 54 liters, with a maximum working pressure of 5,000 psi.

 

In either mode of assistance, the engine consumes less or no fuel.  Effenco says its system reduces fuel consumption by 15-25% and increases the lifespan of brakes by a factor of 3.

 

The HEAD system can be installed or retrofitted on any chassis,  according to the company. With a parallel configuration, the system does  not affect the truck’s reliability; the truck can operate normally even  if the HEAD system is temporarily offline.

 

An onboard screen provides the driver with dynamic driving guidance about driving efficiency.

 

Current price of the system is $50,000; there are 7 HEAD hybrid systems on trucks on the road, and 5 to be delivered.

 

Source GreenCarCongress

  • transportation
  • automotive
  • hybrid