Transportation & Automotive
  • Technologies
  • More
Transportation & Automotive
Documents Mitsubishi Motors to introduce the New Outlander at Geneva show
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Transportation & Automotive to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: autoembedded
  • Date Created: 9 Feb 2012 4:23 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 4:48 AM
  • Views 518 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Mitsubishi Motors to introduce the New Outlander at Geneva show

Mitsubishi Motors Corporation (MMC) will present the global debut of the all-new Outlander at the 82nd Geneva International Motor Show, 6-18 March. During fiscal 2012 Mitsubishi Motors will add an EV-based Outlander model which will use a plug-in hybrid system derived from MMC’s already existing EV technology.

 

Also on display on the Mitsubishi Motors stand will be the MiEV House, a model for a near-future “EV (electric vehicle) lifestyle” that maximizes household energy usage with the help of an EV.

 

The new Outlander will be launched first in Russia this summer, after which it will make its debut in European, Japanese, Oceania, Chinese and North American markets.

 

The European-market specification Outlander is offered with a choice of gasoline and diesel engines. Gasoline models are powered by the 4J11 2.0-liter in-line 4-cylinder SOHC MIVEC engine which employs an all-new valvetrain. Diesel models use the 4N14 2.2-liter in-line 4-cylinder turbocharged MIVEC engine with a very low compression ratio of 14.9:1 that meets European diesel emission regulations.

 

The diesel Outlander (2WD drivetrain, 4N14 engine with 6-speed manual transmission) is targeting CO2 emissions of under 130 g/km through the use of MMC’s Auto Stop&Go idle-stop system and its lighter body that stems from optimization of the body structure, the use of high-tensile strength paneling and from improved aerodynamics.

 

The new Outlander will also be equipped with an “eco-friendly driving system” that notifies the driver when he or she is driving at maximum efficiency. With this system, the driver can choose to drive at maximum efficiency to enhance actual fuel consumption of the vehicle.

 

Source Green Car Congress

  • plug-in
  • car
  • mitsubishi
  • automotive
  • hybrid
  • cars
  • auto