Business of Engineering
  • Technologies
  • More
Business of Engineering
Blog Rethink safety for autonomous vehicles
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Business of Engineering to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: yoSoyTono
  • Date Created: 18 Jul 2018 12:48 PM Date Created
  • Views 2204 views
  • Likes 4 likes
  • Comments 8 comments
  • driverless
  • autonomous
  • sensors
  • lidar
  • cameras
  • radar
  • code
  • gps
  • Self-driving
  • software
Related
Recommended

Rethink safety for autonomous vehicles

yoSoyTono
yoSoyTono
18 Jul 2018

Nearly in every case of the accidents involving self-driving vehicles, unexpected circumstances not catered for by human programming was the cause of the problem —the Google shuttle in Las Vegas, some Ubers in Arizona, the Tesla car in Florida, and several others in California. If driverless vehicles are supposed to make safer roads, the bigger question is What should these cars or trucks do to reduce accidents?

 

Engineers are struggling to figure out the underlying safety challenge: even when autonomous vehicles are doing what they are supposed to, all nearby cars and trucks drivers are flawed and capable of making errors.

 

There are two principal crashing causes involving self-driving vehicles:

- The sensors are not detecting what is happening around the vehicle due to its quirks: cameras only work correctly with enough light, LiDAR struggles to operate through the fog, Radar is not exceptionally accurate, and GPS performs better with a clear view of the sky. Nowadays, engineers are defining the right mix of sensors to be implemented, as the solution is just not adding more of them on self-driving vehicles because both cost and computing power are limiting factors.

- The software is mishandling unexpected situations when the vehicle faces conditions that is not programmed to do. All self-driving vehicles have to make hundreds of decisions every second and adjusting the path using the incoming data from the environment, just like human drivers.

 

Engineers must combine the data from all the sensor inputs and create an accurate computerized model of the vehicle surrounding; then the code can interpret that representation to instruct the car or truck on how to navigate and interact with whatever might be happening nearby. Basically, the vehicle will not take the right decisions if the perception of the system is not accurate. It will not be enough for autonomous vehicles to drive safely to fulfill expectations of reducing crashes; they must become the ultimate defensive driver, ready to react when other vehicles nearby drive unsafely.

 

Some of the incidents with driverless vehicles show machines did not entirely understand the situation to define the correct action; those vehicles executed the rules they had but were not making sure their decisions were the safest ones —because of the way most self-driving vehicles are being programmed and tested. Engineers need to code autonomous vehicles with instructions on how to behave when some vehicle do something out of the ordinary; besides, testers should consider other vehicles as adversaries while developing plans for extreme situations. The basic standard for both is making driverless vehicles follow the laws of the road: obeying traffic lights and signs, knowing local transit rules, and behave as a law-abiding human driver.

 

However, what should an autonomous vehicle do if a car is driving in the wrong direction? Currently, self-driving vehicles totally stop and wait for the situation to change —definitely, no human driver would do this. A person would take evasive action and switch lanes without signaling, driving onto the shoulder, or speeding up to avoid a crash —even if those meant breaking a traffic rule. Engineers need to teach autonomous vehicles to understand not only the surroundings but the context. A truck approaching from the front means no harm if it is in the other lane, but is entirely different if it is in the same lane.

image

 

As car makers are becoming better at implementing self-driving technologies, they must rethink safety for autonomous vehicles and test them under complex tasks (like parking in a crowded lot or changing lanes in a work zone) to analyze and improve how they perform, not only on lonely unidirectional or multi-lane highways under good weather. Those driverless tests might be similar to human driving tests, but is exactly what it should be if autonomous vehicles and human drivers will have to coexist safely on the roads.

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 8 years ago +3
    I'm unsure how you can make this statement Nearly in every case of the accidents involving self-driving vehicles, human error was that cause of the problem and not the autonomous vehicle (I highlighted…
  • ntewinkel
    ntewinkel over 8 years ago in reply to mcb1 +3
    > I'm unsure how you can make this statement >>Nearly in every case of the accidents involving self-driving vehicles, human error was that cause of the problem and not the autonomous vehicle I agree with…
  • mcb1
    mcb1 over 8 years ago in reply to ntewinkel +3
    So in reality all you have is an adaptive cruise control and no real autonomous driving. Great. This issue is even worse than I'd heard, so thanks for sharing it. Once again the car manufacturers are being…
  • mcb1
    mcb1 over 8 years ago in reply to ntewinkel

    So in reality all you have is an adaptive cruise control and no real autonomous driving.

    Great.

     

    This issue is even worse than I'd heard, so thanks for sharing it.

     

    Once again the car manufacturers are being led by PR people, and have a delivered a product with known design flaws.

    What surprises me if the likes of Ralph Nader has even allowed them on the road.

     

    Mark

    PS lucky your wife was paying attention, otherwise you could have both been hurt.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to ntewinkel

    Oh, this explains why the Tesla we were driving didn't want to stop - the truck in front of us was standing still, in a line at a red traffic light. The car that was in front of us had moved to the left-turn lane, if I recall correctly.

     

    From that same article, about Tesla's sensors:

    "“The radars they use are apparently meant for detecting moving objects (as typically used in adaptive cruise control systems), and seem to be not very good in detecting stationary objects,""

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to mcb1

    > They didn't say it had self stopping, that's why she was there .... image

    Hahaha! yes true that.

    In our case it was rainy but visibility was quite good. I kinda wonder if they just can't handle the higher vehicles.

     

    >hello it's still a really large metallic object.!

    Hi!  image

    Yes don't they have radar?

     

    Looks like there's some serious issues that still need to be worked out, like dealing with still-standing fire trucks:

    https://www.wired.com/story/tesla-autopilot-why-crash-radar/

     

    This bit  is scary, to do with Volvo, but sounds like Tesla does the same:

    "Say the car in front of the Volvo changes lanes or turns off the road, leaving nothing between the Volvo and a stopped car. "Pilot Assist will ignore the stationary vehicle and instead accelerate to the stored speed," ... In other words, your Volvo won't brake to avoid hitting a stopped car that suddenly appears up ahead. It might even accelerate towards it."

     

    Hopefully by the time we're too old to drive they'll have these details figured out image

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to ntewinkel
    in self-driving mode

    They didn't say it had self stopping, that's why she was there .... image

     

    I believe the one that killed someone they blamed on a white truck against a light background ... hello it's still a really large metallic object.!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to mcb1

    >I'm unsure how you can make this statement

    >>Nearly in every case of the accidents involving self-driving vehicles, human error was that cause of the problem and not the autonomous vehicle

     

    I agree with Mark. I also think marketing hype has something to do with this.

    We test drove a Tesla last winter, and were told all about the self driving capabilities yada-yada-yada. But as part of the sales pitch they never tell you the limitations and what it *cannot* do.

    This became obvious when my wife was at the wheel in self-driving mode and the car came up behind a commercial transport truck at speeds much too fast - she had to hit the brakes very hard to avoid a collision. The car obviously did not detect the truck, which was obviously a serious failure of that self-driving follow-traffic feature they were trying to sell us on.

    So that technology is lacking in a big way - seriously, missing a huge truck?

     

    -Nico

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
>