Circuit Protection
  • Technologies
  • More
Circuit Protection
Forum HELP!!!.... Blown Electric Mistress pedal
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Circuit Protection to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 48 replies
  • Subscribers 71 subscribers
  • Views 10205 views
  • Users 0 members are here
Related

HELP!!!.... Blown Electric Mistress pedal

Andy Betts
Andy Betts over 6 years ago

I have made a huge school boy error... i was looking at running my original Electric Mistress pedal for a recording I'm doing and needed to run it off an external power supply. I had a 18v supply to hand which I just needed to connect up to a DC plug so that I could power the pedal. In my haste, I accidentally connected the negative and voltage wires the wrong way round...... connected the pedal, switched on the power and I immediately heard a small pop and the smell of burning. I have blown an original 1977 Electro Harmonix Electric Mistress effects pedal worth around $500!!! however, i'm sure it's not dead yet, and it can be brought back to life... Hence this post.

 

For your reference I have attached the schematic.

 

can anyone advise the best place to start troubleshooting, I'm assuming anything on the ground side of things could have been the first thing to blow, and I'm thinking a transistor.... bearing in mind the 18v supply was connected to the ground, and the ground was connected to the voltage in. Anything can be replaced, the only issue is if the culprit ends up being the SAD1024 chip that's it... the pedal is a gonner. However I very much doubt the voltage got that far in the circuit to be honest (hopefully)

Attachments:
imageMistress_v2_schematic.pdf
  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 6 years ago +4
    Hi Andy, I wanted to understand the voltage regulator a little better so I built one on the bread board. My original intention was to also hook it up backwards to see how it failed. I have decided not…
  • Andy Betts
    Andy Betts over 6 years ago in reply to Andy Betts +4
    repaired... Transistor was around the wrong way
  • DAB
    DAB over 6 years ago +3
    Bad luck is a pain. I looked over your schematic and you will probably need to replace all electrolytic capacitors as they do not tolerate being hooked up wrong. If you smelled or saw smoke, you probably…
Parents
  • jw0752
    jw0752 over 6 years ago

    Hi Andy,

     

    I wanted to understand the voltage regulator a little better so I built one on the bread board. My original intention was to also hook it up backwards to see how it failed. I have decided not to waste the parts as the way your BC 309 failed is excellent evidence that reversed voltage got past the regulator to your circuit. Here is my set up:

     

    image

     

    image

    Output voltage of the regulator circuit

    image

    Load current on the regulator circuit.

     

    The voltage input to the regulator above is 18.3 Volts and the Output voltage is 13.35. It is under a load of 42 mA. I found that this was all the load that I could put on the regulator before it started to pull the voltage down. To me this indicates that your circuit that is being powered by the regulator can be expected to take something less than 40 mA. I mention this as you should be able to try to power the 13 Volt rail with a current limited power supply. As long as the current draw is below the 40 mA things may be OK. If you see any sign that the circuit tries to draw more than 40 mA you will have to continue to search for problems and damaged components.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jw0752
    jw0752 over 6 years ago

    Hi Andy,

     

    I wanted to understand the voltage regulator a little better so I built one on the bread board. My original intention was to also hook it up backwards to see how it failed. I have decided not to waste the parts as the way your BC 309 failed is excellent evidence that reversed voltage got past the regulator to your circuit. Here is my set up:

     

    image

     

    image

    Output voltage of the regulator circuit

    image

    Load current on the regulator circuit.

     

    The voltage input to the regulator above is 18.3 Volts and the Output voltage is 13.35. It is under a load of 42 mA. I found that this was all the load that I could put on the regulator before it started to pull the voltage down. To me this indicates that your circuit that is being powered by the regulator can be expected to take something less than 40 mA. I mention this as you should be able to try to power the 13 Volt rail with a current limited power supply. As long as the current draw is below the 40 mA things may be OK. If you see any sign that the circuit tries to draw more than 40 mA you will have to continue to search for problems and damaged components.

     

    John

    • Cancel
    • Vote Up +4 Vote Down