Circuit Protection
  • Technologies
  • More
Circuit Protection
Forum Have a question about Circuit Protection? Ask our Expert, Abhishek Rao
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Circuit Protection to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 26 replies
  • Subscribers 71 subscribers
  • Views 3495 views
  • Users 0 members are here
  • expert
  • overcurrent_protection
  • littelfuse
  • circuit_protection
  • question
Related

Have a question about Circuit Protection? Ask our Expert, Abhishek Rao

AbhishekRao
AbhishekRao over 15 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Power Management in the element14 Community Power Management group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community

image

 

Abhishek Rao

Abhishek is a technical team lead and has extensive experience and expertise in the field of circuit protection. He holds B.E in Electronics & Telecom Engineering and extends application support for the Littelfuse line of products.


  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    I have a heating problem with a CB. Here is its the description:- ABB  S282  UC  K 10A

    Any specs. that you can supply will be very much appreciared.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • AbhishekRao
    AbhishekRao over 14 years ago in reply to e14 Contributor

    Hi,

     

    Most circuit breaker problems are due to loose electrical connections; however, there are some inheritance problems with specific brands of circuit breakers.

    When a circuit breaker trips, it releases a cocked spring mechanism that separates the electrical contacts. Circuit breakers have two means of tripping:

    1. An electromagnet that trips almost instantaneously when the current is between nine (9) and 15 times the rated current of the circuit breakers.

    2. A temperature sensitive bimetal strip that bends and releases the spring mechanism at a calibrated temperature. Usually, the temperature of the bimetal strip is proportional to the amount of current passing through the circuit breaker. However, the bimetal strip will react and bend to any rise in temperature. The rise in temperature may be due to a loose wire connection, misalignment of the circuit breaker contacts, or the heat from a fire.

    Hence to overcome the heating problem kindly check if the breaker contacts or connections are proper.

     

    Thanks & Regards,

     

    Abhishek.R.Rao

     

    Technical Support team

    element14

    www.element14.com

    Disclaimer:

    The ultimate decision on the suitability of parts or advice in the customer's application is solely a decision that should be made by your customer.

    P Please consider the environment before printing this email

     

     

     

    From: ramongk

    Sent: Tue 2/14/2012 9:31 PM

    To: Abhishek Rao

    Subject: - Re: Have a question about Circuit Protection? Ask our Expert, Abhishek Rao

     

     

     

     

    Re: Have a question about Circuit Protection? Ask our Expert, Abhishek Rao

    created by Ray King in Circuit Protection - View the full discussion

     

     

    I have a heating problem with a CB. Here is its the description:- ABB  S282  UC  K 10A

    Any specs. that you can supply will be very much appreciared.

    Reply to this message by going to element14

    Start a new discussion in Circuit Protection at element14

    Sitemap | Feedback & Support | Contact Us | Terms of Use | FAQ | About element14

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to AbhishekRao

    Thank you Abhishek

     

    Our solar panels were only installed about three months ago. The array is divided into two groups of ten panels each. Each DC circuit is protected by a CB just before it enters the inverter.

    The nominal capacity is a total of 4 kW with each DC circuit carrying 8.2 A. The breakers are double pole and have a rating of 10 A. They are mounted side by side in a fairly roomy but airtight plastic box.

    I shall call them (A)and (B). (B) has tripped once in December, once in January and three times in February. The first time, the plant had been operating at 50% capacity for 14 days before I noticed it. (There is no alarm for this condition.) Since then I have been keeping a constant survellance.

    Yesterday was a fine summer day with a clear blue sky. I read the LCD display on the inverter at about midday and an average current in (A) was about 7.9 A and in (B) 8.4 A + peaks up to 8.8  (A cooling breeze on a hot day improves the efficiency of PV cells, causing the displayed results to vary constantly.)

     

    I have proved that the conductors are securely fixed to the terminals and that's all that I can do. I have also discovered that after the plant has been operating at near maximum OP and placing ones fingertips on the top of each CB, the temperature is such that I cannot bear it for more than 5-10 seconds. I deduce from this and from the information supplied by you that the CBs are of the bi-metal type. I have been in touch with the installer who seems to give this problem a low priority and I have no date for repairs. I suspect he will replace CB (B).  I am concerned that prolonged operation at such high temperature will have a detrimental effect over time.

    Maybe I am wrong. Would you like to express an opinion about this?

     

    Many thanks, Regards, Ray

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • AbhishekRao
    AbhishekRao over 14 years ago in reply to e14 Contributor

    Hi Ray,

     

     

     

    Use of CB is not recommended by IEC or UL Standard for Solar Panel Protection, both these standard recommends the use of specially designed Solar fuses for Solar Panel Protection.

     

     

     

    Every time CB operates it loses the efficiency & will not have the same efficiency again & will start leaking current.

     

     

     

    The uniqueness of Solar fuses when compared to CB are, solar fuses can protect the Solar panels against lower levels of fault current in the order of 1.3In (where In is the rated current of the panel), this feature is not offered by CB, hence it is highly recommended to go for Solar fuses instead of CB.

     

     

     

    In the past CB were used for domestic installation but with many reported field failures, we see customers moving towards Solar Fuses.

     

     

     

    Currently in the market the maximum current rating available for Array Junction Box fuses used in Solar Plant is 30A only (32A fuse rating is not available), and Littelfuse is the only manufacturer to have 30A fuse available in 10X38 size. The part number of the fuse is 0SPF030.T0SPF030.T and the fuse is rated for 1000Vdc or less, hence suitable to be use in 48Vdc conditions.

     

     

     

    Below is the datasheet for the fuse, please go through it :

     

     

     

    http://www.littelfuse.com/data/en/Data_Sheets/Littelfuse-Fuses-Solar-SPF.pdf

     

     

     

    http://in.element14.com/jsp/search/results.jsp?N=0&Ntk=gensearch&Ntt=0SPF&Ntx=mode+matchallpartial&suggestions=false&ref=globalsearch&_requestid=1950457&isGoback=false&displaytext=&isRedirect=false

     

     

     

    Hope this addresses your concern.

     

     

     

    Thanks & Regards,

     

    Abhishek.R.Rao

     

    Technical Support team

    element14

     

    www.element14.com <http://www.element14.com>

     

    Disclaimer:

     

    The ultimate decision on the suitability of parts or advice in the customer's application is solely a decision that should be made by your customer.

     

    P Please consider the environment before printing this email

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • schuetma
    schuetma over 14 years ago in reply to AbhishekRao

    Hi Abhishek

     

    I appreciate your comment about fuse and CB technology. Nevertheless I would like to mention that beside the Littelfuse product there is as well the Schurter Solar Fuse and Solar Fuse holder available.

     

    http://in.element14.com/jsp/search/browse.jsp;jsessionid=OJRNGFVVIMYJGCWNBBSBFWI?N=0&Ntk=gensearch&Ntt=aso&Ntx=mode+matchallpartial&suggestions=false&ref=globalsearch&_requestid=1746267

     

    http://www.schurter.co.uk/var/schurter/storage/ilcatalogue/files/document/datasheet/en/pdf/typ_ASO_10.3x38.pdf

     

    http://in.element14.com/jsp/search/browse.jsp;jsessionid=OJRNGFVVIMYJGCWNBBSBFWI?N=0&Ntk=gensearch&Ntt=fso&Ntx=mode+matchallpartial&suggestions=false&ref=globalsearch&_requestid=1747885

     

    http://www.schurter.co.uk/var/schurter/storage/ilcatalogue/files/document/datasheet/en/pdf/typ_FSO.pdf

     

    Best regards

    Martin Schuetz

    Schurter Ltd.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to AbhishekRao

    Hi Abhisuek

     

    Thank you very much for your informative information and comments. ( I suppose I should have stated that we have a grid feed-in inverter.)

     

    I also wish to thank Mr Schuetz for his contribution.

     

    Weather conditions are contributing to even higher generating figures and for the time being, I have managed to control the temperature of the CBs by propping open the transparent flap on the front of the mounting box while the weather remains fine.

    Here in Australia, the regulating authority has knowledge of a small percentage of CBs being installed incorrectly and has ammended the rules to include the use of non-polarized isolators. Casual inquiries to date, indicate that the use of isolators has become preferred to that of CBs. I have yet to discover the position with regard to the use here of fuses.

     

    Thanks once more.

    Regards, Ray

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to AbhishekRao

    Hi Abhisuek

     

    Thank you very much for your informative information and comments. ( I suppose I should have stated that we have a grid feed-in inverter.)

     

    I also wish to thank Mr Schuetz for his contribution.

     

    Weather conditions are contributing to even higher generating figures and for the time being, I have managed to control the temperature of the CBs by propping open the transparent flap on the front of the mounting box while the weather remains fine.

    Here in Australia, the regulating authority has knowledge of a small percentage of CBs being installed incorrectly and has ammended the rules to include the use of non-polarized isolators. Casual inquiries to date, indicate that the use of isolators has become preferred to that of CBs. I have yet to discover the position with regard to the use here of fuses.

     

    Thanks once more.

    Regards, Ray