Circuit Protection
  • Technologies
  • More
Circuit Protection
Forum How to decide the Temperature range of an IC??
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Circuit Protection to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 3 answers
  • Subscribers 74 subscribers
  • Views 7550 views
  • Users 0 members are here
Related

How to decide the Temperature range of an IC??

rishi2628
rishi2628 over 10 years ago

I am using a MAX3241E ic in a device that has to run 24x7 out in the open. I am facing a problem deciding the temperature range of the the IC. Since it is out in the open, the ic has to withstand the heat from the sun plus the heating effect due to losses and resistances, etc. I am living in Delhi, India and here the temperature easily reaches 35 degrees. This ic that I have choosen can bear a max temp of 70 degrees. Should I use this ic or should I go for a higher temperature one? Also please tell how should one decide the max temperature of any ic?

 

Datasheet of the IC: - http://www.mouser.com/ds/2/256/MAX3222E-MAX3246E-99333.pdf

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 10 years ago +2 suggested
    Hi Rishi, This chip should have no problem operating where the ambient temperature is 35 degrees C or even in the full sun light though it isn't a good idea to leave it exposed to the direct sun or the…
  • D_Hersey
    D_Hersey over 10 years ago +1
    Hi, John, I trust that you are well. Thermo-electric cooler, also called a Peltier cooler. Very useful in chilling detectors in telescopes, for example
  • D_Hersey
    D_Hersey over 10 years ago +1
    On the topic of TECs, I would like to try to use them for crystal growing. I would pour a nearly boiling saturated solution of, say, copper sulphate, into a squarish glass container. I would have washed…
Parents
  • jw0752
    0 jw0752 over 10 years ago

    Hi Rishi,

     

    This chip should have no problem operating where the ambient temperature is 35 degrees C or even in the full sun light though it isn't a good idea to leave it exposed to the direct sun or the rain. If it is protected and the case is in the sun light I would expect ambient temps in the enclosure to rise to as much as 50 degrees C. This should still be acceptable for the operation of the chip but be sure to factor this temperature into your design as other components may drift from nominal values at this temperature. If self heating of the IC is an issue it will likely be covered in the data sheet with specific directions for heat sinking the component. I could find nothing about heat sinking on this IC.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 10 years ago

    Hi Rishi,

     

    This chip should have no problem operating where the ambient temperature is 35 degrees C or even in the full sun light though it isn't a good idea to leave it exposed to the direct sun or the rain. If it is protected and the case is in the sun light I would expect ambient temps in the enclosure to rise to as much as 50 degrees C. This should still be acceptable for the operation of the chip but be sure to factor this temperature into your design as other components may drift from nominal values at this temperature. If self heating of the IC is an issue it will likely be covered in the data sheet with specific directions for heat sinking the component. I could find nothing about heat sinking on this IC.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • rishi2628
    0 rishi2628 over 10 years ago in reply to jw0752

    will this ic work for an ambient temperature of 45 degrees??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 10 years ago in reply to rishi2628

    All IC's operating temperatures are documented in their data sheets however there are three general temperature specifications that almost all ICs use:

     

    Commercial  0 deg. C to 70 deg. C

    Industrial  -40 deg. C to 85 deg. C

    Military to -55 deg. C to 125 deg. C