Circuit Protection
  • Technologies
  • More
Circuit Protection
Forum Transistors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Circuit Protection to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 71 subscribers
  • Views 961 views
  • Users 0 members are here
Related

Transistors

e14 Contributor
e14 Contributor over 16 years ago
Is a

BC549 TO-92 NPN general purpose transistor any good for the below schematic?

 

Sorry the schematic is 2 images but I couldn't fit it all on one screen.

 

Cheers,

Chris

Attachments:
Led Cube Schematic.rtf
  • Sign in to reply
  • Cancel
Parents
  • Catwell
    0 Catwell over 16 years ago

    Chris,

     

    As long as the LED draw doesn't exceed the transistor limits, you're fine.

     

    I look forward to seeing your final creation.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to Catwell

    Cheers Cabe,

     

    I was impressed with myself when I drew that up lol.

     

    Chris.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • WarrenW
    0 WarrenW over 16 years ago in reply to e14 Contributor

    It looks very much like you will be multiplexing the outputs and will only be switching on any pair of transistors for a brief period. As long as you do not exceed the current limitations of the BC547 100mA or 200mA pulsed you should be ok.

    I would seriously suggest a current limiting resisitor in the supply lines to each of the three top transistors or even better a constant current source (depends on the number of LEDS you want on in any one branch at a time). The calculation of current is simple if you have only one LED on at a time and due to the high speed switch available with components and the slow decay response of the LED technology this is a practicle solution by strobing the LEDS they will appear to be on at the same time.

     

    Cheers

    Warren

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • WarrenW
    0 WarrenW over 16 years ago in reply to e14 Contributor

    It looks very much like you will be multiplexing the outputs and will only be switching on any pair of transistors for a brief period. As long as you do not exceed the current limitations of the BC547 100mA or 200mA pulsed you should be ok.

    I would seriously suggest a current limiting resisitor in the supply lines to each of the three top transistors or even better a constant current source (depends on the number of LEDS you want on in any one branch at a time). The calculation of current is simple if you have only one LED on at a time and due to the high speed switch available with components and the slow decay response of the LED technology this is a practicle solution by strobing the LEDS they will appear to be on at the same time.

     

    Cheers

    Warren