• Products and Partners
    Products and Partners
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
Code Exchange
  • Technologies
  • More
Code Exchange
Blog C++ Tutorial - Hello Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: oneleggedredcow
  • Date Created: 2 Jan 2013 2:53 AM Date Created
  • Views 13947 views
  • Likes 9 likes
  • Comments 13 comments
  • Code Exchange
  • raspberry_pi
  • code
  • rpi
  • c++
  • learnc++
Related
Recommended

C++ Tutorial - Hello Raspberry Pi

oneleggedredcow
oneleggedredcow
2 Jan 2013

Background

In this tutorial series, we are going to learn modern c++ using the raspberry pi.  So, what do I mean when I say modern?  In August of 2011, a new version of the c++ standard was released that included some exciting new features.  So, in this tutorial series, we will be taking advantage of these enhancements.

 

This tutorial series will start with the basics and then quickly move on to more advanced topics. Occasionally, we will take a step back and use what we have learned so far to do a project, so that you can exercise the skills that you have learned and build something exciting.  By the end, you should have a great foundation in c++ that you can use to build your own projects.

Setup

For this tutorial series, we are going to be using the Raspbian OS.  It’s very easy to install and set up and it seems to be the most popular OS for the raspberry pi.  Raspbian comes with all of the tools that we need to start programming, so let’s dive in.

Code

Here’s the code to print out a message to the screen:

 

#include <iostream>

using namespace std;

 

 

int main()

{

          cout << "Hello Raspberry Pi!" << endl;

          return 0;

}

 

The first line includes a library.  Libraries are prewritten code that you can leverage to do things faster and easier. Many common functions, such as writing a message to the screen, have already been written, so you can just reuse them and focus on aspects of your program that are unique to the problem that you are trying to solve.

 

The next line makes it so that you don’t have to prefix the functions in the library with the name of the namespace that it is in.  This is to help fix name collision problems.  Imagine if I wrote a function called foo and someone else wrote a function with the exact same name.  If I tried to call that function the computer wouldn’t know which one I wanted, so to help with this namespaces were created.  This line tells the computer that if it is looking for a function, that it should start by looking in the std namespace.

 

The next line declares a function.  A function is a group of code that takes a set of inputs and produces an output.  A simple example would be a sine function. The function would take in an angle, do some computations on that angle and then return the sine of the given angle. This function is called main and it doesn’t take any inputs, so there are just empty parenthesis after the name of the function.  The function returns an error status.  This is used to let other programs know if the program succeeded or failed.  The main function is a very special function. It lets the computer know where your program starts, so every program must have a main function.

 

The curly braces signify the start and end of the function.  Inside the function we only have two lines. The first one writes the phrase given to the screen, and the second one tells the computer that the program succeeded.  If you change the text in between the two double quotes, you can make the computer write anything that you want to the screen.

Compiling and Running

So, take the above code and paste it into a file called 01_HelloRPi.cpp.  Now open up a command prompt and navigate to the directory that contains the file.  In the command prompt type:

 

g++ -std=c++0x 01_HelloRPi.cpp -o01_HelloRPi

 

This will take the code that you have written and create a program that can be run.  The name of the program to create is specified with the –o flag, in this case we called it 01_HelloRPi.  The –std=c++0x flag tells the compiler to use the latest version of the c++ standard.  Then to run the program type in:

 

./01_HelloRPi

 

And that will write your message to the screen.

Summary

In this first tutorial we set up our environment to get ready to code and wrote a small program that prints a message to the screen.

 

In the next tutorial, we discuss how to read in data from the user to make an interactive program.

 

If you have any questions or comments about what was covered here, post them to the comments.  I watch them closely and will respond and try to help you out.

Tutorial Index

01 - Hello Raspberry Pi

02 - Reading User Input

03 - If Statement

04 - For Loops

05 - While Loops

06 - Functions

07 - Data Types

08 - Arrays

09 - Structures

10 - Classes

11 - Pointers

12 - Dynamic Arrays

13 - Linked List

14 - Linked List Operations

15 - STL List/Vector

16 - Templates

17 - Inheritance

18 - File I/O

19 - Strings

20 - Constants

21 - Hash Tables

Attachments:
01_HelloRPi.cpp.zip
  • Sign in to reply

Top Comments

  • oneleggedredcow
    oneleggedredcow over 11 years ago in reply to shabaz +3
    Thanks shabaz , it was great to see your comments today! I also updated my previous response. (That's what I get for trying to answer a question in a rush!)
  • mcb1
    mcb1 over 11 years ago in reply to shabaz +3
    Well said Shabaz!. Strangely it takes some people a lot of time to learn that constructive critisism usually results in a better outcome. Using your own experiences with poor service/experience and projecting…
  • Anonymous-342052
    Anonymous-342052 over 11 years ago +3
    This is a REALLY COOL tutorial
  • oneleggedredcow
    oneleggedredcow over 11 years ago in reply to shabaz

    Thanks shabaz, it was great to see your comments today!

     

    I also updated my previous response.  (That's what I get for trying to answer a question in a rush!)

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago

    Hi Chip,

     

    You were rude. Provide your feedback in a polite manner, or keep it to yourself.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago

    Shaun wrote and has stood by this tutorial for two years, and is responding to you at no cost, and has been polite throughout.

    You've come to it now, and speak of being frustrated from the many experiences _you_ have had talking to programmers as you say.

     

    You talk about programmers having bad communication skills, yet you were the one that was incapable of conveying your findings without being rude. It's not an opinion, it's a fact:

     

    Chip Reuben wrote:

     

    Once again you are incomplete, and in this case just plain wrong. In order to get BOTH OUTPUT AND ERROR to write to the file, you have to use:

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago

    Hi Chip,

     

    Firstly, Linux shell specifics can be obtained from all over the Internet, it's not a big deal.

    Shaun's tutorial covers some C/C++ essentials really well - there may be some typo's but they are easily resolved in the discussion comments, which Shaun is doing, and so are you, _but_ :

    Chip Reuben wrote:

     

    Once again you are incomplete, and in this case just plain wrong. In order to get BOTH OUTPUT AND ERROR to write to the file, you have to use:

     

     

    It sounds from your rude response that you are frustrated with the tutorial. If that is the case, as a suggestion, please keep it civil or to yourself, because no-one wants to hear it. Shaun has spent a lot of effort preparing the tutorial, as a former C++ developer I can confirm that it is mostly error-free (more error-free than some textbooks) and politeness costs nothing from you.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • oneleggedredcow
    oneleggedredcow over 11 years ago

    I think I fixed the problem with copying and pasting the compile line.  It looks like the second "-" is a weird character.

     

    If the errors are overflowing your screen, try writing the output to a file.  To redirect the standard output (stdout), just add a "> file" to the end of your command.  However, compile errors go through the error output (stderr).  In that case you can redirect the output to a file with a "2> file".  It is also pretty common to want to capture both of them.  To do this add a ">& file".  This will redirect the error output (stderr) into the same stream as the normal output (stdout).  So, in this case:

     

    g++ -std=c++0x 01_HelloRPi.cpp -o01_HelloRPi >& errors.txt

     

    Now errors.txt will contain all of the output from the compilation (from stdout and stderr).  Just open up that file and then you can see what is going on.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>