Connector Technology & Design
  • Technologies
  • More
Connector Technology & Design
Polls Poll: How Can Connectors Be Improved?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Connector Technology & Design to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 29 Aug 2019 7:23 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:59 PM
  • Views 2650 views
  • Likes 2 likes
  • Comments 13 comments
Related
Recommended

Poll: How Can Connectors Be Improved?

Improve. Diversify. Innovate. Evolve. I see these terms applied to the current trends in connector technology nearly every day. Connectors are faster, smaller, offer more protection, more durable and can handle higher currents in a smaller package. There are explosion proof connectors, switch-rated connectors and smart connectors. Connectors will continue to evolve...but how?

 

In what area do you see a need for connectors to improve?

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • 14rhb
    14rhb over 7 years ago +7
    cstanton comment about heat made me think, A friend showed me their cooker some weeks ago which has developed many faults over the years - I'll withold the manufacturer's name so as not to get in a legal…
  • koudelad
    koudelad over 7 years ago +5
    Connectors are getting smaller and smaller. However, the signal cables (with a demand on increasing data speed rate and getting through more power) are tougher and thicker - more cable pairs, more shielding…
  • 14rhb
    14rhb over 7 years ago +3
    That could go a number of different ways as listed. On the subject of connectors it would be nice if automobile manufacturers used the same connector on a particular model - I can spend a huge amount of…
  • dougw
    dougw over 7 years ago

    I think there is a lot of scope to design better PCB-mounted connectors, especially panel-mounted PCB connectors. I love to use PCB-mounted connectors in my designs and I hate making wiring harnesses to go from PCB to panel connector. There are several significant issues with PCB-mounted panel connectors that often have poor solutions or no solutions. But it is possible with a little thought to make good solutions and hopefully with enough thought they can be low cost.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • koudelad
    koudelad over 7 years ago

    Connectors are getting smaller and smaller. However, the signal cables (with a demand on increasing data speed rate and getting through more power) are tougher and thicker - more cable pairs, more shielding etc. This creates a huge leverage on the connector soldered to a board.

     

    One practical example: I got a new laptop with USB-C. In order to push up to 100 W, monitor image and USB port, it had such a tough cable, I damaged the connector during insertion.

    If you take this to a repair center, they say it is mechanical damage, of course. It made me angry, because I am extra cautious and never broke a single micro USB connector.  (And I have seen many of them broken by other people.)

     

    Do you also see a need for "not so small and fragile" connectors for consumer electronics?

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 7 years ago

    That could go a number of different ways as listed.

     

    On the subject of connectors it would be nice if automobile manufacturers used the same connector on a particular model - I can spend a huge amount of time working out how to disengage the locking mechanism only to move onto the next component (on the same vehicle) and find a completely different connector. Its like some sort of Mensa test!

     

    Connector pin density will likely increase, perhaps without many more additional pins but in a smaller form factor. Take the FMC connectors on the Xilinx boards as an example of high density: FMC Connectors

     

    I also have recently become aware that some connectors have very limited number of mating cycles before they degrade, eg the U.Fl connectors used on Molex antennas Molex 2.4GHz / 5GHz Antenna Kit - Review

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<