Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog Debugging Embedded Systems: the Problems and Solutions
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 10 Jun 2016 10:57 AM Date Created
  • Views 1459 views
  • Likes 1 like
  • Comments 5 comments
  • somnium
  • ide
  • drt
  • somniumdrt
  • eclipse
  • arm cortex-m
  • live expressions
  • debugging
Related
Recommended

Debugging Embedded Systems: the Problems and Solutions

e14 Contributor
e14 Contributor
10 Jun 2016

This blog is the first in a series on the new debug features in SOMNIUM DRT.

We all know from experience (and this is confirmed by many studies) that debugging takes up a significant part of the time in software development. Software systems are complex and debugging is hard. This is especially true for embedded systems where there may be real-time constraints on when data is received or sent, the timing of interrupts, and so on. This means that traditional techniques, such as breakpoints or changing to code to print out state information, cannot be used because they will drastically change the timing and therefore the behavior of the program. Program flow is often controlled by asynchronous and external events, for example inputs from touch sensors and other peripherals. Therefore the real-time behavior of the program cannot be understood simply by looking at the control flow in the source code.

SOMNIUM DRT includes features to support debugging embedded systems. One of these enables the live, non-intrusive display of interesting data. Another is the ability to trace program flow so you can step backwards and forwards through the execution history to see how you to to a particular state.

SOMNIUM DRT is is a set of development tools for ARM Cortex-M based devices [such as the Kinetis and LPC devices from NXP and the STM32 devices from STMicroelectronics]. It is fully compatible with industry-standard tools such as the GNU toolchain and Eclipse IDE. DRT uses our patented techniques to produce highly optimized code by exploiting information about the embedded processor, the memory system and other peripherals to deliver improved performance, lower code size and reduced energy use.

It also includes some great debugging tools such as trace, live expressions and fault diagnosis.

Live Expression View

The first of these is the live view of expressions. This enables you to see the value of global variables, and expressions using them, change as the program runs. This is minimally intrusive - it cycle-steals from the bus to grab the data but does not affect the processor itself - so there is far less chance that it will change the behavior of the running program. There are no source code changes required, you just need to click the icon in the expressions view to enable live updates. The debugger will periodically read the selected memory locations and update the values in the expressions view without interrupting program execution.

This video is unavailable.
You don't have permission to edit metadata of this video.

A free trial of DRT is available. DRT is able to automatically import projects from other Eclipse-based development environments, making it simple to migrate your projects to DRT so you can quickly see the benefits for yourself. Download your free trial today and try out these powerful debug features for yourself.

  • Sign in to reply
Parents
  • DAB
    DAB over 10 years ago

    In formal engineering, we use the term testing.

     

    Test planning begins with requirements and is fleshed out during design.

     

    Often, the level of effort for testing is equal to or exceeds the effort to design and build a device.

     

    So some tools can help, but good testing/debugging begins with a full understanding of your system and what it needs to do, followed by a defined test to verify that the device works as expected.

     

    I have been on many a program where little or no budget was spent on test planning and disaster usually followed.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to DAB

    Hi DAB,

    I think that testing and debugging are rather different processes. However, I agree completely that having a good specification and a test plan right up front can reduce both the time spent debugging and the time spent testing.

    Jamie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to DAB

    Hi DAB,

    I think that testing and debugging are rather different processes. However, I agree completely that having a good specification and a test plan right up front can reduce both the time spent debugging and the time spent testing.

    Jamie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • DAB
    DAB over 10 years ago in reply to e14 Contributor

    True, debugging begins as soon as something does not test to expectations.

     

    That is why a good test plan has enough component tests included to make sure that the hardware is working to spec.

     

    Then you can trace through the software to see where the data is being incorrectly processed.

     

    That is why I always test one thread at a time.  It limits your focus and keeps interoperability issues to a minimum.

     

    DAB