Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog ESP32 Cheap Yellow Display (CYD) Guide with a Jellyfish example
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 29 Mar 2026 6:15 PM Date Created
  • Views 20673 views
  • Likes 8 likes
  • Comments 7 comments
  • esp32
  • platformio
  • espressif
  • Cheap Yellow Display
  • CYD
  • ESP32-2432S028
Related
Recommended

ESP32 Cheap Yellow Display (CYD) Guide with a Jellyfish example

shabaz
shabaz
29 Mar 2026

Table of Contents

  • Introduction
  • CYD Features
  • Board Dimensions / Technical Drawing
  • Is It Any Good?
  • CYD Connections Reference
    • RGB LED
    • Micro SD Socket
    • UART and BOOT pin
    • Audio Output
    • Spare Input/Output Connections
    • Touch Interface
    • TFT Screen, Backlight and Light Sensor (Light Dependent Resistor)
  • Install VS Code, and PlatformIO Extension
  • Download the Jellyfish Project
  • Open the Project Folder in VS Code
  • Build the Project
  • Uploading Firmware to the Board
  • Summary

Introduction

The Cheap Yellow Display (CYD) is a very low-cost board with a 2.4” RGB TFT screen on one side, and an ESP32 module on the other! The formal name is ESP32-2432S028 but it’s known as the CYD for self-explanatory reasons.

I recently saw a project on Hackaday.io (a site I usually ignore, because most projects documented there are incomplete, usually missing schematics or code) and was happy to see the author had provided a GitHub repository link to the code. The project used the CYD, and I thought it would be a nice gift for my little niece.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

This blog post describes the CYD, the connections present on it, and how to go about using the CYD! It's a very short process; about an hour from start to finish.

In brief, using the CYD entails connecting it to the PC using the supplied USB cable, and then in terms of the software environment, one can install Visual Studio Code (VS Code), and then withing that select to install an extension called PlatformIO, and that will provide task items in a list, that can be clicked to build code, and upload it to the board. All the steps are described further below. The example project will be the jellyfish project as mentioned above.

CYD Features

The CYD diagram here shows what’s on the board, and it can be used as a pinout reference when coding.

image

The component side has an ESP32 module (PDF Datasheet) with approximately 4 Mbyte Flash, and about 520k RAM, 2.4 GHz wireless LAN capability, and Bluetooth Low Energy (BLE).

There is also an RGB LED, a 1W audio amplifier, Micro SD card socket (very useful for logging or configuration files for projects) and very few spare GPIO connections brought out to a couple of connectors.

The board I purchased had both USB-C and Micro-USB connectors, but they are attached to the same signals, so both must not be used simultaneously.

Power entry can come from either the connector labelled P5, or either of the USB sockets. Software can be debugged using the USB Serial interface present on the USB connectors, or using an external USB-UART adapter connected to P5.

There are boot and reset buttons, which are needed during device programming.

image

The other side contains just the TFT touchscreen, and a little light sensor (Light Dependent Resistor).

image

Board Dimensions / Technical Drawing

The overall board is 86 x 50 mm, it's a standard 1.6 mm thick PCB. The 70 x 50 mm TFT screen has a 4 mm height above the board surface. Visible area is 59.5 x 45 mm. 

On the other side of the board, most parts protrude 4 mm or less from the board surface, except the Reset and Boot buttons and the speaker connector which are all approx. 4.8 mm tall. 

Click the image to enlarge (all measurements are likely only accurate to within a millimeter, and may vary since not all CYD boards may be identical).

image

Is It Any Good?

The board arrives with a USB-C to Type A cable (a USB-C to USB-C cable will not work), and a short 4-wire cable if required for any external UART or GPIO connections, and a little plastic stylus, although the touchscreen can be pressed with fingers too.

The 2.4” 240 x 320 resolution TFT screen is very basic, the contrast is quite poor, but that’s to be expected at such a low price. I think it is very good value for money, and the board can be used for user interfaces (for example).

The board I purchased has space for an additional Flash chip to be installed, but that was not fitted on the board; the only Flash memory present is that inside the ESP32 module.

CYD Connections Reference

There isn’t an official schematic, but it’s possible to figure out the connections. Here they are!

Note: all connectors are Molex PicoBlade (1.25 mm pitch), sometimes known as JST 1.25 (even though JST doesn't manufacture them!).

RGB LED

There is a large RGB LED near the ESP32 module. The GPIO pins need to be pulled low to turn on the LEDs.

GPIO# Connection
4 Red Cathode
16 Green Cathode
17 Blue Cathode

Micro SD Socket

The Micro SD interfaces uses a Serial Peripheral Interface (SPI):

GPIO# Connection
5 *CS
23 MOSI
19 MISO
18 SCLK

UART and BOOT pin

The serial interface connects to both the USB connector (via a CH340C USB-to-Serial converter) and to a board connector P5, through 100 ohm resistors. A supplied cable can be used.

ESP32 Signal Name Description
RDX0 ESP32 Board Rx, and P5 pin 3 (Blue wire)
TXD0 ESP32 Board Tx, and P5 pin 2 (Yellow wire)

The detail for connector P5:

P5 Pin Description
1 5V Board Power Input (Red wire)
2 ESP32 Board Tx (Yellow wire)
3 ESP32 Board Rx (Blue wire)
4 GND (Black wire)

The ESP32 boot pin is GPIO#0, and it is connected to a push-button to the left of the ESP32. It may need to be held down, while tapping RST, when programming the board. The boot pin is also connected to the CH340C chip to try to automate the boot control from the PC during device programming, but it didn’t work for me, and I had to use the push-button.

Audio Output

One pin (GPIO26) is wired to an SC8002B audio amplifier IC, which is a 1W 8-ohm bridge-tied-load amplifier, wired to a 2-pin connector labelled SPEAK. The connection is through an RC filter. GPIO26 can be operated in a DAC mode (peripheral signal name DAC_2) or perhaps PWM could be performed (no idea).

image

Spare Input/Output Connections

A few GPIO pins are brought out to two connectors, called CN1 and P3.

CN1:

CN1 Pin Connection
1 3.3V
2 GPIO27
3 GPIO22 (also present on conn P3)
4 GND

P3:

P3 Pin Connection
1 GPIO21
2 GPIO22 (also present on conn CN1)
3 GPIO35
4 GND

Touch Interface

There is a resistive touch layer on the TFT screen, and it can be pressed by fingers or using the supplied stylus. The touch interface uses an XPT2046 IC (PDF datasheet) in a TSSOP package.

GPIO# Connection
36 Touch *PENIRQ (input to ESP32)
32 Touch DIN (MOSI output from ESP32)
39 Touch DOUT (MISO input to ESP32)
25 Touch DCLK (output from ESP32)
33 Touch *CS (output from ESP32)

TFT Screen, Backlight and Light Sensor (Light Dependent Resistor)

The TFT screen uses an ILI9341_2 software driver (Driver IC PDF datasheet). The reset pin is hard-wired to the board reset circuitry, i.e. a capacitor keeps it low at power-up briefly.

The Light Dependent Resistor (LDR) is attached to GPIO pin that may need a pull-up configured in software, perhaps.

GPIO# Connection
14 TFT SCLK
2 TFT DC (Data/*Command)
15 TFT *CS
13 TFT MOSI (ESP32 Output)
12 TFT MISO (ESP32 Input)
21 TFT Backlight PWM (High = ON)
34 (ADC1_CH6) Light Dependent Resistor to GND

Install VS Code, and PlatformIO Extension

To get going with the CYD, first install VS Code. Then, install the PlatformIO extension by following the steps shown in this screenshot:

image

Then, restart VS Code!

Later, you might see Installing PlatformIO Core messages at the bottom-right of the VS Code window at some point, such as when a project folder is opened. If you see that, let it complete, and then click Reload Now.

image

Download the Jellyfish Project

Create a general projects folder, for instance, C:\DEV\projects

Ensure you have git installed (install it using https://git-scm.com/download/win )

Open PowerShell, navigate to that general projects folder, and type the following, which will create a folder called denki-kurage and the source code will be placed there by the command:

git clone https://github.com/likeablob/denki-kurage.git

Open the Project Folder in VS Code

Go to File->Open Folder and select the downloaded project folder denki-kurage. Click to trust the folder if prompted.

You can view the code, by clicking on the left side explorer view, for instance, click on src and select main.cpp. The code will appear in the main pane.

You should see a load of messages appear in VS Code at the lower-right, regarding PlatformIO performing project configuration operations. It may take a quarter of an hour or so to complete, even on a fast PC, and it may well sit at 100% for quite a while, seemingly doing nothing, but let it complete. I wasn’t impressed by PlatformIO’s poor status messages and the crazily long install time.

Eventually you should see this:

image

Build the Project

Click on the PlatformIO icon on the left side icon bar, it looks like an alien head. Then click on cyd->General and then select Build.

image

You should see a load of messages appear at the bottom, followed by Success messages.

image

Uploading Firmware to the Board

Plug in the USB cable into to the board and into your PC. You should hear a Windows device installed sound after a few seconds. Windows Device Manager will show a port installed, in my case, it was COM3 but the number will vary.

image

The display on the board should be lit up, and may display an image that is part of any factory firmware that may be in Flash memory.

Look at the back of the board, and locate the two buttons. The top one is labelled RST (Reset) and the one below it is labelled BOOT. The plan will be to click on Upload in VS Code, and then when you see a Connecting… message appear, quickly press down BOOT, and while holding it down, press and immediately release RST. Then you can release BOOT. What this does, is essentially ensure that BOOT is pressed during a board reset.

Click on cyd->General->Upload, and notice the Connecting… text at the bottom:

image

Now, as soon as that text appears, hold down the lower button (BOOT), then tap the top button (RST) and then release BOOT. You should see some uploading messages appear, followed by Success messages:

image

Take a look at the LCD on the board, and a jellyfish should be present! Tap the jellyfish to change its colour.

image

The jellyfish happened to be on a white background which I didn't like, so I edited the src/config.h file, to add the following line:

#define CYD_INVERT_DISPLAY

After that, I re-built and re-uploaded the firmware, and all was well.

Summary

The Cheap Yellow Display is a very low cost ESP32 microcontroller board with built-in touchscreen TFT. To get going with it, VS Code was downloaded, a PlatformIO extension installed, and then it was just a matter of clicking to build and upload any code. My board required the BOOT and RST buttons to be used during the code upload process.

For next steps, I'd like to personalize the display, and maybe get it to display the time at the bottom too, so it can function as a desk clock. For other unrelated projects, the code could perhaps be used as a template, for custom code.

Thanks for reading!

  • Sign in to reply

Top Comments

  • shabaz
    shabaz 5 months ago +1
    Despite planning to rely on BLE for config, I realized that a minimal on-screen menu might be occasionally helpful for projects, for instance, to switch BLE on or off, or to enter a passkey to enable BLE…
  • shabaz
    shabaz 5 months ago in reply to shabaz +1
    I couldn't bring myself to use this module, after I realized it's a 5V RTC. Seems like a dead end to want to write code for it. Instead I've ordered some NXP PCF85263A chips, they seem to be a good compromise…
  • shabaz
    shabaz 4 months ago

    Measured up and added a board dimensions illustration to the blog with locations of the display center, board connectors, etc.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 5 months ago in reply to shabaz

    I couldn't bring myself to use this module, after I realized it's a 5V RTC. Seems like a dead end to want to write code for it. Instead I've ordered some NXP PCF85263A chips, they seem to be a good compromise between low price, availability and performance with a typical crystal won't be too bad. Plus it's quite low power, so a coin cell should last ages. There's actually already a library for it, so technically I don't need to write any code, but might do if that library is too bloated.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 5 months ago

    The menu is slowly coming along..

    There are just three types of things to tap on:

    (a) plain buttons,
    (b) buttons with a built-in value display, and
    (c) buttons with on/off slider.

    All the above can be individually dimmed as required, if (say) if an admin password is not entered.


    For almost zero additional code, the menu code is reused to provide "MsgBox"- type functionality (see Status in the video) by simply removing the Cancel button.

    Poor quality handheld video:

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    Another option could be to use LVGL, which apparently "ESPHome" uses, and then menus can be created with config files (I believe). It might be more heavyweight in terms of resource consumption though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 5 months ago

    Despite planning to rely on BLE for config, I realized that a minimal on-screen menu might be occasionally helpful for projects, for instance, to switch BLE on or off, or to enter a passkey to enable BLE or whatever.

    I'm sure menu systems must exist for the CYD, but I figured it would be worth starting from scratch, to ensure very little Flash and RAM is required, and to try to keep it very general, for flexibility.

    This uses C arrays, for storing each menu detail. There is a class called MenuSystem, with a displayMenu method, e.g.

    menu.displayMenu(MENU_TOP,  "-") would show the following:

    image

    So, if the user was to (say) press on the PWM button, then menu.displayMenu(MENU_PWM, "-") would be called (the "-" can be replaced with a default value so the user can see what's currently configured). And no backspace, just cancel to keep the code simple.

    image

    (The minus button shouldn't be there, that was a mistake in the array of button names for that particular menu).

    The code allows up to 12 arbitrary buttons per menu, which is just enough for numeric, but of course insufficient for full text extry (I think that would be tedious to enter on such a small screen anyway, so it would be better to just use the BLE menu option, then do the rest on the mobile phone.

    Once this is working I'll put it on GitHub.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 5 months ago in reply to kmikemoo

    Hi Mike, I thought I was using the site wrong too, until others concurred that it's hopeless! : (

    Just been experimenting with the code a bit this evening, and managed to get the ESP32 Bluetooth LE functioning, the plan is to use that to set the time (or the time could be set with the touch display, but I think BLE will be easier to work with, rather than a graphical user interface on that screen). And ordered this RTC, which has a coin cell holder on the back:

    image

    So, with that wired to the CYD, a clock display should be feasible! GPIO#21 and 22 are SDA and SCL it seems.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>