Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog MCU-less Industry-certified Bluetooth Low Energy Module from Microchip
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 23 Jul 2014 9:39 PM Date Created
  • Views 824 views
  • Likes 1 like
  • Comments 1 comment
  • bluetooth
  • low_energy
  • microchip
  • cabeatwell
  • mcu
  • wireless
  • communcation
  • power
  • pic
Related
Recommended

MCU-less Industry-certified Bluetooth Low Energy Module from Microchip

Catwell
Catwell
23 Jul 2014
image


The RN4020 Bluetooth Smart Module is Microchip Technology’s, first Bluetooth 4.1 Low Energy module. It comes industry-certified and functions completely as a stand alone or in conjunction with any microcontroller.

 

The module not only functional immediately but also carries various international certifications right out of the box, including certification from Bluetooth Special Interest Group.

 

The RN4020 Bluetooth module also comes with the Microchip Low-energy Data Profile pre-installed, enabling immediate compatibility across the BTLE network. It is also stack-on-board and can either connect directly to Microchip’s line of PIC MCUs with a UART interface (or any microcontroller with a UART interface) and it can operate independently for basic uses, such as the collection and transmission of data.

 

It’s the first of its kind at Microchip and the micro tech giant hopes to provide developers with an easy solution for the next generation of wireless products that will eat up less power.

 

Microchip hopes that its RN4020 revolutionizes the development of Internet of Things devices by providing energy-efficient access to Bluetooth technology on a chip. If MCU-powered devices gain access to Bluetooth, they can revolutionize the industry, enhancing a wide range of products, from consumables to medical devices.

 

Imagine if pacemakers, for example, began utilizing Bluetooth technology. The device would not only save the life of its host, but could even transmit critically important data to doctors, such as technical malfunctions and abnormalities. There are a lot of requirements for on patient products including FDA approval; off the shelf Bluetooth product are not necessarily certified for use in medical care.

 

The RN4020 LE Smart module comes preloaded with useful profiles, such as MLDP, Bluetooth SIG low-energy, public and private profiles via the ASCII command interface.

 

The RN4020 also comes equipped with a PCB antenna, capable of 7 dBm transmission and -92.5 dBm receiving sensitivity over 300ft. The module itself is 11.5 x 19.5 x 2.5 mm and will retail to manufacturers and developers at $6.78 each, sold in quantities of 1000 units.

 

C

See more news at:

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • DAB
    DAB over 12 years ago +1
    The wireless components are maturing quite nicely. The easier they can make it to connect, the more applications people will use them in. DAB
Parents
  • DAB
    DAB over 12 years ago

    The wireless components are maturing quite nicely.

    The easier they can make it to connect, the more applications people will use them in.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 12 years ago

    The wireless components are maturing quite nicely.

    The easier they can make it to connect, the more applications people will use them in.

     

    DAB