Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog Microchip releases the PIC24F MCU, hardware encryption, µA current!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 7 Jul 2014 10:52 PM Date Created
  • Views 587 views
  • Likes 0 likes
  • Comments 0 comments
  • hardware_encryption
  • microchip
  • pic24f
  • cabeatwell
  • microcontroller
  • encryption
  • pic
Related
Recommended

Microchip releases the PIC24F MCU, hardware encryption, µA current!

Catwell
Catwell
7 Jul 2014


Microchip Technology Inc., recently announced a new line of eXtreme Low Power PIC microcontroller that are more secure, more cost effective and feature faster throughput. Your home phone technology will never be the same.

 

Microcontrollers are tiny computers that are programmed for very specific functions, such as running our household appliances. They are also very unique, in that they must run on extremely low power and are expected to last for more than a decade or two.

 

From running the microwave and home phone to powering many emerging products within the Internet of Things, these cheap, simplistic chips power much of the world around us. Because of their importance, Mircrochip, a leading manufacturer of microcontrollers, decided to up its game-on-a-chip with its new XLP line, the PIC24F ‘GB2’ family.

 

The PIC24F line features a hardware crypto engine, One-Time-Programmable passcode storage and Random Number Generator for increased security. It also runs on less energy while in sleep mode, in which MCUs remain more than 90 percent of the time.

 

The PIC24F microcontroller line also features up to 128KB Flash and 8KB RAM hardware in packages that vary from 28 to 44-pin. Microchip says its line is ideal for IoT sensor nodes, security systems and units with keyless access. The microcontroller ‘giant’ also claims the GB2 line allows for faster throughput, longer battery life (180 µA/MHz Run currents and 18 nA Sleep currents), more secure data and lower cost.

 

Microchip is convinced its new nanotechnology will have a large impact within the world of the IoT. With enhanced security, PIC24F microcontrollers may find their way into the growing industry of home automation. Also, with longer battery life and less energy consumption, the PIC24F chip may become a favorite among pacemaker manufacturers too.

 

PIC24F GB2 chips will work seamlessly with Microchip’s entire line of programs and tools for developers. The chip will sell with and without USB access and will be available to manufacturers in SOIC, SSOP, SPDIP and QFN packages starting at $1.30 each when purchased in volume.

 

While the new microcontrollers will last longer and consume less power, it is often not the microchip, but the hardware of a device, that fails us long before the 20-year mark. Microchip told me during an interview at Sensor Expo 2014, they are definitely not expanding into the mobile (smartphone) industry. However, Microchip continued that they may find a way to extend the life of our household appliances then they will really be in business. Here’s hoping.


You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

C

See more news at:

http://twitter.com/Cabe_Atwell