Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog MSPM0 C++ project: service handler considerations
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 6 Sep 2026 3:21 PM Date Created
  • Views 137 views
  • Likes 4 likes
  • Comments 2 comments
  • gcc
  • MSPM0
  • easyL1105
  • c++
Related
Recommended

MSPM0 C++ project: service handler considerations

Jan Cumps
Jan Cumps
6 Sep 2026

You can use C++ for MSPM0 designs.
There's one watch-out: if you have your event handlers in a .cpp file, you have to wrap those functions in an extern "C" {} wrapper.

The SysConfig mechanism expect that the handlers have a particular name. But the C++ compiler will "mangle" function names in .cpp files. Surrounding the functions with the extern directive, tells the compiler to leave the function signature alone. 

In this example, I have a handler for a DMA interrupt. The SDK expects signature void DMA_IRQHandler (void).

If you don't wrap your handler, the linker will call the (predefined as weak) handler in the controller SDK's startup file. And that's a catchall handler (called Default_Handler) that 'll make the controller loop forever.
The linker will only have your handler called if its signature exactly matches the definition. Unmangled.
image

Because the default one in the SDK is flagged as weak, and your implementation not, the linker will ignore the SDK one and link in your function.

There are a few ways to wrap your handlers:

Surround the function

extern "C" {
void DMA_IRQHandler(void)
{
    /* Example interrupt code -- just used to break the WFI in this example */
    switch (DL_DMA_getPendingInterrupt(DMA)) {
        case DL_DMA_EVENT_IIDX_DMACH0:
            gChannel0InterruptTaken = true;
            break;
        default:
            break;
    }
}
}

Mark as external in with forward declaration

extern "C" {
    void DMA_IRQHandler(void);
}


// ...

int main(void)
{
    // ...
}

void DMA_IRQHandler(void)
{
    // ...
}

Both constructs have the same effect. 

There is no runtime cost. This is a build time mechanism to notify the toolchain. No code or data is added to your firmware.

  • Sign in to reply
Parents
  • shabaz
    shabaz 1 month ago

    Super useful! This is also handy if writing or porting a library of code that might be marginally more convenient in C just for a bit more portability (since some microcontrollers might not offer C++ compiler), and then using that everywhere, including C++ programs.

    I think I've not written any C++ for MSPM0 yet, looking forward to doing that, since it's quite hard restricting to plain C, I always get the urge to write classes..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz 1 month ago

    Super useful! This is also handy if writing or porting a library of code that might be marginally more convenient in C just for a bit more portability (since some microcontrollers might not offer C++ compiler), and then using that everywhere, including C++ programs.

    I think I've not written any C++ for MSPM0 yet, looking forward to doing that, since it's quite hard restricting to plain C, I always get the urge to write classes..