Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog New Sensor Hub from Texas Instruments Debuts at Design West
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: GardenState
  • Date Created: 25 Apr 2013 3:37 PM Date Created
  • Views 757 views
  • Likes 1 like
  • Comments 2 comments
  • design_west_2013
Related
Recommended

New Sensor Hub from Texas Instruments Debuts at Design West

GardenState
GardenState
25 Apr 2013

Texas Instruments has announced the Sensor Hub BoosterPack for its Tiva C Series TM4C123G LaunchPad at Design West 2013. The new BoosterPack is a plug-in daughter card that allows ARM Cortex-M4 MCU developers to create products with up to seven types of motion and environmental sensing capabilities. This BoosterPack and accompanying TivaWare software enables measurement of pressure, humidity, ambient and infrared (IR) light along with temperature and motion (including acceleration, orientation and compass).

 

Developers can use the board to create sensor fusion applications such as global positioning system (GPS) tracking, home and building automation, portable consumer electronics, games and many more applications.

 

The  BoosterPack leverages the processing, floating-point and communication capabilities of TI's Tiva C Series TM4C123GH6 ARM Cortex-M4 MCU for enhanced sensor accuracy. TI's TivaWare software, provided with the LaunchPad kit, includes a Sensor Driver Library, providing developers with a sensor fusion API and several example applications that demonstrate how each of the sensors operate individually or in collaboration.

 

Similarly, TivaWare software also includes the Peripheral Driver Library to configure and operate the on-chip peripherals with a set of example applications. These applications demonstrate the capabilities of the Tiva TM4C123GH6 MCU, as well as provide a starting point for users to develop their final applications.

  • Sign in to reply
  • Capper
    Capper over 13 years ago

    MSRP $49.99

     

    http://www.ti.com/general/docs/lit/getliterature.tsp?literatureNumber=spmt282&fileType=pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 13 years ago

    Did they indicate the range of the pricing for the hub?

     

    It looks like a promising way to begin to interface sensors to the Tiva processor line.

     

    It would also probably work with the MSP430 and C2000 launchpads.

     

    If you made some connectors, you could also probably attach it to an Arduino, Beagle or RPi.

     

    DAB